IGBT vs MOSFET: Which Power Switch for Your Application?

  • Home
  • SUPPLY CHAIN INSIGHTS
  • IGBT vs MOSFET: Which Power Switch for Your Application?

    When a power electronics designer sits down to choose a switching device, two options come up in almost every conversation: the MOSFET (Metal-Oxide-Semiconductor Field-Effect Transistor) and the IGBT (Insulated Gate Bipolar Transistor). Both are voltage-controlled, both can handle significant power, and both share a superficially similar gate drive interface. Yet underneath those similarities, the two devices are built around fundamentally different physics — and that physics determines which one belongs in a given design.

    Choosing wrong is not just an academic mistake. Putting a MOSFET where an IGBT belongs can mean excessive heat and wasted efficiency at high current; putting an IGBT where a MOSFET belongs can mean sluggish switching that limits operating frequency and inflates passive component sizes. This article walks through the structural differences, the electrical trade-offs, and the quantitative decision thresholds that separate one device’s natural territory from the other’s — so you can make an informed choice rather than a habitual one.

    Power Electronics Guide
    IGBT vs MOSFET

    Which power switch belongs in your design? A practical comparison of switching speed, voltage range, conduction loss, and real-world applications.

    <10 ns
    MOSFET Switch Time
    20 A
    Crossover Current @ 600 V
    6.5 kV
    Max IGBT Voltage
    MHz+
    MOSFET Frequency Range

    Head-to-Head Comparison

    M
    MOSFET
    • ▶ Unipolar — majority carriers only
    • ▶ Resistive loss: I² × RDS(on)
    • ▶ Switching: <10 ns, up to MHz range
    • ▶ Best voltage: Below 250–600 V
    • ▶ Gate drive: 10–15 V
    • ▶ No tail current — fast clean turn-off
    ⚠ Limitation

    RDS(on) scales steeply (VBR2.5) — inefficient above ~600 V

    VS
    I
    IGBT
    • ▶ Bipolar — electrons + holes (conductivity modulation)
    • ▶ Flat loss: I × VCE(sat) (~1.5–3.5 V)
    • ▶ Switching: Tail current; <100 kHz (typically 1–30 kHz)
    • ▶ Best voltage: 400 V – 6.5 kV
    • ▶ Gate drive: +15 V / 0 V (or negative)
    • ▶ Short-circuit: Robust — ~10 µs withstand
    ⚠ Limitation

    Minority carrier tail (0.5–5 µs) limits max operating frequency

    The Conduction Loss Crossover

    The critical equation: set losses equal to find which device wins at a given current.

    MOSFET Loss
    I² × RDS(on)
    ← Crossover →
    IGBT Loss
    I × VCE(sat)

    Current Level Example: 600 V silicon devices
    MOSFET Wins
    20A
    IGBT Wins
    Low Current ↑ ~20 A Crossover High Current

    Crossover I = VCE(sat) / RDS(on). Example: 2 V ÷ 100 mΩ = 20 A at 600 V. Threshold varies by specific parts selected.

    Voltage Zone Decision Guide
    ⚡
    <200 V
    Silicon MOSFET
    Almost always the right choice. Low RDS(on), fast switching, small magnetics.
    ⚖
    200–600 V
    Contested Zone
    Requires calculation. Check frequency, current, and loss crossover — no rule of thumb applies.
    ⚡
    >600 V
    IGBT (or SiC MOSFET)
    IGBT default at high current. SiC MOSFET if higher frequency or premium efficiency is needed.

    Typical Applications

    M
    MOSFET Use Cases
    • ■ Switched-mode power supplies (SMPS) & offline converters
    • ■ DC-DC buck/boost converters — computing, telecom, automotive
    • ■ Synchronous rectifiers replacing diodes
    • ■ Low-voltage motor drives: 24 V/48 V robotics, drones, BLDC
    • ■ Battery management & protection switches (EVs, portable)
    • ■ Point-of-load regulators & VRMs in data centers
    I
    IGBT Use Cases
    • ■ Industrial variable-frequency drives (VFDs) for AC motors
    • ■ Traction inverters: EVs, trains, light rail (600–1200 V)
    • ■ Solar PV & wind inverters for grid-tied energy conversion
    • ■ UPS systems & active front-end rectifiers
    • ■ Induction heating & welding at sustained high-current
    • ■ HVDC transmission & multi-kilovolt grid-scale converters

    5-Question Selection Framework
    1
    What is the bus voltage?
    Below 200 V → MOSFET. Above 600 V → IGBT or SiC MOSFET. Between 200–600 V → continue to Q2.
    2
    What switching frequency is required?
    Above 100 kHz → MOSFET or SiC only. Below 20–30 kHz → IGBT’s conduction advantage fully realized. 30–100 kHz → calculate explicitly.
    3
    What is the peak and continuous current?
    At 400–600 V, calculate crossover: I > VCE(sat) / RDS(on) → IGBT wins. Below crossover → MOSFET more efficient.
    4
    What are the fault and short-circuit requirements?
    Motor drives with shoot-through risk → prefer IGBT with specified ~10 µs short-circuit withstand for simpler protection design.
    5
    What are cost and supply chain constraints?
    Silicon IGBTs & MOSFETs are mature commodities. SiC MOSFETs carry a price premium. Consider 10–15 year lifecycle availability for industrial products.

    ⚠
    Don’t Forget SiC MOSFETs

    Wide-bandgap SiC keeps RDS(on) low at 1200–1700 V+ while switching without tail current — enabling higher frequency at voltages where silicon IGBTs are standard. Premium cost applies; best suited for high-end EV inverters, solar, aerospace, and applications where efficiency justifies the investment.

    Key Engineering Takeaways
    ⚡
    Speed vs. Efficiency

    MOSFETs switch in nanoseconds enabling MHz operation. IGBTs carry a 0.5–5 µs tail capping practical frequency at 20–30 kHz in high-power designs.

    📈
    Loss Profiles Differ

    MOSFET loss is I²R — quadratic with current. IGBT loss is I×VCE(sat) — nearly linear. At high current, the IGBT always wins on conduction.

    🔥
    Three Numbers Decide

    Bus voltage, switching frequency, and continuous current together determine the right device. No single rule of thumb replaces the crossover calculation.

    🔒
    Fault Robustness Matters

    IGBTs tolerate short-circuit conditions for ~10 µs — a meaningful advantage in motor drive and inverter designs where protection response time is finite.

    WIN SOURCE
    Global independent distributor of electronic components
    Power MOSFETs · IGBTs · Discrete Semiconductors
    win-source.net

    What Are MOSFET and IGBT?

    A MOSFET is a unipolar transistor: current flows through it using only majority carriers (electrons in an N-channel device). Because no minority carriers are involved, the device responds almost instantly when the gate voltage changes, and there is no stored charge to clear during turn-off. A MOSFET’s conduction loss is purely resistive, governed by its drain-to-source on-resistance RDS(on). That resistance is very low at modest voltages, but it scales steeply with voltage rating — following roughly a VBR2.5 relationship for conventional silicon devices — which is why silicon MOSFETs become increasingly inefficient as operating voltages rise above roughly 200–300 V.

    An IGBT is a hybrid device. Its input stage is a MOSFET gate structure, so it is still voltage-controlled and easy to drive. Its output stage, however, is a bipolar PNP transistor, which means current flows via both electrons and holes. When the IGBT turns on, it floods its drift region with minority carriers in a process called conductivity modulation. That injection dramatically reduces the effective on-state resistance at high voltages and high currents — something a silicon MOSFET simply cannot replicate. The trade-off is that those minority carriers must recombine or be swept out during turn-off, creating the device’s defining limitation: a lingering tail current.

    Structure and Operating Principles

    How a MOSFET Works

    A power MOSFET has three terminals: gate, drain, and source. A thin insulating oxide layer separates the gate from the semiconductor channel beneath it. When gate voltage exceeds the threshold, an inversion layer (the conduction channel) forms between source and drain and current begins to flow. Remove the gate voltage and the channel collapses immediately — there is no stored charge to delay the transition. This makes MOSFETs naturally suited to high-frequency operation, with switching transitions measured in nanoseconds. Modern devices can operate from 100 kHz well into the MHz range, enabling compact magnetics and fast control loops.

    The fundamental limitation comes from the physics of building a high-voltage drift region in silicon. To withstand higher breakdown voltages, the drift region must be made thicker and more lightly doped, which directly raises RDS(on). This inherent trade-off between breakdown voltage and on-resistance is sometimes called the silicon limit. Engineers use techniques like superjunction structures and trench gates to improve the trade-off, but for silicon MOSFETs the practical upper limit for competitive efficiency sits around 600–900 V. Above that range, the conduction losses become difficult to justify.

    How an IGBT Works

    An IGBT shares the gate and N-drift region of a MOSFET but adds a P+ collector layer at the back of the device. Its three terminals are gate, collector, and emitter. When the gate turns the MOSFET section on, the resulting current forward-biases the internal PNP transistor, flooding the drift region with holes. This conductivity modulation keeps the collector-to-emitter saturation voltage VCE(sat) relatively flat — typically 1.5–3.5 V — regardless of how much current is flowing. At high voltages and high currents, this is a decisive advantage over the I² × RDS(on) conduction loss of a MOSFET.

    The same minority carrier injection that enables low VCE(sat) becomes a liability at turn-off. After the gate signal drops, those injected holes do not disappear instantly; they recombine over a characteristic tail time of roughly 0.5–5 microseconds depending on device technology. The resulting tail current, which continues to flow while the collector voltage is already rising, creates an overlap of voltage and current that generates switching loss. This mechanism limits the practical switching frequency of standard silicon IGBTs to below 100 kHz, and in high-power motor drive applications where heatsink constraints are real, the practical limit is closer to 20–30 kHz.

    Key Differences: MOSFET vs IGBT

    The table below condenses the most important parameters for a side-by-side comparison. Use it as a quick reference, but read the sections that follow to understand why these numbers matter in a real design.

    Parameter MOSFET IGBT
    Conduction type Unipolar (majority carriers only) Bipolar (electrons and holes)
    On-state loss mechanism Resistive: I² × RDS(on) Voltage drop: I × VCE(sat) (~1.5–3.5 V)
    Switching speed <10 ns; 100 kHz to MHz range Tail current limits to <100 kHz (typically 1–30 kHz in practice)
    Optimal voltage range <250–600 V (silicon) >400 V; routinely 600 V–6.5 kV
    Preferred current level Lower to moderate High (>20 A at 600 V is typical crossover)
    Gate drive 10–15 V (logic-level variants: 4.5 V) +15 V / 0 V (or negative for fast turn-off)
    Short-circuit withstand Limited Typically 10 µs; robust in protected designs
    Typical application DC-DC converters, SMPS, synchronous rectifiers Motor drives, traction inverters, solar/wind inverters, UPS

    Switching Speed and Frequency Limits

    Switching speed matters for two reasons: it sets the upper operating frequency of the converter, and it determines the switching loss that must be dissipated as heat. MOSFETs have no minority carrier storage, so their transitions are controlled purely by how quickly the gate charge can be moved by the drive circuit. State-of-the-art silicon MOSFETs switch in under 10 nanoseconds, enabling converter operating frequencies from several hundred kilohertz up into the megahertz range. Running a converter at higher frequency means smaller inductors and capacitors, which translates directly to a more compact, lighter design.

    IGBTs tell a different story. Even after the gate turns off, the tail current from recombining minority carriers can persist for 0.5–5 microseconds. During that interval, the collector voltage has already risen to the bus voltage, so the product of voltage and current is nonzero — that energy is lost as heat on every switching cycle. Multiply by switching frequency and the switching loss grows proportionally. For typical silicon IGBTs, the practical upper frequency is below 100 kHz, and in high-power motor drive applications with real heatsink constraints, 20–30 kHz is a more realistic ceiling. Newer punch-through and field-stop IGBT designs reduce the tail, but the fundamental physics remains.

    It is worth noting that MOSFET switching is not entirely loss-free either. Gate capacitance (including the Miller capacitance) must be charged and discharged on every cycle, drawing power from the gate driver. At very high frequencies, gate driver power dissipation can become a meaningful overhead. Neither device is ideal; the art is in matching each device to the frequency regime where its loss profile is favorable.

    Conduction Loss: The Crossover That Decides the Winner

    This is the most important concept for practical device selection, and it is the one most often glossed over in introductory comparisons. MOSFET conduction loss follows I² × RDS(on): it scales with the square of current and rises steeply with voltage rating. IGBT conduction loss is approximately I × VCE(sat), where VCE(sat) stays nearly constant regardless of current or voltage rating. At low currents, the quadratic nature of MOSFET loss keeps it below the IGBT’s fixed-offset loss. But as current rises, the MOSFET’s loss eventually overtakes the IGBT’s.

    The crossover can be approximated by setting the two loss expressions equal: I > VCE(sat) / RDS(on). As a concrete example, a 600 V silicon MOSFET might have an RDS(on) of 100 mΩ. A comparable IGBT might have VCE(sat) of 2 V. The crossover current works out to roughly 20 A — meaning that below 20 A the MOSFET has lower conduction loss, and above 20 A the IGBT wins. The threshold shifts depending on the specific parts compared, but the principle is consistent: IGBTs become more efficient at higher currents, and the advantage grows larger as voltage increases, because RDS(on) scales so steeply with rated voltage in silicon MOSFETs while VCE(sat) in an IGBT barely changes from a 600 V to a 1200 V device.

    As a rough rule of thumb that engineers frequently cite: below about 200 V, a silicon MOSFET is almost always the better choice on conduction efficiency; above 600 V and at currents beyond 20–30 A, the IGBT typically wins; and the 200–600 V band is genuinely contested, requiring a calculation rather than a rule of thumb.

    Thermal Behavior and Temperature Effects

    Both devices are sensitive to temperature, but in different ways. A MOSFET’s RDS(on) increases with junction temperature — a positive temperature coefficient. This means that as the device heats up, conduction loss grows, which heats it further. In parallel configurations, this self-regulating behavior is actually helpful: if one device runs hotter and its resistance rises, it naturally shares less current with its cooler parallel partners, promoting current balance. Designing MOSFET parallels is therefore relatively straightforward.

    IGBTs exhibit a more complex thermal profile. VCE(sat) may initially decrease at moderate temperatures before increasing at higher temperatures, depending on the specific device generation. Modern field-stop IGBTs are generally designed with a positive temperature coefficient for VCE(sat) to support safe parallel operation, but it is worth verifying this in the datasheet. IGBTs also need careful attention to the tail current behavior at temperature, because minority carrier lifetime increases with temperature, lengthening the tail and increasing switching loss at high junction temperatures.

    Typical Applications

    Where MOSFETs Are Used

    MOSFETs are the default choice in switching power supplies, DC-DC converters, and synchronous rectifiers operating at voltages below a few hundred volts. A 12 V or 48 V bus converter running at 300 kHz or more is squarely in MOSFET territory — an IGBT would be both too slow and unnecessarily lossy in conduction at those current levels. MOSFETs are also standard in battery management systems, motor drivers for small brushless DC motors, Class D audio amplifiers, and RF switching circuits where speed and low gate charge matter above all else.

    • Switched-mode power supplies (SMPS) and offline flyback/LLC converters at low to medium power
    • DC-DC buck, boost, and buck-boost converters in computing, telecom, and automotive electronics
    • Synchronous rectifiers replacing diodes in high-efficiency power paths
    • Low-voltage motor drives (24 V, 48 V) for robotics, drones, and BLDC motors
    • Battery management and protection switches in portable electronics and EV battery packs
    • Point-of-load regulators and VRMs in servers and data center infrastructure

    Where IGBTs Are Used

    IGBTs are the workhorses of medium- and high-power industrial and energy systems. Anywhere a designer needs to switch hundreds of volts at tens or hundreds of amperes, the IGBT’s flat VCE(sat) characteristic and its tolerance for short-circuit conditions make it the dominant choice. The frequencies involved — typically 1 kHz to 20 kHz for motor drives — suit IGBTs well, since switching loss at those rates is manageable and the conduction efficiency advantage at high current is fully realized.

    • Industrial variable-frequency drives (VFDs) controlling AC induction and permanent-magnet motors
    • Traction inverters in electric vehicles, trains, and light rail (600 V–1200 V bus)
    • Solar photovoltaic and wind inverters for grid-tied energy conversion
    • Uninterruptible power supplies (UPS) and active front-end rectifiers
    • Induction heating and welding equipment requiring sustained high-current pulses
    • HVDC transmission systems and large grid-scale power converters at the multi-kilovolt level

    A Note on SiC MOSFETs

    No honest comparison of MOSFET and IGBT today can ignore Silicon Carbide (SiC) MOSFETs. SiC is a wide-bandgap semiconductor material with a critical electric field roughly 10 times higher than silicon’s. This allows SiC MOSFET drift regions to be much thinner and more heavily doped for the same breakdown voltage, which keeps RDS(on) low even at 1200 V, 1700 V, and beyond — voltage ranges where silicon MOSFETs are simply not competitive. Because SiC MOSFETs are still majority-carrier devices, they switch without a tail current, enabling operating frequencies far above what silicon IGBTs can achieve at comparable voltages.

    In practical terms, SiC MOSFETs are increasingly replacing silicon IGBTs in high-end EV traction inverters, solar inverters, and other applications where higher efficiency and higher switching frequency justify the cost premium. The wafer fabrication cost for SiC is substantially higher than for silicon, and yield improvements are still maturing. SiC devices are also well suited for sectors like aerospace and defense where performance takes priority over unit cost. For budget-sensitive, high-volume applications at standard industrial voltages, silicon IGBTs retain a compelling cost and reliability advantage — they have decades of proven performance in the field, and their failure modes are thoroughly understood. The practical picture for most designers today is that silicon MOSFETs, silicon IGBTs, and SiC MOSFETs each occupy a distinct zone, and the choice between the three depends on voltage, frequency, current density, cost target, and thermal budget together.

    How to Choose: A Practical Decision Framework

    Rather than a simple voltage cutoff, think of device selection as a multi-axis problem. The following questions, asked in order, will usually lead to the right answer:

    1. What is the operating bus voltage? Below 200 V, a silicon MOSFET is almost certainly the right device. Above 600 V, an IGBT (or SiC MOSFET if budget allows) is the default. Between 200 V and 600 V, proceed to the next questions.

    2. What switching frequency does the design require? Above 100 kHz, a silicon MOSFET or SiC MOSFET is needed — an IGBT’s tail current will generate unacceptable switching loss and thermal load at these rates. Below 20–30 kHz, the IGBT’s superior conduction loss at high current can be fully exploited. In the 30–100 kHz band, the trade-off must be calculated explicitly.

    3. What is the peak and continuous current? At moderate voltages (e.g., 400–600 V), calculate the conduction loss crossover: if the load current consistently exceeds VCE(sat) / RDS(on), the IGBT wins on conduction efficiency. At lower currents, a MOSFET is more efficient in the on-state.

    4. What are the short-circuit and fault-withstand requirements? IGBTs are generally more robust in short-circuit conditions, withstanding fault events for a defined protection time (typically 10 µs). This robustness matters in motor drives and inverters where shoot-through or load short-circuits are credible failure modes. Selecting an IGBT with a specified short-circuit withstand time can simplify the protection design considerably.

    5. What are the cost and component availability constraints? Silicon IGBTs for industrial voltages are mature, widely available commodity parts from manufacturers including Infineon, STMicroelectronics, and onsemi. Silicon MOSFETs at low to medium voltages are similarly commoditized. SiC MOSFETs carry a price premium and, in some ratings, can face tighter supply. These supply and lifecycle factors are worth considering alongside the electrical parameters, particularly in long-lifecycle industrial products where component availability over a 10–15 year product life matters.

    Conclusion

    MOSFET and IGBT are not competing for the same applications so much as they are each optimized for a different region of the power electronics design space. The MOSFET’s majority-carrier conduction and near-instantaneous switching make it the right device when speed matters and voltage is modest. The IGBT’s conductivity modulation and flat VCE(sat) characteristic make it the right device when voltage is high, current is heavy, and switching frequency is in the low-to-medium kilohertz range. The practical decision hinges on three numbers: bus voltage, switching frequency, and continuous current — and on the calculated crossover point where one device’s loss profile overtakes the other’s.

    For engineers sourcing these components, having access to a broad and reliable supply of both device families matters as much as making the right selection decision. Discrete semiconductors, IGBT modules, and power MOSFETs from manufacturers like Infineon, STMicroelectronics, onsemi, and Vishay are all part of a well-stocked catalog for power electronics design. WIN SOURCE, a global independent distributor of electronic components, stocks power MOSFETs and IGBTs across current-production and hard-to-find part numbers, and supports engineers and procurement teams with shortage sourcing, lifecycle management and alternative solutions. Whether you are designing a new power conversion system or managing a long-running production line, having a supply chain partner engaged early reduces the risk of component-level surprises later.

    Frequently Asked Questions

    What is the main difference between an IGBT and a MOSFET?

    A MOSFET conducts with majority carriers only, so its on-state loss is resistive (I² × RDS(on)) and it switches in nanoseconds with no stored charge. An IGBT adds a bipolar output stage whose conductivity modulation gives a nearly flat on-state voltage (VCE(sat), typically 1.5–3.5 V) at high voltage and current, at the cost of a tail current that limits switching frequency.

    When should I use an IGBT instead of a MOSFET?

    When the bus voltage is high (above roughly 600 V), the current is heavy (tens of amperes and up) and the switching frequency is modest (below about 20–30 kHz in high-power designs). Motor drives, traction inverters, solar and wind inverters and UPS systems are typical IGBT territory.

    How do I calculate the conduction-loss crossover between the two?

    Set the two loss expressions equal: the crossover current is VCE(sat) ÷ RDS(on). For a 600 V silicon MOSFET at 100 mΩ against an IGBT at 2 V, that is 20 A — below it the MOSFET has lower conduction loss, above it the IGBT does. The figure moves with the specific parts, so recalculate for the devices you are actually comparing.

    Why can’t IGBTs switch as fast as MOSFETs?

    Because the holes injected into the drift region during conduction must recombine or be swept out at turn-off. That produces a tail current of roughly 0.5–5 µs that overlaps with the rising collector voltage and generates switching loss on every cycle, which is why practical silicon IGBT frequencies stay below about 100 kHz.

    Do SiC MOSFETs replace IGBTs?

    In some applications, yes. SiC’s much higher critical field keeps RDS(on) low at 1200–1700 V and above, and as majority-carrier devices SiC MOSFETs have no tail current, so they switch far faster than silicon IGBTs at the same voltage. They cost more, so silicon IGBTs remain the choice for cost-sensitive, high-volume industrial designs at standard voltages.

    Part discontinued, obsolete or hard to find?

    WIN SOURCE is a global independent distributor of electronic components, supporting component supply, shortage sourcing, lifecycle management and alternative solutions. Visual inspection, non-destructive testing and electrical testing are applied according to material risk, customer requirements and the applicable quality process, and orders are covered by the published return policy and a 3-year warranty on eligible components.

    Stock and pricing are updated daily — search a part number or contact us for current availability, lead time and a quote.

    Search a Part Number  Upload a BOM / RFQ

    © 2026 Win Source Electronics. All rights reserved. This content is protected by copyright and may not be reproduced, distributed, transmitted, cached, or otherwise used without the prior written permission of Win Source Electronics.