Every electronic circuit needs protection against overcurrent events — but replacing a blown fuse buried inside a sealed device, an automotive dashboard, or a battery pack is inconvenient at best and impossible at worst. The PTC resettable fuse solves this problem by combining overcurrent protection with automatic self-recovery. When a fault current passes through it, its resistance surges dramatically to limit the current. When the fault clears and the device cools, it resets itself and returns to normal operation — no replacement required.
This article explains the physics behind that behavior, walks through the key specifications you need to understand before selecting one, and covers practical design considerations that prevent common mistakes. Whether you are protecting a USB port, a lithium-ion battery pack, or an industrial sensor line, the selection logic is the same.
How it works, key parameters, and a step-by-step selection guide for engineers.
|
|
|
|
|
The phase-transition mechanism behind self-resetting protection
|
🟢
Normal State
Semi-crystalline polymer. Carbon particles tightly packed. Very low resistance (mΩ range). |
🔴
Fault Detected
Overcurrent raises temperature to 85–125°C. Polymer transitions to amorphous state. |
|
😖
Tripped State
Resistance surges to MΩ range. Current drops to leakage level. Device stays warm. |
✅
Auto-Reset
Fault clears. Device cools, recrystallizes. Resistance returns to low value. |
Two technologies, different niches — choose the right one for your design
|
|
What each datasheet specification actually means in circuit terms
|
🔓
Ihold
Holding Current
Max continuous current without tripping at 23°C. Must be derated for elevated temperatures. |
⚡
Itrip
Trip Current
Min current guaranteed to trip the device. Typically ~2× Ihold. Gap between the two is intentional. |
⚡︎
Vmax
Max Voltage
Highest voltage the device sustains when tripped. Must exceed rail voltage with ≥20% margin. |
|
⚠️
Imax
Max Interrupt Current
Max fault current without permanent damage. Exceeding this can destroy the device. |
🔌
Rᵢ
Initial Resistance
Room-temp resistance before any trip. Rises slightly after each trip — factor into voltage budgets. |
Work through each step in order — each one constrains the next
Record Iop, supply voltage, max ambient temp at PCB location, and worst-case fault current. |
Ihold drops with temperature. Use the manufacturer derating curve. Add ≥20% safety margin above Iop. |
Must exceed max fault voltage with ≥20% margin. 5 V USB → Vmax ≥ 6 V. 12 V auto → Vmax ≥ 16 V. |
Confirm the interrupting rating exceeds worst-case short-circuit current. Exceeding Imax causes permanent device failure. |
Use the time-current curve. High overcurrent → fast trip. Near Itrip → may take seconds. Must protect before component damage. |
SMD (0603–2920) for automated reflow. Radial through-hole for high current or rework. Battery strap for cell packs. |
Where self-resetting protection delivers the most value
|
🔌
USB Ports
Auto-resets on unplug
|
🔋
Battery Packs
Li-ion / NiMH sealed
|
🚗
Automotive
ECU, ADAS, lighting
|
|
📡
Industrial / Telecom
Line cards, sensors
|
📱
Consumer Electronics
Phones, tablets, chargers
|
Avoid these common mistakes in your design
|
Response Speed
Trip time: ms to seconds. No protection against ESD/surges — use a TVS diode upstream for those. |
Leakage Current
Tripped state is NOT a complete open circuit. Tens to hundreds of mA still flow. Not a standalone solution where full de-energization is required. |
|
Aging & Trip Count
Base resistance rises over thousands of trips. Account for increased quiescent resistance in voltage-budget calculations over product life. |
PCB Thermal Placement
Keep away from heat sources (regulators, transformers). Adjacent heat reduces Ihold and can cause nuisance trips at normal operating current. |
|
Never Parallel Devices
Resistance mismatch causes uneven current sharing, one device trips first, the other carries full load. Always select a single higher-rated device instead. |
|
|
|
|
|
WIN SOURCE
Global independent distributor of electronic components — PTC resettable fuses, current-production and hard-to-find
|
Browse PTC Resettable Fuses → |
What Is a PTC Resettable Fuse?
A PTC resettable fuse — also called a PPTC (Polymeric Positive Temperature Coefficient) device, polyfuse, or polyswitch — is a passive electronic component placed in series with a circuit to protect it from overcurrent faults. The term “PTC” refers to a fundamental material property: resistance increases as temperature rises. In a PTC resettable fuse, that property is engineered to be extreme — resistance can jump by several orders of magnitude over a narrow temperature window, effectively interrupting the current path during a fault.
Unlike a traditional one-time fuse, which permanently opens when it blows, a PTC resettable fuse recovers once the fault is cleared and the device cools. This self-resetting behavior makes it particularly valuable in applications where manual fuse replacement is impractical, such as sealed enclosures, automotive electronics, and high-volume consumer products where field service costs are a concern.
How a PTC Resettable Fuse Works
The most widely used PTC resettable fuses are built from a matrix of crystalline polymer — typically a polyolefin such as polyethylene — loaded with conductive carbon black particles. At room temperature, the polymer is in a semi-crystalline state that keeps those carbon particles tightly packed together. The packed particles form continuous conductive pathways through the material, resulting in very low electrical resistance (typically in the milliohm to low-ohm range), so the device has negligible impact on normal circuit operation.
When excessive current flows through the device, resistive heating (governed by P = I²R) raises the temperature. Once the material reaches its switching point — typically somewhere between 85°C and 125°C depending on the formulation — the polymer undergoes a phase transition from crystalline to amorphous. The material expands, the carbon particle chains separate, and the conductive pathways are broken. Resistance surges to the megohm range, which drops the current through the protected circuit to a small leakage value. A small current continues to flow and is sufficient to keep the device warm, holding it in the high-resistance state for as long as the fault voltage is applied.
Once the circuit is de-energized (or the fault is cleared and the voltage drops low enough), the device cools. The polymer recrystallizes and contracts, the carbon particles re-form their conductive network, and resistance returns toward its original low value. This recovery typically takes a few seconds for a light trip, but a recently tripped device may retain a somewhat elevated resistance for minutes or hours — a normal aging characteristic to account for in designs with tight voltage-drop budgets.
Polymer PTC vs. Ceramic PTC: Two Technologies, Different Niches
There are two fundamentally different material technologies used to make PTC resettable fuses. Understanding the distinction matters for selecting the right device.
Polymer PTC (PPTC) is the dominant technology in the market — the vast majority of resettable fuses sold today are polymer types. They offer very low on-resistance, compact SMD packages (down to 0402), excellent recovery characteristics, and a wide current range. They are the practical choice for most PCB-level protection tasks: USB ports, battery packs, microcontroller power rails, and similar low-to-medium current applications.
Ceramic PTC (CPTC) uses a doped ceramic semiconductor (typically barium titanate-based) that also exhibits sharply increasing resistance with temperature, but through a different physical mechanism. Ceramic PTCs tend to have higher on-resistance than polymer types and recover more slowly, but they offer better stability in applications where resistance must remain consistent after repeated trips. They are commonly found in telecom line protection and motor demagnetization circuits where post-trip resistance drift is a critical concern. For general overcurrent protection purposes, polymer PPTC devices are almost always the better fit.
| Property | Polymer PPTC | Ceramic CPTC |
|---|---|---|
| On-resistance | Very low (mΩ range) | Relatively higher |
| Package size | Very compact (SMD 0402+) | Relatively larger |
| Recovery after trip | Excellent | Good, slower |
| Resistance drift | Some aging expected | More stable post-trip |
| Primary use case | Overcurrent protection | Telecom, heating, demagnetization |
Key Parameters Explained
PTC resettable fuse datasheets share a common set of parameters. Getting the selection right depends on understanding what each one actually means in circuit terms.
Holding Current (Ihold) is the maximum continuous current the device can carry at a specified ambient temperature (typically 23°C) without tripping. Normal circuit operating current must stay below this value. Because Ihold decreases as ambient temperature rises, this parameter requires thermal derating before use — more on that in the selection guide.
Trip Current (Itrip) is the minimum current at which the device is guaranteed to trip into its high-resistance state within a specified time. It is typically about twice Ihold. There is an intentional gap between Ihold and Itrip — current falling in that window may or may not cause a trip, depending on ambient temperature, PCB thermal environment, and time. Designs should not rely on protection activating at currents close to Ihold.
Maximum Voltage (Vmax) is the highest voltage the device can safely sustain in its tripped (high-resistance) state without breakdown. This must exceed the maximum voltage that could appear across the device during a fault. For a simple DC circuit, this is the supply rail voltage. Always choose a device with Vmax comfortably above the circuit operating voltage — a 20% margin is a standard starting point.
Maximum Interrupting Current (Imax) is the maximum fault current the device can handle without sustaining permanent damage at rated voltage. If a short-circuit scenario could produce a current above this value, the device may fail catastrophically rather than protect the circuit.
Initial Resistance (Ri) is the device resistance at room temperature before any trip event. Lower is better for minimizing normal-operation power dissipation and voltage drop. Note that after one or more trip events, the device’s resistance may settle at a somewhat higher level than its original factory value — this is normal and should be accounted for in voltage-sensitive designs.
How to Choose a PTC Resettable Fuse: A Step-by-Step Guide
Selection follows a straightforward process once you have the circuit parameters documented. Work through each step in order, since each constrains the next.
- Define the circuit parameters — Record the maximum continuous operating current (Iop), the supply voltage, the maximum ambient temperature at the device location on the PCB under worst-case load conditions, and the maximum fault current (Imax) that could appear during a short circuit.
- Apply temperature derating to find required Ihold — A device rated 1.0 A hold current at 23°C may only reliably hold 0.75 A at 60°C. Look up the manufacturer’s derating curve or table for the specific device. Calculate the required Ihold at 25°C as: Ihold_required = Iop ÷ derating factor at Tmax. Add an additional safety margin of at least 20% above Iop to avoid nuisance trips from minor surges or measurement uncertainty.
- Select Vmax — Choose a device with Vmax greater than the maximum voltage that could appear across it during a fault, with at least a 20% margin. For a 5 V USB circuit, select Vmax ≥ 6 V. For automotive 12 V systems, select Vmax ≥ 16 V.
- Verify Imax — Confirm the device’s interrupting rating exceeds the worst-case fault current your circuit could produce. If board-level calculations suggest a short could drive several hundred amperes for a fraction of a second, verify the device is rated for that peak. Exceeding Imax can permanently damage the device.
- Check trip time at fault current — Consult the manufacturer’s time-current curve. This curve shows how long the device takes to trip at a given overcurrent. If the protected component can only tolerate 100 ms of overcurrent, confirm the PTC trips faster than that at the expected fault level. Higher overcurrent produces faster trips — but at modest overcurrents near Itrip, response can be measured in seconds.
- Select the package — Match the form factor to the assembly process and PCB space available. SMD packages (0603, 0805, 1206, 1210, 1812, 2920) are suited to automated reflow soldering; through-hole radial devices handle higher currents and are easier to rework manually; battery strap formats are designed for spot-welding directly onto cell packs.
Package Types and Form Factors
PTC resettable fuses are available in three main physical configurations, each suited to a different assembly environment.
Surface Mount (SMD) devices are the most widely used format in modern PCB designs. Standard package codes follow the EIA size convention: 0603, 0805, 1206, 1210, 1812, and 2920 are the most common, covering Ihold ranges from roughly 0.05 A to 5 A. SMD devices are compatible with automated pick-and-place and reflow soldering, making them appropriate for high-volume consumer electronics production.
Radial Leaded (Through-Hole) devices are the older form factor but remain relevant for high-current applications and designs where manual soldering or in-field replacement is required. They generally handle higher currents than equivalent-footprint SMD devices and offer better thermal mass, which can be an advantage in industrial applications with significant power dissipation.
Battery Strap and Surface Mount Cell Types are purpose-built for integration directly into lithium-ion and NiMH battery packs. They are designed to be spot-welded onto cell terminals, providing overcurrent protection within the pack without adding significant size or weight. These are a common sight in portable power tools, laptops, and consumer battery packs.
Where PTC Resettable Fuses Are Used
The self-resetting characteristic makes PTC fuses most valuable wherever repeated fault events are expected, replacement is difficult, or a human intervention requirement would be unacceptable. The following are the most common application categories:
- USB and power interface ports — Protecting host-side USB power lines from overcurrent caused by faulty or incompatible peripherals. A tripped PTC resets automatically once the offending device is unplugged, eliminating the need for end-user service.
- Battery packs — Overcurrent protection for Li-ion and NiMH cell packs in laptops, power tools, and portable electronics, where the pack is sealed and fuse replacement is not practical.
- Automotive electronics — ECUs, ADAS modules, infotainment systems, door lock actuators, and LED lighting circuits benefit from PTC protection because an automotive environment produces periodic overcurrent events (motor stall, wiring chafing) that should not require a service visit each time.
- Industrial and telecom equipment — Line cards, sensor interfaces, and communication ports where a fault on one port should not require a technician to open the enclosure and replace a fuse.
- Consumer electronics — Smartphones, tablets, game controllers, and chargers, where device reliability and elimination of field returns drives the design decision.
Design Cautions and Limitations
A PTC resettable fuse is not a universal solution to every protection problem. Being clear about its limitations avoids design mistakes.
Response speed. PPTC trip time ranges from tens of milliseconds to several seconds, depending on the overcurrent magnitude. For nanosecond-scale transients such as ESD or lightning surges, a PTC fuse provides no meaningful protection. Those events require a TVS diode or GDT upstream. In fact, a common design pattern places a PTC fuse in series on the rail (for sustained overcurrent protection) with a TVS diode across the line downstream of it (for fast transient clamping). The TVS absorbs the energy spike; the PTC handles a prolonged fault that would otherwise overstress the TVS.
Leakage current in the tripped state. A PTC fuse does not create a complete open circuit when tripped. A small leakage current continues to flow — typically tens to hundreds of milliamps — because the residual current maintains the device’s elevated temperature. This is an important difference from a traditional fuse or circuit breaker. In circuits where the load must be completely de-energized during a fault, a PPTC may not be appropriate as a standalone solution.
Aging and trip count limitations. Each trip event causes minor, cumulative internal changes that gradually raise the device’s base resistance. Devices are typically rated to maintain their specification for several thousand trip cycles, but they are not indefinitely durable. In applications that see frequent fault events, the increased quiescent resistance should be accounted for in voltage-budget calculations over the product’s service life.
Thermal environment on the PCB. Because Ihold decreases with rising temperature, placing a PTC next to a heat-generating component (a power transistor, voltage regulator, or transformer) can cause nuisance trips at normal operating currents. Leave adequate clearance around the device and avoid placing it in a thermally confined area or under a conformal coating that traps heat.
Do not parallel devices. Connecting two PTC fuses in parallel to increase current capacity is unreliable. Small differences in initial resistance cause one device to carry more current, heat up sooner, increase its resistance, and shift even more current to the other — potentially causing one to trip while the other carries the full load. Select a single higher-rated device instead.
PTC Resettable Fuse vs. Traditional Fuse: A Quick Comparison
It is worth being explicit about the trade-off, because a traditional fuse is not always the inferior choice. Traditional fuses completely interrupt the circuit when they blow, leaving zero leakage current through the fault path and providing a clear, deterministic open-circuit condition. They are simpler, cheaper per unit, and their protection behavior does not degrade with repeated trips. For applications where fuse replacement is easy and the fault is expected to be infrequent and severe — automotive blade fuses, household appliance protection — a traditional fuse often makes more sense.
PTC resettable fuses earn their keep when the fault condition is expected to be transient and recoverable (a motor stall that self-clears, a peripheral device that is unplugged), when replacement access is limited, or when reducing service calls and field returns justifies the higher unit cost. They also excel in high-volume automated PCB assembly because they can be placed by machine exactly like any other passive component.
| Feature | PTC Resettable Fuse | Traditional (One-Time) Fuse |
|---|---|---|
| Reusable after fault | Yes, auto-reset | No, must replace |
| Circuit isolation during fault | Partial (leakage current remains) | Complete open circuit |
| Response speed | Milliseconds to seconds | Microseconds to milliseconds |
| Unit cost | Higher | Lower |
| Field service required | No | Yes (after each trip) |
| PCB mount (SMD) | Yes | Limited (cartridge/blade types) |
Summary
The PTC resettable fuse is a well-established, passive circuit protection solution with a clear and predictable operating principle. Understanding the phase-transition physics behind its behavior — and applying it correctly through proper thermal derating, voltage margin, and trip-time verification — is the difference between a reliable design and one that generates unexpected field returns. Pair it with a TVS diode for transient protection, keep it away from heat sources on the PCB, select a single appropriately rated device rather than paralleling, and always work from the manufacturer’s derating curve rather than the nominal 25°C specification alone.
WIN SOURCE, a global independent distributor of electronic components, stocks PTC resettable fuses and other circuit protection parts from manufacturers including Littelfuse, Bourns and Eaton, covering current-production part numbers as well as parts that are hard to find, and supports shortage sourcing, lifecycle management and alternative solutions across a product’s full lifespan, not just at initial build. Any substitute part is subject to final approval by the customer’s engineering team.
Frequently Asked Questions
What is the difference between holding current and trip current on a PTC fuse?
Holding current (Ihold) is the maximum current the device carries continuously at the rated ambient (usually 23°C) without tripping; trip current (Itrip) is the minimum current guaranteed to trip it, typically about twice Ihold. Currents between the two may or may not trip depending on temperature and time, so normal operating current must sit below Ihold with margin, after temperature derating.
Does a PTC resettable fuse fully disconnect the circuit when it trips?
No. In the tripped state it goes to a very high resistance, but a small leakage current — typically tens to hundreds of milliamps — keeps flowing and keeps the device warm. Where a load must be completely de-energized during a fault, a traditional fuse, circuit breaker or an active disconnect is needed instead of, or alongside, the PTC.
How do I derate a PTC fuse for temperature?
Ihold falls as ambient temperature rises, so look up the manufacturer’s derating curve for the worst-case temperature at the device’s location on the board and divide your operating current by that factor to get the required 23°C rating. Add at least 20% margin above the operating current to avoid nuisance trips, and keep the device away from regulators, transformers and other heat sources.
Can I use a PTC fuse instead of a TVS diode for surge or ESD protection?
No. PTC trip times run from tens of milliseconds to seconds, far too slow for nanosecond transients. Use a TVS diode or gas discharge tube for the transient, and let the PTC in series handle the sustained overcurrent that would otherwise overstress the TVS.
Can two PTC fuses be paralleled for more current?
It is not recommended. Small differences in initial resistance make one device carry more current, heat faster and rise in resistance, pushing still more current to the other until one trips and the other carries the whole load. Select a single device with a higher rating instead.
Part discontinued, obsolete or hard to find?
WIN SOURCE is a global independent distributor of electronic components, supporting component supply, shortage sourcing, lifecycle management and alternative solutions. Visual inspection, non-destructive testing and electrical testing are applied according to material risk, customer requirements and the applicable quality process, and orders are covered by the published return policy and a 3-year warranty on eligible components.
Stock and pricing are updated daily — search a part number or contact us for current availability, lead time and a quote.
© 2026 Win Source Electronics. All rights reserved. This content is protected by copyright and may not be reproduced, distributed, transmitted, cached, or otherwise used without the prior written permission of Win Source Electronics.