What Is an FPGA? How It Differs From an ASIC and a Microcontroller

  • Home
  • SUPPLY CHAIN INSIGHTS
  • What Is an FPGA? How It Differs From an ASIC and a Microcontroller

    When you’re designing an embedded system or selecting components for a new board, three types of devices keep coming up: FPGAs, ASICs, and microcontrollers. Each is a programmable or configurable integrated circuit at some level, but they operate on fundamentally different principles and serve very different engineering purposes. Picking the wrong one early in a project means revisiting the decision at significant cost later.

    This article breaks down what each device actually is, how its internal architecture differs from the others, where each one excels, and — critically — where the economics of each choice tend to shift. Whether you’re an engineer evaluating options for a new design, a procurement professional trying to understand what’s in a BOM, or simply someone who keeps seeing these three terms used interchangeably, this guide lays out the distinctions clearly and honestly.

    ⎨
    Visual Reference Guide
    FPGA vs. ASIC vs. Microcontroller

    Understand the core architecture, trade-offs, and ideal use cases for each device type — so you choose right the first time.

    6-input
    LUTs in modern FPGAs
    5
    Core FPGA components
    10k+
    Units: typical ASIC break-even
    12–18
    Months: ASIC tape-out

    What Is Each Device?
    □
    FPGA

    Field-Programmable Gate Array. Configured after manufacture via a bitstream. Implements hardware logic directly — fully reprogrammable, unlimited times.

    ✓ Reconfigurable parallel hardware
    ◆
    ASIC

    Application-Specific Integrated Circuit. Logic physically built into silicon at fabrication. Fixed forever — no changes after manufacture.

    ✓ Maximum performance & efficiency
    ■
    Microcontroller

    MCU: CPU + Flash + RAM + Peripherals on one chip. Runs firmware sequentially in C/C++. The most widely deployed programmable logic device.

    ✓ Low cost, simple development

    Inside an FPGA: 5 Core Components
    1
    CLBs

    Configurable Logic Blocks with LUTs, flip-flops & carry chains — the core compute fabric.

    2
    Interconnects

    Programmable switch boxes & routing fabric that wire all blocks together at config time.

    3
    I/O Blocks

    Configurable I/O for voltage, drive strength & direction — connects fabric to the real world.

    4
    BRAM & DSP

    Hard memory blocks & multiply-accumulate units for fast, power-efficient signal processing.

    5
    Clock & Config

    PLLs for clock synthesis; SRAM-based config is volatile but infinitely reprogrammable.

    Head-to-Head Comparison
    Factor FPGA ASIC MCU
    Processing Parallel HW Parallel HW (fixed) Sequential SW
    Reconfigurable? ✓ Unlimited ✗ Fixed forever ✓ Firmware only
    NRE Cost Low Millions Very Low
    Per-Unit Cost Higher Lowest at volume Low
    Power Draw ~1W–10W+ Optimized (best) 1mW–500mW
    Time to Market Fast 12–18+ months Fast
    Sweet Spot Low–mid volume Tens of thousands+ Control tasks

    How to Choose: Decision Guide
    ➤

    Need true parallelism or sub-microsecond timing?

    Choose FPGA — MCU sequential execution introduces unacceptable latency for high-speed signal processing or precision control loops.

    ➤

    Stable design shipping tens of thousands of units or more?

    Evaluate ASIC — the NRE becomes justifiable and per-unit savings at volume are significant.

    ➤

    Control or monitoring task without unusual speed demands?

    Choose MCU — simpler, cheaper, mature ecosystem. Reaching for an FPGA here is overengineering.

    ➤

    Hardware updates needed after deployment?

    FPGA wins — load a new bitstream in the field. ASICs require a full new fabrication run; MCUs can update firmware but not hardware architecture.

    Real-World Applications
    ⎨ FPGA Applications
    • 5G baseband & telecom
    • Aerospace / radar signal processing
    • Data center AI inference
    • Automotive ADAS & LiDAR
    • ASIC prototyping & RTL validation
    ◆ ASIC Applications
    • Smartphone SoCs & Wi-Fi chips
    • Crypto mining hardware
    • HFT ultra-low latency NICs
    • Display drivers & codecs
    • Power management ICs
    ■ MCU Applications
    • Industrial automation & PLCs
    • Home appliances & HVAC
    • Medical monitors & pumps
    • Automotive ECUs & BMS
    • IoT sensor nodes (ultra-low power)

    5 Key Takeaways
    1

    FPGAs implement hardware, not software — the entire configured circuit runs in parallel with deterministic, cycle-accurate timing.

    2

    ASICs win on efficiency at scale — but only in the tens of thousands of units and up, where the multi-million-dollar NRE is economically justifiable.

    3

    MCUs are the workhorses of the embedded world — low cost, fast dev cycles, and mature ecosystems make them right for the vast majority of control tasks.

    4

    FPGA → ASIC is a proven workflow — prototype and validate in FPGA first; migrate RTL to ASIC once design is stable and volumes justify it.

    5

    Real systems often use all three — FPGA for high-speed front-end processing, MCU for system control, ASIC for fixed high-volume sub-functions.

    Global independent distributor of electronic components

    Source FPGAs, MCUs & Embedded ICs

    WIN SOURCE supports component supply, shortage sourcing, lifecycle management and alternative solutions across FPGAs, microcontrollers and the wider embedded IC range — current-production parts as well as part numbers that are hard to find.

    Submit Your RFQ / BOM →

    What Is an FPGA?

    FPGA stands for Field-Programmable Gate Array. It is an integrated circuit that can be configured by the user after it leaves the factory — hence “field-programmable.” Rather than running a sequence of software instructions like a processor, an FPGA implements hardware logic directly. You describe a circuit in a hardware description language (HDL) such as VHDL or Verilog, synthesize that description into a bitstream, and load it onto the device. The FPGA then physically reconfigures its internal routing and logic to become that circuit.

    The defining characteristic is reconfigurability. The same physical chip can be a high-speed serial decoder one day and a custom motor controller the next, simply by loading a different bitstream. This makes FPGAs useful in situations where the circuit design may still be evolving, where the application demands custom data paths that no off-the-shelf chip provides, or where field upgrades after deployment are valuable. FPGAs represent a broad and growing product category that spans entry-level development boards all the way to high-density devices used in data centers and defense systems.

    The FPGA market reflects this expanding role, with growth driven by AI inference at the edge, 5G infrastructure, data center acceleration, and automotive ADAS workloads. FPGAs are no longer niche devices used only in specialized telecom racks — they are increasingly common in any system where both performance and post-deployment flexibility matter.

    Inside the Architecture: How an FPGA Works

    Understanding why an FPGA behaves the way it does requires a look at what’s inside. Modern FPGA architecture is built around five main types of components, all of which are configurable at programming time.

    Configurable Logic Blocks (CLBs)

    CLBs are the fundamental compute units of an FPGA fabric. Each CLB contains lookup tables (LUTs), flip-flops, carry-chain logic, and multiplexers. A LUT is essentially a small truth-table memory: you load it with the desired Boolean function, and it evaluates inputs combinatorially at very high speed. By chaining LUTs together and registering results in flip-flops, an FPGA can implement virtually any digital function, from simple logic gates to complete arithmetic units, limited only by the number of available resources on the device. Modern devices such as those in the Xilinx (AMD) Artix-7 family use 6-input LUTs, each capable of representing up to 64 input combinations in a single element.

    Programmable Interconnects

    Interconnects are the routing fabric that ties everything together. Programmable switch boxes and connection blocks sit at the intersections of horizontal and vertical wire channels throughout the device, allowing signals to travel between CLBs, memory blocks, I/O interfaces, and DSP units along paths that are defined at configuration time. The quality and density of the interconnect is one of the main factors determining how fast signals can propagate across the chip — and it is one of the reasons FPGAs consume more power and die area than an equivalent ASIC implementation of the same function.

    I/O Blocks (IOBs)

    I/O blocks connect the FPGA fabric to pins on the package, and through those pins to the external world. They are configurable for voltage standard, drive strength, termination, and direction (input, output, or bidirectional). This flexibility allows a single FPGA device to interface with a wide range of external components — DDR memory, high-speed serial links, sensors, or legacy parallel buses — without requiring external level-shifters or glue logic in many cases.

    Block RAM (BRAM) and DSP Blocks

    Dedicated Block RAM columns provide fast, on-chip data storage without consuming LUT resources. They support various configurations (single-port, dual-port, different widths and depths) and are used for FIFOs, buffers, lookup tables in signal processing, and local data caches. Alongside BRAM, most mid-range and high-end FPGAs include DSP blocks: hardened multiply-accumulate units optimized for arithmetic-intensive workloads like digital filters, FFTs, and matrix operations. Using these hard blocks instead of implementing the same function in LUTs dramatically improves both performance and power efficiency.

    Clock Management and Configuration Memory

    Phase-locked loops (PLLs) and clock management tiles generate and distribute clean clock signals across the fabric, supporting multiple clock domains and frequency synthesis. The configuration itself is typically stored in external flash and loaded into on-chip SRAM at power-up. This SRAM-based configuration is volatile — the bitstream must be reloaded each time the device powers on — but it also means the device is fully reprogrammable an unlimited number of times with no wear-out mechanism.

    What Is an ASIC?

    An Application-Specific Integrated Circuit (ASIC) is a chip designed and fabricated to perform one specific function or set of functions, permanently. Where an FPGA’s logic is defined by a software bitstream loaded at runtime, an ASIC’s logic is physically built into the silicon during manufacturing, through a process that requires custom photolithographic masks. Once an ASIC is fabricated, its function cannot be changed. Any design revision requires a new mask set and a new production run.

    The reason companies go through the cost and complexity of building a custom ASIC rather than using an FPGA comes down to three factors: performance, power, and per-unit cost at volume. An ASIC implementation of a given function will typically outperform an FPGA implementation of the same function in all three dimensions. There is no overhead from the programmable routing fabric, no SRAM configuration cells consuming power and area, and the logic can be laid out at the transistor level for maximum efficiency.

    The trade-off is the non-recurring engineering (NRE) cost. ASIC development at advanced process nodes carries NRE that runs into the millions of dollars, with the mask set alone a major line item. Any change after tape-out restarts that expenditure. This front-loaded cost structure makes ASICs economically sensible only when production volumes are high enough to amortize the NRE. As a rough guideline, the break-even point between an FPGA and an ASIC typically falls in the tens of thousands of units, though the actual crossover depends heavily on chip complexity, die size, process node, and product lifetime. Below that threshold, FPGAs tend to be more economical.

    What Is a Microcontroller?

    A microcontroller (MCU) is an integrated circuit that combines a CPU core, program memory (typically Flash), data memory (RAM), and a set of peripheral interfaces — timers, GPIO, ADC, UART, SPI, I2C, and so on — into a single package. It is, in effect, a small computer on a chip. You write firmware in C or C++ (or occasionally Assembly), compile it, and flash it to the device. The CPU then fetches and executes those instructions sequentially, one at a time, using the on-chip peripherals to interact with the outside world.

    Microcontrollers are by far the most widely deployed programmable logic device on the planet. They are in household appliances, industrial sensors, automotive ECUs, medical monitors, power management systems, and virtually every consumer electronic product with any kind of user interface or control loop. Their popularity comes from a combination of low cost, low power consumption, ease of programming, fast development cycles, and an enormous ecosystem of tools, libraries, and community knowledge. Vendors like Texas Instruments, STMicroelectronics, Microchip, NXP, and Infineon each offer hundreds of MCU families spanning from low-cost 8-bit parts to 32-bit Arm Cortex-M devices running at hundreds of megahertz with rich peripheral sets — see the microcontrollers category for the range.

    The key architectural constraint of a microcontroller is its sequential execution model. No matter how fast the CPU clock is, the processor can only work on one instruction at a time. This is entirely adequate for the vast majority of control and monitoring applications, but it becomes a bottleneck in tasks that require processing multiple high-speed data streams simultaneously — which is exactly where FPGAs are at an inherent architectural advantage.

    FPGA vs. ASIC: Key Differences

    FPGAs and ASICs are both hardware solutions — neither executes software instructions the way a microcontroller does — but they sit at opposite ends of a flexibility-versus-efficiency spectrum. The table below captures the principal differences, followed by a deeper discussion of the factors that drive real-world design decisions.

    Factor FPGA ASIC
    Reconfigurability Fully reprogrammable, unlimited times Fixed at fabrication; no changes possible
    Upfront NRE cost Low (no mask costs) High (millions of dollars at advanced nodes)
    Per-unit cost at volume Higher (wide range by device size) Lowest at high volume
    Performance (raw speed) High, but constrained by routing overhead Maximum — optimized at transistor level
    Power consumption Higher due to SRAM config fabric overhead Lower — can be fully optimized for the application
    Time to market Fast — no fabrication lead time Long — 12–18+ months for tape-out and verification
    Post-deployment updates Yes — new bitstream can be loaded in the field No
    Optimal volume range Low to medium (prototype through tens of thousands of units) High volume (tens of thousands of units and up)

    One practical workflow that many teams follow is to prototype and validate a design in FPGA first, then migrate the verified RTL to an ASIC once the architecture is stable and volumes justify the NRE. This phased approach reduces risk: the FPGA prototype catches design bugs at a fraction of the cost of discovering them after tape-out. FPGAs are also used as long-term production devices in cases where volumes never reach the ASIC crossover point, or where field upgradeability is a requirement that outweighs the per-unit cost premium.

    It is also worth noting that in the AI era, this dynamic is shifting somewhat. FPGAs are increasingly being deployed in edge AI inference roles — processing neural network workloads at the board level — because their reconfigurability allows teams to update models and quantization schemes as algorithms evolve, rather than being locked into the architecture of a fixed-function AI accelerator chip.

    FPGA vs. Microcontroller: Key Differences

    The FPGA-versus-microcontroller comparison is arguably more nuanced than FPGA-versus-ASIC, because both devices are reprogrammable and both are routinely found in embedded system designs — sometimes on the same board. The distinction comes down to what “programmable” means for each device and how they process work.

    A microcontroller runs software. Its CPU fetches instructions from flash memory, decodes them, executes them, and moves to the next one. This is fundamentally a sequential process. Even when a microcontroller uses interrupts, DMA, or multiple timer channels, the CPU itself is always executing one instruction per clock cycle (or a small, fixed number on pipelined architectures). An FPGA, by contrast, implements hardware circuits. When you configure an FPGA, you are physically defining the connections between logic elements. The resulting circuit runs entirely in parallel — all parts of it are always active simultaneously. There is no instruction fetch, no decode stage, no software scheduler.

    This distinction has direct practical consequences. An FPGA can process dozens of independent data streams at the same time with deterministic, cycle-accurate timing. A microcontroller reading from multiple sensors must time-multiplex that work, introducing latency and jitter that may or may not be acceptable depending on the application. For tasks like real-time motor control with sub-microsecond PWM deadband requirements, high-speed serial protocol bridging, radar signal processing, or custom image filtering pipelines, an FPGA’s parallel execution model is the right tool. For tasks like reading a temperature sensor over I2C, updating a display, and controlling a relay based on user input, a microcontroller is simpler, cheaper, and easier to develop for.

    Factor FPGA Microcontroller
    Processing model True parallel hardware execution Sequential instruction execution
    Architecture Configurable logic fabric (CLBs, BRAM, DSP) Fixed: CPU + Flash + RAM + peripherals on one chip
    Programming language VHDL, Verilog (hardware description) C, C++, Assembly (software)
    Timing determinism Cycle-accurate, fully deterministic Deterministic in bare-metal; less so under RTOS
    Power consumption Higher (typically ~1W to 10W+ for larger devices) Lower (often 1mW to 500mW, with sleep modes)
    Unit cost Higher — wide range by device size Lower — commodity pricing for common parts
    Development complexity Higher — requires HDL expertise and synthesis tools Lower — large community, extensive libraries
    Boot time Milliseconds to seconds (bitstream load required) Microseconds to milliseconds (executes from flash directly)

    It is common for complex systems to use both. The FPGA handles high-speed, latency-sensitive data processing (for example, a sensor front-end or a communication PHY), while a microcontroller manages system state, user interfaces, and communication with higher-level software. Each device does what it does best, and they talk to each other over a standard serial interface like SPI or a parallel bus.

    Side-by-Side Comparison: FPGA, ASIC, and Microcontroller

    Attribute FPGA ASIC Microcontroller
    Function definition Bitstream (HDL-derived) Fixed in silicon at fab Firmware (C/C++)
    Reconfigurable? Yes, unlimited No Yes (firmware updates)
    Processing style Parallel hardware Parallel hardware (fixed) Sequential software
    NRE / development cost Low–Medium Very High Low
    Per-unit cost at scale Medium–High Very Low Very Low
    Power efficiency Moderate Best Best (for control tasks)
    Time to market Fast Slow (12–18+ months) Fast
    Best for Custom high-speed logic, low-to-mid volume High-volume, fixed, performance-critical Control, sensing, cost-sensitive embedded

    Where Each Technology Is Used

    The choice of device type tends to follow the application’s demands rather than any single preference. Here is where each technology most commonly appears in practice today.

    FPGA Applications

    • Telecommunications and 5G infrastructure: baseband processing, protocol adaptation, and signal encoding/decoding where standards evolve faster than ASIC development cycles allow.
    • Aerospace and defense: radar signal processing, avionics control, and secure communications — areas where deterministic timing, radiation tolerance in specific device families, and the ability to update hardware post-deployment are all valued.
    • Data centers and AI acceleration: FPGA-based inference cards and SmartNICs for workloads where flexibility in model deployment outweighs the efficiency advantage of a fixed accelerator ASIC.
    • Automotive ADAS and sensor fusion: LiDAR preprocessing, camera pipeline acceleration, and real-time decision logic in systems that are still evolving before ASIC consolidation.
    • ASIC prototyping: validating RTL design on an FPGA before committing to tape-out, which is nearly universal in modern ASIC development flows.

    ASIC Applications

    • Consumer electronics at mass scale: smartphone application processors, Wi-Fi and Bluetooth SoCs, power management ICs — parts made in the hundreds of millions where the NRE is trivially amortized.
    • Cryptocurrency mining hardware: the canonical case of an application so computationally uniform and volume-sensitive that custom silicon dominates entirely.
    • High-frequency trading: ultra-low latency network interface cards where even FPGA routing overhead is too much and a fixed pipeline is required.
    • Display drivers, codecs, and other media processing: fixed-function blocks optimized for a specific encoding standard.

    Microcontroller Applications

    • Industrial automation: PLC-adjacent sensing, actuator control, machine monitoring, and HMI interfaces.
    • Consumer and home appliances: washing machines, thermostats, HVAC controllers, smart lighting — anywhere a simple, low-cost control loop is sufficient.
    • Medical devices: infusion pumps, patient monitors, glucose meters — applications where low power, reliable sequential execution, and certification-friendly C codebases matter.
    • Automotive body and powertrain control: ECUs, instrument clusters, and battery management systems in EVs often use microcontrollers from families like NXP S32, STM32, or Renesas RH850.
    • IoT sensor nodes: edge devices running on coin cells or energy harvesting, where the ultra-low-power sleep modes of modern MCUs are a core feature.

    How to Choose the Right Device for Your Project

    No single device is universally better. The right answer depends on a combination of technical requirements and project economics. The following questions help narrow the decision quickly.

    Does your task require true parallelism or deterministic sub-microsecond timing? If yes, an FPGA is likely the better fit. A microcontroller executing code sequentially will introduce latency and jitter that may be unacceptable in high-speed signal processing, custom protocol implementation, or precision control loops.

    Is the design stable and will it ship in volumes in the tens of thousands of units or more over its lifetime? If yes, evaluating an ASIC path makes economic sense. Below that threshold, the NRE is rarely justifiable unless there are extreme power or performance requirements that an FPGA cannot meet. The cost crossover is not a hard rule — it shifts based on chip complexity, die size, process node, and how long the product will stay in production.

    Is the application primarily a control or monitoring task without unusual speed requirements? A microcontroller is almost certainly the right choice. The development ecosystem is mature, costs are low, and the device will do the job reliably. Reaching for an FPGA in a context that doesn’t need parallel hardware is overengineering.

    Will the design need hardware updates after deployment? An FPGA’s in-field reprogrammability is a genuine advantage in systems where protocols or algorithms evolve. An ASIC will need a new spin; a microcontroller can receive firmware updates but cannot change its hardware architecture.

    What are the power constraints? Battery-powered edge devices almost always gravitate toward microcontrollers, which can operate at milliwatt levels with aggressive sleep modes. FPGAs typically consume at least one watt even in modest configurations, and large devices can exceed 10 watts under load. ASICs can be designed to meet essentially any power target but require the volume economics to justify that investment.

    In practice, many systems combine more than one approach. A common pattern is an FPGA handling high-speed front-end processing and a microcontroller managing system logic and communication — each contributing what it does best. Sourcing both device types reliably, especially through extended product lifecycles, is where a supply chain partner becomes relevant. WIN SOURCE, a global independent distributor of electronic components, stocks FPGAs and microcontrollers across current-production and hard-to-find part numbers and supports shortage sourcing, lifecycle management and alternative solutions across the full component lifecycle — with any substitute subject to final approval by the customer’s engineering team.

    Conclusion

    FPGAs, ASICs, and microcontrollers occupy distinct positions in the digital design landscape. A microcontroller runs software sequentially and is the practical, cost-effective choice for most control and sensing applications. An FPGA implements hardware logic in a reconfigurable fabric, enabling true parallel processing and post-deployment flexibility at the cost of higher unit price and power draw. An ASIC goes further still — locking in a circuit design permanently in exchange for maximum performance, minimum power, and lowest per-unit cost at high volume, though with substantial NRE and development time as the entry cost.

    Understanding the trade-offs between these three device types allows engineers and procurement teams to make better decisions earlier in a design cycle. The best choice is not the most powerful technology on paper — it is the one that fits the application’s performance requirements, volume economics, development timeline, and lifecycle expectations. In many real systems, more than one of these technologies will appear together, each doing the work it is structurally suited for.

    Frequently Asked Questions

    What is the difference between an FPGA and a microcontroller?

    A microcontroller runs firmware sequentially on a CPU with on-chip flash, RAM and peripherals; an FPGA is configured by a bitstream into a hardware circuit whose parts all run in parallel with cycle-accurate timing. MCUs are cheaper, lower-power and easier to develop for control and sensing tasks; FPGAs win when many high-speed data streams or deterministic sub-microsecond timing are required.

    When does an ASIC make more sense than an FPGA?

    When the design is stable and lifetime volume is high enough — typically tens of thousands of units and up, depending on complexity and process node — to amortize the multi-million-dollar NRE, or when power or performance targets exceed what an FPGA can reach. Below that, the FPGA’s zero mask cost, fast time to market and field reprogrammability usually win.

    Can an FPGA be reprogrammed after deployment?

    Yes. SRAM-based FPGAs load their configuration from external flash at power-up and can be reprogrammed an unlimited number of times, so a new bitstream can change the hardware function in the field. An ASIC is fixed at fabrication; a microcontroller can take firmware updates but its hardware architecture does not change.

    What are the main building blocks inside an FPGA?

    Configurable logic blocks (lookup tables, flip-flops and carry chains), the programmable interconnect that routes signals between them, configurable I/O blocks, hard block RAM and DSP multiply-accumulate units, and clock management (PLLs) plus the configuration memory that holds the bitstream.

    Do systems use FPGAs, ASICs and microcontrollers together?

    Often. A common pattern is an FPGA handling the high-speed front end — a sensor interface or communication PHY — while a microcontroller manages system state, user interface and communications, with an ASIC or SoC covering fixed high-volume functions. Each device does what it is structurally suited for and they communicate over SPI or a parallel bus.

    Part discontinued, obsolete or hard to find?

    WIN SOURCE is a global independent distributor of electronic components, supporting component supply, shortage sourcing, lifecycle management and alternative solutions. Visual inspection, non-destructive testing and electrical testing are applied according to material risk, customer requirements and the applicable quality process, and orders are covered by the published return policy and a 3-year warranty on eligible components.

    Stock and pricing are updated daily — search a part number or contact us for current availability, lead time and a quote.

    Search a Part Number  Upload a BOM / RFQ

    © 2026 Win Source Electronics. All rights reserved. This content is protected by copyright and may not be reproduced, distributed, transmitted, cached, or otherwise used without the prior written permission of Win Source Electronics.