• Home
  • Q&A
  • Industrial Controls, Meters
  • What types of inverters are classified according to control methods?

    * Question

    What types of inverters are classified according to control methods?

    * Answer

    Inverters, which convert direct current (DC) into alternating current (AC), are classified into different types based on their control methods. Each type uses a specific technique to control the output waveforms, influencing the efficiency, complexity, and cost of the inverter. Here are the main types of inverters classified according to their control methods:

    1. Square Wave Inverters: These are the simplest form of inverters and produce a square wave output. The control is straightforward, switching the DC input voltage fully on and off to produce a waveform that approximates an AC signal. While easy to implement, square wave inverters are typically only suitable for very basic applications due to their high harmonic content, which can be damaging or cause inefficient operation in sensitive electronic devices.

    2. Modified Sine Wave Inverters (or Quasi-Sine Wave Inverters): These inverters offer a compromise between complexity and output waveform quality. The output more closely resembles a sine wave than a square wave by using multiple steps or pulses in the output waveform. They are more compatible with a variety of household appliances than square wave inverters but still may cause problems with more sensitive equipment or appliances that rely on a precise sine wave.

    3. Pulse Width Modulated (PWM) Inverters: PWM inverters are more sophisticated and can provide a very high-quality sine wave output. The inverter controls the output voltage and frequency by varying the width of the pulses in the output waveform. This method allows for precise control over the output, leading to high efficiency and suitability for a wide range of applications, including sensitive electronic devices, medical equipment, and renewable energy systems.

    4. Sinusoidal Pulse Width Modulation (SPWM) Inverters: A specific type of PWM inverter, SPWM inverters aim to replicate a pure sine wave more closely than standard PWM techniques. By adjusting the duty cycle of the pulses to follow a sinusoidal reference, these inverters can significantly reduce harmonic distortion and improve the quality of the output waveform.

    5. Space Vector PWM (SVPWM) Inverters: This is an advanced modulation technique that provides better utilization of the DC supply voltage and reduces harmonic distortion further than traditional PWM techniques. It is widely used in applications requiring high precision and efficiency, such as in electric vehicle drives and industrial motor controls.

    6. Sliding Mode Control (SMC) Inverters: These inverters use a control law that forces the inverter’s output to “slide” along a defined dynamic system trajectory, drastically reducing the effects of system uncertainties and improving robustness. This method is highly effective in environments where the load or input conditions are variable and unpredictable.

    Each type of inverter has its suitable applications based on the needs for power quality, cost, complexity, and efficiency. The choice of inverter control method depends on the specific requirements of the application it is intended for.