![](https://blog.win-source.net/wp-content/uploads/2023/09/5-What-is-an-18650-lithium-battery-650x368.jpg)
Meet the 18650, a remarkable lithium-ion rechargeable battery that goes by the formal name 18650 cells. These batteries operate at a voltage of 3.7 volts and come with varying capacities, typically ranging from 1800mAh to 3500mAh (milliamp-hours).
Notably, the 18650s may exhibit a voltage spectrum spanning from 2.5 to 4.2 volts or a charging voltage of 4.2 volts. However, the standard nominal voltage for a typical 18650 cell is 3.7 volts.
Within this category, there exist two distinct types: protected and unprotected. It’s highly recommended to opt for the protected cell 18650 batteries. Protected cells incorporate a safety-protection circuit, ensuring they won’t be overcharged, thus bolstering safety.
On the flip side, unprotected cells lack this safeguard, which means they have the potential to be overcharged, leading to ruptures and, in extreme cases, fire hazards—unless specific electronics are in place to shield the battery. Notably, some popular models like LG HG2, INR, and Samsung 25r and 35e fall into the category of UNPROTECTED batteries, and they should only be used in devices designed to accommodate such cells.
Another essential consideration is the quality of the 18650 battery. Sticking with well-established brand names is prudent to avoid subpar imitations that might falsely advertise higher capacities (mAh).
Regarding recharging, the average 18650 battery requires around 4 hours for a full charge. However, this charge time can vary based on factors such as the amperage and voltage of the charger, as well as the specific battery type you’re using.
The 18650 battery represents a noteworthy advancement in rechargeable power. Still, it comes with critical nuances, including the choice between protected and unprotected versions, the importance of brand reliability, and the variable charge times based on charger specifications and battery type. Understanding these intricacies ensures a safe, efficient, dependable experience with the 18650 Marvel.
Table of Contents
ToggleDiverse Battery Dimensions Unveiled: A Visual Comparison
Below is an illustrative depiction of various battery sizes, each possessing unique cubic millimeter measurements. The 18650 battery occupies 1170 cubic mm, while the 14500 and AA batteries share a volume of 700 cubic mm, with the AAA battery compactly residing within 467 cubic mm.
It’s worth noting that while the 14500 battery resembles the AA size, it’s only universally compatible with some AA devices if those devices support both 3.7-volt and 1.5-volt batteries. A noteworthy distinction arises with the 21700 battery, taking up 1550 cubic mm, surpassing the 18650 battery in size—highlighting that the 21700 and 18650 are not interchangeable.
Now, let’s compare 18650 batteries with other commonly used battery types, considering essential attributes such as rechargeability, voltage, maximum milliamp hours (mAh), watt hours (Wh), and length and diameter measurements.
● Nitecore 21700: Rechargeable, 3.7v, 5000 mAh, 18.5 Wh, L: 74mm, D: 21.4mm.
● XTAR Li-ion 14500: Rechargeable, 3.7v, 800 mAh, 2.9 Wh, L: 50mm, D: 14mm.
● Eneloop Pro AA: Rechargeable, 1.2v, 2550 mAh, 3.0 Wh.
● Eneloop Pro AAA: Rechargeable, 1.5v, 950 mAh, 1.4 Wh.
As a point of comparison, a 12v car battery is included, showcasing its considerable capacity with 40,000 mAh and a remarkable 480 Wh. This comprehensive overview underscores the unique features of each battery type, making it easier to select the right battery for specific applications based on rechargeability, voltage, capacity, and size requirements.
Understanding 18650 Battery Terminology: Demystifying the Features
When faced with a battery labeled as “protected mode 3.7v 18650 3000 mAh low self-discharge for high-drain devices,” it’s essential to decode the meaning behind these specifications.
Protected Mode indicates that the 18650 battery possesses built-in safeguards against overcharging and excessive discharging through an embedded circuit within the battery casing, enhancing safety
3.7v: This value signifies the optimal voltage or the peak power output. However, as the battery is used, the voltage will gradually drop.
3000 mAh: This measurement denotes the battery’s capacity, expressed in milliampere-hours (mAh). A higher number is preferable, but it’s essential to note that the most realistic capacity available today for 18650 batteries is around 4000 mAh. Claims exceeding this value often lean toward marketing hype.
Low Self-Discharge: This positive attribute indicates that the battery can retain its unused charge. Batteries with low self-discharge lose minimal charge during storage, ensuring more power is available for devices when needed, such as flashlights.
For High-Drain Devices: This specification signifies that the battery is optimized for high-drain devices, which consume power rapidly. Examples include RC toy cars and other devices with significant power requirements.
Now, let’s delve into the distinction between protected and unprotected 18650 batteries:
Protected 18650 Batteries: These batteries feature an embedded electronic circuit within the cell packaging, offering protection against overcharging, overheating, over-discharging, overcurrent, and short circuits. Opting for a protected 18650 battery enhances safety, reducing the likelihood of overheating, bursting, or fire hazards.
Unprotected 18650 Batteries: Although cheaper, we strongly advise against using unprotected batteries without external monitoring and control of load, draw, and charging. Typically, protected batteries have a “button top,” but it’s crucial to check specifications. Flat-top 18650 batteries generally lack the protection circuit.
If you encounter any damaged or corroded 18650 batteries or if they appear leaking, ensure proper disposal at a battery recycling center for safety.
Power Capacity of an 18650:
A typical 3.7v 3400mAh 18650 can store around 2 ampere-hours (aH) to a maximum of 3.5 aH, translating to approximately 10 to 13 watt-hours (Wh). To put this in perspective, a small air conditioning unit capable of cooling around 9000 BTUs consumes about 1100 watts per hour. Running this air conditioner for an hour would require over 110 of these 18650 batteries.
In comparison, achieving the exact power requirement using traditional car batteries would necessitate three 12v 40 amp car batteries. Notably, the compact size of 110 18650 batteries surpasses that of three car batteries while meeting the same energy demand. This highlights the remarkable energy density of these small but potent 18650 cells.
Summary
In the world of rechargeable batteries, the 18650 stands tall. It holds its charge, serves high-drain devices with excellence, and even plays a role in the sustainable future of energy storage. Though seemingly diminutive, its impact is substantial. It’s a reliable companion, powering flashlights, RC cars, and many other devices.
COMMENTS