Taoglas is a leading provider of high-performance antenna solutions for the IoT and M2M industries. With over 12 years of experience, Taoglas has continuously pushed the boundaries of antenna technology to provide connectivity solutions that enable devices to communicate reliably and efficiently.
One such advancement from Taoglas is their A.03.C.1001111 Antenna – a game-changing product designed for GPS and Galileo receivers.
The Need for High-Performance Antennas in GPS and Galileo Receivers
GPS (Global Positioning System) and Galileo are two of the most widely used global navigation satellite systems. They provide precise positioning, navigation, and timing information to a wide range of applications such as vehicle tracking, fleet management, precision farming, and more. However, for these systems to function accurately, they require high-performance antennas.
Antennas play a critical role in GPS and Galileo receivers as they are responsible for capturing the satellite signals and converting them into usable information. A weak or poorly performing antenna can lead to inaccurate positioning information, which can be detrimental in critical applications like aviation or emergency response.
Introducing the A.03.C.1001111 Antenna
The A.03.C.1001111 Antenna from Taoglas is a three-stage 40dB LNA (Low Noise Amplifier) antenna designed specifically for GPS and Galileo receivers. It boasts an impressive 50 Ω impedance, making it compatible with most GPS receiver modules on the market. Additionally, it has a maximum frequency of 1.57742 GHz, making it suitable for high-precision applications.
What Sets A.03.C.1001111 Apart from Other Antennas?
There are several factors that set the A.03.C.1001111 apart from other antennas in the market, making it a game-changing product for GPS and Galileo receivers.
Three-Stage 40dB LNA
One of the key features of the A.03.C.1001111 is its three-stage 40dB LNA, which amplifies weak signals from satellites before they are transmitted to the receiver. This feature ensures that even in areas with poor satellite coverage or in urban environments with high levels of interference, the antenna can still capture and amplify the signals for accurate positioning.
Height and Diameter
Another notable feature of this antenna is its compact size. At only 29mm high and 52mm in diameter, it complies with the latest EU directives for height restrictions while still providing excellent performance. This makes it a perfect choice for vehicles or assets where space is limited, or covert operation is necessary.
IP65 Rated and Durable
The A.03.C.1001111 is designed for heavy-duty use, with a one-piece C&C machined nickel steel base plate and threads that ensure durability even in harsh environments. Moreover, it has an IP65 rating, making it resistant to water and dust ingress, perfect for outdoor use.
Long Cable Lengths
Unlike other antennas that may suffer from signal loss or degradation over long cable lengths, the A.03.C.1001111 is specifically designed for use with cables longer than 5m (15 feet). This makes it a reliable choice for applications that require extended cable lengths, such as large fleet vehicle tracking or remote monitoring.
Frequency Bands and Signal Processing
The A.03.C.1001111 supports a single frequency band of 1575.42MHz ± 2MHz, which is the standard for GPS and Galileo receivers. This allows for efficient signal processing and reduces interference from other bands, ensuring accurate positioning data.
Furthermore, the antenna has a high gain of 40dB, which amplifies weak signals and improves signal-to-noise ratio for better reception.
Apart from amplifying weak signals, the A.03.C.1001111 also filters out unwanted noise and interference with its low noise figure (LNF) of less than 2dB. This means that only relevant satellite signals are received and processed, improving the overall performance of the receiver.
Applications of A.03.C.1001111
The A.03.C.1001111 Antenna is a versatile product that can be used in various applications where GPS and Galileo receivers are required. Some of the common uses include:
● Vehicle Tracking: With its compact size and high-performance capabilities, the A.03.C.1001111 is an ideal choice for tracking vehicles in large fleets. Its long cable length compatibility makes it suitable for use in larger vehicles, such as trucks or trailers.
● Precision Agriculture: In precision farming applications, where accurate positioning is crucial for tasks like crop spraying or harvesting, the A.03.C.1001111 provides reliable and precise location data.
● Emergency Response: During natural disasters or other emergency situations, accurate positioning information is vital for rescue operations. The A.03.C.1001111 antenna ensures that emergency response teams have accurate location data to guide them.
● M2M Applications: With the rise of IoT and M2M applications, the demand for high-performance antennas has also increased. The A.03.C.1001111 provides a reliable solution for transmitting data in machine-to-machine communication.
The A.03.C.1001111 Antenna from Taoglas is an excellent product that addresses the need for high-performance antennas in GPS and Galileo receivers. Its three-stage 40dB LNA, compact size, durability, and compatibility with long cable lengths make it stand out among other antennas in the market.
If you’re looking for a reliable and efficient antenna for your GPS or Galileo receiver, or compatible gps receiver modules, check out WIN SOURCE. As a leading distributor of electronic components, WIN SOURCE offers a wide range of products from top manufacturers.

COMMENTS