Overview
The STM8L151K4U6TR is an 8-bit microcontroller (MCU) launched by STMicroelectronics, designed for ultra-low power applications. It combines high-performance processing capabilities and energy efficiency, making it an ideal choice for applications such as portable devices, smart home systems, and industrial control.
Specification
Core architecture : | STM8 |
Operating voltage range : | 1.8V to 3.6V |
Flash capacity : | 16KB |
SRAM capacity : | 2KB |
Operating temperature range : | -40°C to +85°C |
Package Type : | LQFP-32 |
Outstanding features of STM8L151K4U6TR
The STM8L151K4U6TR microcontroller is designed to integrate STMicroelectronics’ leading low-power technology and rich peripheral interfaces, making it an ideal balance between energy efficiency, functionality and flexibility. Here are some of the salient features of this microcontroller:
· Ultra-low power design : This MCU adopts STMicroelectronics’ unique ultra-low power technology, which can reduce power consumption to less than 1µA in deep sleep mode, making it ideal for applications that have strict requirements on battery life.
· Rich peripheral interfaces : STM8L151K4U6TR is equipped with rich peripheral interfaces, including I²C, SPI, USART, etc., providing users with flexible design choices and can be easily integrated into various systems.
· Wide operating voltage range : Supports an operating voltage range of 1.8V to 3.6V, ensuring stable operation under different voltage conditions and increasing the diversity of application scenarios.
· High reliability : The microcontroller has passed rigorous industrial-grade testing and can maintain reliable performance in extreme environments, making it suitable for a variety of demanding industrial applications.
Application Areas
The STM8L151K4U6TR excels in the following areas with its low power consumption and high performance:
· Portable electronic devices : such as smart watches, fitness trackers, etc., which need to operate for long periods of time and rely on efficient power management.
· Smart home control systems : such as thermostats, smart lighting controls, etc., the STM8L151K4U6TR can minimize energy consumption while ensuring rich functionality.
· Industrial Automation : In industrial control systems that require stable and reliable performance, the STM8L151K4U6TR provides excellent processing power and extensive interface support.
Comparative analysis: STM8L151K4U6TR vs other microcontrollers
The STM8L151K4U6TR has a clear competitive advantage in the market due to its ultra-low power consumption and rich peripheral interfaces. The following is a comparison between it and other similar microcontrollers:
Features/Specifications | STM8L151K4U6TR | Other 8-bit microcontrollers |
Core Architecture | STM8 | Other 8-bit architectures |
Flash capacity | 16KB | 8KB – 32KB |
Operating voltage range | 1.8V to 3.6V | 2.0V to 5.5V |
Power consumption | Ultra-low (deep sleep < 1µA) | Moderate (deep sleep > 10µA) |
Package Type | LQFP-32 | LQFP-32 or larger |
Manufacturer Background
As one of the world’s leading semiconductor companies, STMicroelectronics is well-known for its innovative and reliable products. The company is committed to providing excellent semiconductor solutions for various electronic applications, and the STM8L151K4U6TR is its representative product in the field of microcontrollers.
Why choose STM8L151K4U6TR?
Choosing the STM8L151K4U6TR is not only choosing a microcontroller with excellent performance, but also choosing STMicroelectronics’ leading edge in ultra-low power technology. Whether it is supporting battery-powered portable devices or ensuring long-term stable operation in industrial automation systems, the STM8L151K4U6TR is an ideal choice for designers.
Frequently asked questions
- How does it maintain data integrity in ultra-low power mode? The STM8L151K4U6TR is designed with a dedicated low-power mode to ensure that all critical data is properly preserved when entering a low-power state.
- Are multiple development tools supported?Yes, STM8L151K4U6TR supports a variety of development environments and tools to ensure that designers can easily integrate and debug. For example, designers can use STM32CubeIDE, an Eclipse-based integrated development environment that provides powerful debugging capabilities and rich library support. In addition, professional development tools such as IAR Embedded Workbench and Keil MDK are also supported, which provide developers with flexible choices to ensure efficient development and testing of projects.
For more details and to explore our inventory, please visit the links below:
- Product Details: <LINK> Win Source – STM8L151K4U6TR
- Quote: <LINK> Win Source – RFQ
©2024 Win Source Electronics. All rights reserved. This content is protected by copyright and may not be reproduced, distributed, transmitted, cached or otherwise used, except with the prior written permission of Win Source Electronics.