In the field of electronics, choosing the right components can make or break your project. Particularly, when it involves detecting object presence or interruption, opto interrupters reign supreme. But with a plethora of options available, selecting the ideal one can be daunting.
Introducing the ITR8307/S17/TR8(B), a tiny powerhouse that might just be your perfect match.
Let’s see if it’s worth it or not.
What is an Opto Interrupter?
An opto interrupter, short for optical interrupter or opto switch, is a device designed to detect interruptions in the transmission of light signals. It consists of a light source, typically an infrared (IR) LED transmitter, and a light-sensitive receiver, often a phototransistor. The basic principle involves the interruption of light between the transmitter and the receiver, triggering a response when the light path is obstructed.
The opto interrupter serves as a crucial component in electronic systems where precise detection of interruptions is essential. It finds applications in various devices and control systems, contributing to the reliable operation of mechanisms such as sensors, encoders, and position detectors.
The speed and accuracy with which opto interrupters can detect changes in light transmission make them valuable in scenarios where precise timing and responsiveness are critical, ranging from consumer electronics to industrial automation. The ITR8307/S17/TR8(B) stands out among opto interrupters, offering a combination of fast response time, high sensitivity, and compact design, making it an optimal choice for a diverse array of applications.
TR8: A Speed Demon with a Keen Eye
First things first, the ITR8307/S17/TR8(B), abbreviated as TR8, boasts lightning-fast response times. This means it can register even the blink of an eye, making it ideal for applications where speed is important. Think high-precision object detection, encoder wheel reading, or even motion-activated security systems.
But speed isn’t everything. The TR8 also shines with its exceptional sensitivity. Its integrated NPN phototransistor is incredibly receptive to infrared light, enabling it to detect even the faintest disruptions in the beam. This heightened sensitivity translates to reliable performance even in dimly lit environments, where other interrupters might falter.
Precision Made for Compact Spaces
Size matters, especially in today’s electronics landscape. The TR8 understands this perfectly, sporting a slim and compact profile. This thin and lightweight design makes it a dream to integrate into space-constrained projects, from miniature robots to portable devices. No more struggling to fit bulky components into your precious PCB real estate.
Going Green with the TR8
In an era of increasing environmental consciousness, the TR8 takes an admirable stand. It’s proudly Pb-free, meaning it eliminates the use of harmful lead in its construction. This not only benefits the environment but also opens doors for applications in eco-friendly products and sensitive medical equipment.
Cut-Off Wavelength: A Tailored Vision
The TR8 operates in the infrared range, specifically with a cut-off visible wavelength. This means it’s blind to visible light, allowing it to focus solely on infrared disruptions. This targeted vision minimizes false triggers from ambient light sources, leading to cleaner and more accurate detection.
Beyond Speed and Size: A Versatile Champion
The versatility of the ITR8307/S17/TR8(B) extends across a myriad of applications, showcasing its adaptability and reliability in diverse electronic systems. Here’s a more in-depth exploration of its applications:
Camera Systems:
The ITR8307/S17/TR8(B) finds a crucial role in camera systems where rapid and accurate interruption of light signals is essential. Its fast response time and high sensitivity contribute to the seamless functioning of cameras, ensuring precise detection of interruptions for optimal image and video capture.
Video Cassette Recorders (VCR):
In-home entertainment, particularly VCRs, the TR8 proves to be a valuable component. Its ability to swiftly interrupt signals enhances the recording and playback processes in VCRs, providing users with a seamless and uninterrupted viewing experience.
Floppy Disk Drives:
Data storage systems, such as floppy disk drives, demand precision and reliability. The ITR8307/S17/TR8(B) meets these requirements with its reliable performance and compact design. Its fast response time is particularly advantageous in ensuring precise data read and write operations in floppy disk drives.
Cassette Tape Recorders:
Audio recording devices, including cassette type recorders, benefit from the TR8’s capabilities. The Opto interrupter ensures that interruptions in the recording process are promptly detected, contributing to the high-quality performance of cassette recorders in capturing and reproducing audio content.
Microcomputer Control Equipment:
The TR8’s adaptability makes it an ideal choice for various microcomputer control equipment. In applications where precise interruption capabilities are paramount, such as in industrial automation, robotics, and electronic control systems, the TR8 ensures accurate and reliable operation.
Printers and Scanners:
The ITR8307/S17/TR8(B) plays a crucial role in the functioning of printers and scanners. Its fast response time facilitates precise paper movement in printers, ensuring accurate printing, while in scanners, it contributes to the accurate reading of documents and images.
Proximity Sensors:
Proximity sensing applications benefit from the TR8’s high sensitivity and compact design. In automated systems, security devices, and robotics, the TR8 serves as an effective proximity sensor, detecting the presence or absence of objects with speed and accuracy.
Industrial Automation:
In industrial automation, the TR8 is employed in various control systems. Its reliability, coupled with the ability to operate in diverse environmental conditions, makes it an essential component for interrupting light signals in industrial processes, contributing to the overall efficiency and safety of automated systems.
The Verdict: Is the TR8 Your Perfect Match?
When it comes to choosing the right opto interrupter, the ITR8307/S17/TR8(B) presents a compelling case. Its blazing speed, keen sensitivity, compact design, and eco-friendly construction make it a top contender for a wide range of applications. So, if you’re looking for a reliable, versatile, and future-proof opto interrupter, the TR8 might just be your knight in shining armor – or rather, infrared beams.
Remember, the suitability of the TR8 ultimately depends on your specific project requirements. However, its impressive capabilities and diverse applications make it a strong contender worth considering. With its well-rounded skill set, the TR8 might just be the missing piece that elevates your project to the next level.
When it comes to sourcing electronic components, WIN SOURCE is a notable distributor that offers a wide range of products.
WIN SOURCE provides a platform for purchasing various electronic components, including semiconductors, integrated circuits, passive components, connectors, and Opto interrupters as well. They cater to the needs of businesses and individuals looking for reliable sources of electronic parts for their projects.
© 2025 Win Source Electronics. All rights reserved. This content is protected by copyright and may not be reproduced, distributed, transmitted, cached or otherwise used, except with the prior written permission of Win Source Electronics.

COMMENTS