* Question
| What are the precautions for using the pulse output command PLS/PLF? |
* Answer
| (1) PLS is the pulse rising edge differential output command, and PIJ is the pulse falling edge differential output command.The PLS and PLF commands can only be used for output relay Y and auxiliary relay M (excluding special auxiliary relays).
(3) When the input relay X0 is turned on, the PLS M0 command will output a pulse when the PIKE is operated by the stop.However, if a battery backup/latch auxiliary relay is used instead of M0, its PLS command will not output a pulse in this case. |

COMMENTS