• Home
  • QUESTIONS & ANSWERS
  • Integrated Circuits (ICs)
  • What are the ways in which message queues work?

    * Question

    What are the ways in which message queues work?


    *
    Answer

    1 one-to-one working mode: This way of working is that one task sends a message to the message queue, and another task reads the message from the message queue. This is the simplest way to work and is the most commonly used 2-to-one job.Mode: This mode of operation means that multiple tasks send messages to the same message queue.


    COMMENTS

    WORDPRESS: 0
    DISQUS: 0