* Question
What are the main advantages of the Sipex series? |
* Answer
(1) Efficient current adjustment scheme.
(2) The operating frequency of 2.4MHz reduces the size and ripple noise of the charge pump chip. (4) The white LED current is set by an external Resistors, RSENSE is used to set the flashlight mode current (FLASH is connected to the low level), and RSET is used to set the flash mode current (FLASH is connected to the high level).And has a shutdown control. (5) Built-in over voltage, over current and over temperature protection.Less than 20 |
COMMENTS