• Home
  • QUESTIONS & ANSWERS
  • Others
  • What is the role of the dual state symbol IO field?

    * Question

    What is the role of the dual state symbol IO field?


    *
    Answer

    The dual state symbol IO field uses a bit variable to switch between two different texts.The symbolic IO field in the figure is connected to the bit change scene “Auto/Manual Switch” for displaying the operating mode of the system.Compared to the multi-state symbol IO field, the dual-state symbol IO field does not require a text list configuration and the configuration is very simple.


    COMMENTS

    WORDPRESS: 0
    DISQUS: 0