What Is a TRIAC? How It Works and How to Choose One

  • Home
  • SUPPLY CHAIN INSIGHTS
  • What Is a TRIAC? How It Works and How to Choose One

    If you have ever adjusted a lamp dimmer, set a fan to half speed, or used an electric blanket with multiple heat settings, a TRIAC was almost certainly doing the work. Short for Triode for Alternating Current, the TRIAC is a three-terminal semiconductor switch that controls AC power by conducting in both directions — something a standard SCR cannot do. It is one of the most practical components in low-to-medium power AC circuits, partly because it requires only a single gate signal to control current flow in either half of the AC cycle.

    This article covers how a TRIAC works from the inside out: its construction, triggering quadrants, phase control behavior, and the dv/dt challenge that trips up designers working with inductive loads. It also walks through the key parameters you need to match a TRIAC to a specific application — voltage rating, RMS current, gate trigger current, holding current, and more. Whether you are specifying parts for a new design or troubleshooting an existing circuit, the goal here is a single reference that answers both the “how does it work” and “how do I pick the right one” questions.

    Technical Reference
    What Is a TRIAC?

    Triode for Alternating Current — The essential semiconductor switch for AC power control. How it works, how it triggers, and how to select the right one.

    5 Key Takeaways
    1

    Conducts in both directions — one gate controls both AC half-cycles

    2

    Self-commutating — turns off automatically at every AC zero crossing

    3

    Phase control — firing angle α (0°–180°) sets delivered power continuously

    4

    Q1 & Q3 are the most sensitive triggering quadrants for most designs

    5

    dv/dt rating is the critical spec for inductive loads — don’t skip it

    ⚡ TRIAC Anatomy at a Glance
    Three Terminals
    MT1

    Main Terminal 1 — voltage reference point for gate signal and curves

    MT2

    Main Terminal 2 — connected to metal tab; attach heat sink here

    GATE

    Single gate controls both directions — always measured relative to MT1

    Equivalent Structure

    Internally = two SCRs in inverse parallel sharing a common gate — integrated into a single three-pin package for simplicity.

    Turn-On

    Gate pulse triggers conduction in microseconds. Device latches on — gate can be removed immediately.

    Turn-Off

    Turns off passively at AC zero crossing — no turn-off circuitry needed. Cannot operate on DC.

    Phase Control — How Power Is Regulated

    Firing angle α determines what fraction of each AC half-cycle reaches the load

    0°
    Firing Angle
    100% Power
    Full cycle delivered
    45°
    Firing Angle
    ~91% Power
    Early fire, high output
    90°
    Firing Angle
    ~50% Power
    Midpoint of half-cycle
    135°
    Firing Angle
    ~9% Power
    Late fire, low output
    180°
    Firing Angle
    ~0% Power
    Near-zero delivery

    Typical circuit: RC network + potentiometer creates variable delay · DIAC sharpens trigger pulse · Naturally operates in Q1 & Q3

    The Four Triggering Quadrants

    MT2 voltage vs. gate polarity — both relative to MT1

    Q1 BEST

    MT2 + · Gate +

    Most sensitive. Lowest gate trigger current. Standard positive half-cycle mode.

    Q2 FAIR

    MT2 + · Gate −

    Similar gate sensitivity to Q1, but lowest latching current sensitivity — light-load latch risk.

    Q3 BEST

    MT2 − · Gate −

    Mirror of Q1 in negative half-cycle. Nearly equal sensitivity. Pairs with Q1 in most designs.

    Q4 AVOID

    MT2 − · Gate +

    Least sensitive. Highest IGT required. Modern 3-quadrant TRIACs omit Q4 for better commutation.

    Note: IGT varies by quadrant — it can differ substantially between most and least sensitive modes. Always check your datasheet per quadrant.

    Key Selection Parameters

    Work through these in order — skipping any is a common source of field failures

    1
    VDRM — Voltage Rating

    Choose at least 2× peak line voltage. Use 400 V for 120 VAC lines; 800 V for 230 VAC mains (600 V where transients are well controlled).

    2
    IT(RMS) — Current Rating

    Rated at a specific case temperature — derate in warm environments. Heat sink mandatory above 4–5 A continuous. Also check ITSM for surge events.

    3
    IGT — Gate Trigger Current

    Specified per quadrant; worst case at lowest temperature. Sensitive-gate (“S”) types work with optocouplers but need better dv/dt protection.

    4
    IH & IL — Holding / Latching

    IH = minimum current to stay on. IL = minimum at gate-pulse removal to latch. Both increase at low temperatures — check cold-start behavior.

    5
    dv/dt — Critical for Inductive

    Commutating dv/dt(c) is much lower than static dv/dt. Inductive loads can exceed this limit at turn-off — causing false firing. Never skip this for motor/transformer loads.

    6
    3Q vs. 4Q — Quadrant Support

    If your drive operates in Q1/Q3, a 3-quadrant device (alternistor) offers better commutating dv/dt immunity and reduced snubber needs.

    Practical Design Considerations
    Snubber Circuit (Inductive Loads)

    RC snubber across MT1–MT2 limits dv/dt at commutation. Typical starting values for 230 V mains: 100 Ω + 100 nF (rated ≥400 V). Exact values depend on load inductance and dv/dt(c) spec.

    Heat Management

    On-state voltage drop VTM ≈ 1.5 V. At 8 A RMS → ~12 W dissipated. Use Rth(j-c) and Rth(c-a) from datasheet to size heat sink. Use insulating pad if MT2 tab mounts to grounded chassis.

    Gate Drive Isolation

    Optocouplers are the standard solution — TRIAC connects directly to AC mains.
    • MOC3041 series: zero-crossing trigger, reduced EMI
    • MOC3020 series: variable firing angle for phase control

    ⚠ TRIAC vs. Back-to-Back SCR

    TRIACs: simpler, compact, good to ~40 A RMS. Above that — or with heavy inductive commutation — inverse-parallel SCR pairs offer better surge handling and robustness.

    ⚙ Common TRIAC Applications
    Light Dimmers

    RC-DIAC phase control varies firing angle per half-cycle

    Fan / Motor Speed

    Phase control reduces average AC voltage to motor windings

    Heater Control

    Integral-cycle (burst-fire) switching for harmonic-free power regulation

    Solid-State Relays

    Many low-current AC SSRs use a TRIAC + optocoupler output

    Soft Starters

    Ramps firing angle from 180° → 0° at startup to limit inrush current

    Quick DMM Test Guide
    Step 1 — Off-State Check

    − lead on MT1, + lead on MT2 → should read very high resistance. Low reading = device shorted.

    Step 2 — Gate Trigger Test

    Briefly connect gate to MT2 → resistance drops near zero and stays low after jumper removed. Stays high = failed gate or junctions.

    Step 3 — Reverse Polarity

    Swap leads (+ on MT1, − on MT2) and repeat trigger test. Both directions must latch to confirm full bidirectional operation.

    ⚠ Note: Some DMMs don’t supply enough current to exceed IH of larger TRIACs. If it won’t latch, use a bench supply (few volts + current-limiting resistor). Always work on isolated, de-energized circuits.

    Need TRIACs or discrete semiconductors?

    Global independent distributor of electronic components · Shortage sourcing & lifecycle management

    What Is a TRIAC?

    A TRIAC is a bidirectional thyristor-famil>What Is a TRIAC?ch alternating current on and off under gate control. The name stands for Triode for Alternating Current, reflecting its three terminals and its intended operating environment. Unlike a diode or a standard rectifier, a TRIAC does not restrict current to one direction; it conducts freely in both the positive and negative half-cycles of an AC waveform once triggered, and it turns off naturally every time the load current falls back to zero — which happens twice per AC cycle.

    Structurally, a TRIAC is equivalent to two silicon-controlled rectifiers (SCRs) connected in inverse parallel, sharing a common gate. Because both internal SCR structures are integrated into a single three-pin package, only one gate terminal is needed to control both directions of conduction. This makes TRIACs considerably simpler and more compact than using two discrete SCRs back-to-back for the same purpose. The tradeoff is that TRIACs are generally limited to medium-power AC applications; for very high current tasks, two separate SCRs in inverse parallel often remain the preferred approach.

    Internal Structure and Terminal Naming

    A TRIAC has three term>Internal Structure and Terminal Naming), MT2 (Main Terminal 2), and the Gate. Because the device conducts in both directions, the conventional anode/cathode labeling used for diodes and SCRs does not apply. Instead, MT1 serves as the voltage reference point for both the gate signal and the characteristic curves. MT2 is typically connected to the metal tab on through-hole packages and is therefore the terminal usually attached to a heat sink.

    The gate shares a physical proximity to MT1, which means the gate signal is always measured and specified relative to MT1. A small current injected into the gate — regardless of whether it is positive or negative — is enough to switch the TRIAC into conduction, provided the main terminal voltage and current exceed the device’s minimum thresholds. Once conducting, the TRIAC latches on and continues to pass current even after the gate signal is removed, until the main current drops to zero.

    How a TRIAC Turns On (and Off)

    A TRIAC stays in a blocking state >How a TRIAC Turns On (and Off) until the gate receives a trigger pulse. When that pulse arrives, the device switches into conduction within a few microseconds, and the load sees current determined by the supply voltage and load impedance. Critically, the gate does not need to remain active after triggering: the TRIAC latches itself on through an internal positive-feedback mechanism involving its equivalent NPN and PNP transistor structures.

    Turn-off is entirely passive. Because the device is conducting AC, the current naturally passes through zero at the end of each half-cycle. At that zero crossing, the TRIAC loses its latching condition and returns to the blocking state, ready for the next gate trigger. This self-commutating behavior is a defining advantage over many other controllable switches — no turn-off circuitry is required. It also means TRIACs cannot be used directly in DC circuits, because a DC load never produces the current zero crossing that the device needs to extinguish.

    The minimum current that must flow through the main terminals to keep the TRIAC latched after triggering is called the holding current (IH). If the load current drops below IH before the next zero crossing — which can happen with light loads — the TRIAC may drop out of conduction unexpectedly. Similarly, the latching current (IL) is the minimum current that must be flowing in the main terminals at the moment the gate pulse ends; if the load has not yet drawn enough current by the time the gate is released, the TRIAC will not latch on at all.

    The Four Triggering Quadrants

    Because MT2 voltage and gate polarity can>The Four Triggering Quadrantse with respect to MT1, a TRIAC has four possible triggering combinations, conventionally mapped to four quadrants:

    • Quadrant I (Q1): MT2 positive, gate positive. The most sensitive and most commonly used mode. Gate current flows in the same direction as main terminal current, which produces the lowest required trigger current.
    • Quadrant II (Q2): MT2 positive, gate negative. Approximately equal in gate sensitivity to Q1, but the lowest latching current sensitivity of any quadrant, which can make it difficult to reliably latch the device at light loads.
    • Quadrant III (Q3): MT2 negative, gate negative. The mirror image of Q1 during the negative half-cycle. Sensitivity is nearly as good as Q1, making Q1 and Q3 together the standard operating pair for most phase-control circuits.
    • Quadrant IV (Q4): MT2 negative, gate positive. The least sensitive quadrant, requiring the highest gate current to achieve reliable firing. Many modern “3-quadrant” TRIACs deliberately omit support for Q4 to improve commutation performance in the other three.

    In most practical designs, the gate current comes from MT2 through a resistor divider or DIAC, so the circuit naturally operates in Q1 and Q3 — the most sensitive quadrants. Designs driven by a microcontroller or digital isolator with a single-polarity supply often operate in Q2 and Q3 instead, with MT1 held at positive voltage and the gate pulled low. Understanding which quadrant your circuit uses is important when reading the gate trigger current (IGT) values on a datasheet, because IGT is specified separately for each quadrant and can differ substantially between the most and least sensitive modes.

    Phase Control: How TRIACs Regulate Power

    The most powerful use of a TRIAC>Phase Control: How TRIACs Regulate Power controlling how much of each AC half-cycle is delivered to the load. This technique is called phase control (or phase-cut dimming). The trigger circuit introduces a time delay after each zero crossing, called the firing angle (α), measured in degrees. The TRIAC fires at angle α, conducts until the next zero crossing, and then resets. By varying α from 0° to nearly 180°, the fraction of each half-cycle that reaches the load changes continuously.

    At α = 0°, the TRIAC fires immediately at every zero crossing and delivers full power. At α = 90°, it fires at the midpoint of each half-cycle and delivers roughly 50% power. At α approaching 180°, it fires very late and delivers only a small fraction. A simple RC network with a potentiometer creates the variable time delay, and a DIAC (a bidirectional breakover device) is commonly used in series with the gate to sharpen the trigger pulse and keep the firing symmetrical on both half-cycles. The DIAC-RC combination naturally triggers in Q1 and Q3 — the optimal quadrants.

    One side effect of phase control is that it chops the AC waveform, which generates harmonic content and can cause electromagnetic interference. For sensitive applications, line filters or zero-crossing switching (where the TRIAC fires only at zero crossings, toggling whole cycles rather than partial ones) may be preferable. Zero-crossing control greatly reduces harmonics and EMI but provides only coarse power resolution.

    TRIAC vs. SCR: When to Use Which

    The TRIAC and SCR are closely related — a TRIAC is in>TRIAC vs. SCR: When to Use Which— but the right choice depends on the application. TRIACs are the simpler, more compact option for AC control circuits up to moderate power levels. A single device, a single gate drive circuit, and a single PCB footprint handle both half-cycles. SCRs, by contrast, conduct only in one direction, so full AC control with SCRs requires two devices in inverse parallel and, in many designs, two separate gate drive circuits.

    The tradeoff appears at higher power levels and in commutation-sensitive applications. TRIACs are generally rated for continuous RMS currents up to roughly 40 A in consumer-grade packages; above that, inverse-parallel SCR pairs offer better surge current handling and more rugged commutation behavior. Inductive loads — motors, transformers, solenoids — are also more demanding for TRIACs than for SCR pairs, because the phase shift between current and voltage causes the TRIAC to see a fast-rising reapplied voltage at commutation, which can cause false triggering (discussed further below). For purely resistive loads at moderate power, TRIACs are almost always the better economic and design choice.

    How to Choose a TRIAC: Key Selection Parameters

    Matching a TRIAC to its application means work>How to Choose a TRIAC: Key Selection Parametersc order. Skipping any of them is a common source of field failures.

    Voltage Rating (VDRM)

    VDRM (peak repetitive off-state voltage) is the maximum>Voltage Rating (VDRM)TRIAC can block in its off state without triggering or being damaged. For a 120 V AC line (170 V peak) or a 230 V AC line (325 V peak), a standard practice is to choose a VDRM of at least twice the peak line voltage to provide margin for transients. A 400 V TRIAC is common for 120 V applications. For 230 V mains, 800 V parts give the full twofold margin; 600 V parts are also widely used where transients are well controlled.

    Current Rating (IT(RMS))

    The RMS on-state current rating defines how much con>Current Rating (IT(RMS))carry without exceeding its maximum junction temperature. This rating is specified at a particular case temperature, so it must be derated if the part runs in a warm environment or without adequate heat sinking. Heat sinking is generally mandatory for continuous currents above 4–5 A. Also check the non-repetitive surge current (ITSM), which governs how well the device handles brief overload events such as motor starting or capacitor inrush.

    Gate Trigger Current (IGT) and Gate Sensitivity

    IGT is the minimum gate current>Gate Trigger Current (IGT) and Gate Sensitivitystate voltage and temperature. It is listed separately for each relevant quadrant, and it typically increases as junction temperature decreases, so the worst case is at the lowest operating temperature. Sensitive-gate TRIACs (sometimes labeled “S” variants, with IGT in the low milliamp range) work well with optocouplers and microcontroller I/O, but they are more susceptible to false triggering from dv/dt transients. Standard-gate parts need more gate drive but offer higher dv/dt immunity.

    Holding Current (IH) and Latching Current (IL)

    IH sets the floor for reliable c>Holding Current (IH) and Latching Current (IL)fore the zero crossing, the TRIAC drops out. This is rarely a problem with resistive loads but matters with light inductive loads, where current waveforms can fall sharply. IL defines the minimum current at gate-pulse removal for the TRIAC to latch. Both parameters increase at lower temperatures, so cold-start behavior in outdoor or unheated enclosure applications deserves a specific check.

    dv/dt Rating

    The static dv/dt rating specifies how fast the off-state voltage a>dv/dt Ratingrise without causing the TRIAC to self-trigger. Resistive loads are generally safe. Inductive loads create a phase-shifted current, so when the TRIAC turns off at current zero, the voltage across it can reapply at a fast rate — potentially exceeding the static dv/dt limit and causing false commutation firing. The datasheet lists a commutating dv/dt (dv/dt(c)) specifically for this scenario, which is usually considerably lower than the static value and must be checked against the actual load inductance and supply voltage.

    Quadrant Support: 3-Quadrant vs. 4-Quadrant

    Standard TRIACs support all four triggering quadrants.>Quadrant Support: 3-Quadrant vs. 4-Quadrantuadrant TRIACs (sometimes called “alternistors”), which deliberately omit Q4 support in exchange for much better commutating dv/dt immunity. If your gate drive circuit operates in Q1 and Q3 — the usual case — a 3-quadrant device can reduce snubber requirements with inductive loads — confirm the substitution against both datasheets, and final approval belongs to the customer’s engineering team. If your drive scheme relies on Q4, use a standard 4-quadrant device.

    Practical Design Considerations

    Snubber Circuits

    Practical Design ConsiderationsSnubber Circuitspt">For inductive loads, an RC snubber connected directly across MT1 and MT2 is almost always required. The snubber — typically a resistor and capacitor in series — limits the rate of voltage rise (dv/dt) at commutation, preventing false triggering. Without a snubber, the oscillation between the load inductance and the TRIAC’s internal capacitance can produce a reapplied dv/dt far above the device’s commutating limit. A well-chosen snubber brings this within the rated value; typical starting values for 230 V mains with moderate inductive loads are around 100 Ω and 100 nF (rated for at least 400 V), though exact values depend on load inductance and the specific TRIAC’s dv/dt(c) rating.

    Heat Management

    A TRIAC dissipates power as heat during conduction, primarily as the product of the on-state >Heat Managementpically around 1.5 V) and the RMS load current. At 8 A RMS, that is roughly 12 W, which is significant enough to require a heat sink for any sustained duty cycle. The datasheet thermal resistance values (Rth(j-c) and Rth(c-a)) let you calculate the required heat sink thermal resistance for a given ambient temperature and maximum junction temperature. If the TRIAC tab (MT2) is mounted to a grounded chassis, an insulating pad is needed between the tab and the metal to avoid shorting MT2 to ground.

    Gate Drive Isolation

    Because the TRIAC connects directly to the AC mains, the gate drive circuit is normally >Gate Drive Isolationcontrol logic. Optocouplers designed for TRIAC triggering (such as MOC3020 or MOC3041 series) are the standard solution. Zero-crossing detector optocouplers (MOC3041 and similar) include an internal zero-crossing circuit that fires the TRIAC only at voltage zero, which reduces EMI. For phase control applications requiring variable firing angle, a non-zero-crossing optocoupler (MOC3020 series) is used, with the firing angle controlled by a microcontroller timer or an analog RC-DIAC network.

    Common TRIAC Applications

    TRIACs — listed as their own Common TRIAC Applicationstarget="_blank" rel="noopener">TRIACs category among discrete semiconductors — appear in a wide range of AC control applications. Their combination of bidirectionality, gate simplicity, and zero-crossing turn-off makes them well suited to any load where smooth, silent, and wear-free switching is needed:

    • Light dimmers: Phase control with an RC-DIAC network adjusts brightness by varying the firing angle on every half-cycle.
    • Fan and motor speed controllers: The same phase-control technique reduces average voltage to a universal or AC induction motor, adjusting speed.
    • Electric heater controls: Integral-cycle (burst-fire) switching toggles full AC cycles on and off to regulate average power to heating elements without generating harmonics.
    • Appliance start circuits: TRIACs can replace mechanical centrifugal switches in capacitor-start motors, eliminating arcing in locations where sparks are a hazard.
    • Solid-state relays (SSRs): Many AC solid-state relays, particularly at lower current ratings, use a TRIAC output stage driven by an optocoupler, replacing a mechanical relay with no moving parts; higher-rated SSRs commonly use inverse-parallel SCRs.
    • Soft starters: A TRIAC-based soft starter ramps the firing angle from ~180° to 0° during motor startup, limiting inrush current and mechanical shock.

    How to Test a TRIAC

    The most reliable way to evaluate a TRIAC is under real operating conditions with an oscillosco>How to Test a TRIACl conduction waveform and any false triggering or commutation failures. When that is not available, a basic out-of-circuit check with a digital multimeter (DMM) set to resistance (Ω) can confirm whether the device is functional or shorted.

    With the negative lead on MT1 and the positive lead on MT2, the DMM should read infinite or very high resistance — the TRIAC is off. Briefly connecting the gate to MT2 with a small jumper wire should cause the resistance to drop near zero as the device latches on; the reading should stay low after removing the jumper. Reversing the leads (positive to MT1, negative to MT2) and repeating the gate trigger test should produce the same result in the opposite polarity direction. A TRIAC that reads low resistance before any gate trigger is shorted. One that never drops to low resistance after triggering has a failed gate or failed junctions.

    Keep in mind that some DMMs do not supply enough current through the resistance range to exceed the holding current of larger TRIACs. If the device appears to trigger but does not latch after removing the jumper, try a bench power supply set to a few volts with a current-limiting resistor to provide a cleaner test current through the main terminals. Always work on isolated, de-energized circuits and discharge any capacitors before probing.

    Summary

    The TRIAC remains one of the most efficient tools for AC power control in the small-to-medium power range. Its>Summaryl conduction, passive zero-crossing turn-off, and single-gate interface make it simpler to use than back-to-back SCR pairs for the same job. Getting the part selection right means working through voltage rating, RMS current, gate sensitivity (IGT per quadrant), holding and latching currents, dv/dt rating, and quadrant support — in that order. For resistive loads, most standard parts work well with minimal external circuitry. For inductive loads, the dv/dt(c) specification and snubber design move to the center of the conversation. Understanding those tradeoffs up front prevents the majority of TRIAC reliability problems in the field.

    Frequently Asked Questions

    What is the difference between a TRIAC and an SCR?

    >Frequently Asked Questions>What is the difference between a TRIAC and an SCR?n one direction only, while a TRIAC conducts in both directions under a single gate, so one TRIAC can control both halves of an AC cycle. For high currents or demanding inductive loads, two SCRs in inverse parallel are often preferred for their surge handling and commutation robustness.

    Can a TRIAC be used on DC?

    Not as a normal switch. A TRIAC turns off only when its current falls below the holding curre>Can a TRIAC be used on DC? zero crossing; a DC load never provides that zero crossing, so the TRIAC stays on once triggered.

    Why does my TRIAC turn on by itself with a motor load?

    With inductive loads, voltage reappears across the TRIAC quickly >Why does my TRIAC turn on by itself with a motor load?ating dv/dt rating the device retriggers. An RC snubber across MT1–MT2, or a 3-quadrant TRIAC with higher commutation capability, is the usual fix.

    What voltage rating should a TRIAC have for 230 V mains?

    230 V AC peaks at about 325 V. Choosing roughly twice the peak po>What voltage rating should a TRIAC have for 230 V mains?transients are well controlled. Check the design’s surge environment before settling on the lower rating.

    How do I choose between a zero-crossing and a random-phase optocoupler?

    Use a zero-crossing optocoupler such as the MOC304>How do I choose between a zero-crossing and a random-phase optocoupler?ero and reduces EMI. Use a random-phase type such as the MOC3020 series for phase-control dimming or speed control, where the firing angle must vary.

    Part discontinued, obsolete or hard to find?

    WIN SOURCE is a global independent distributor of electronic components, supp>Part discontinued, obsolete or hard to find?cle management and alternative solutions. Visual inspection, non-destructive testing and electrical testing are applied according to material risk, customer requirements and the applicable quality process, and orders are covered by the published return policy and a 3-year warranty on eligible components.

    Stock and pricing are updated daily — search a part number or contact us for current availability, lead time and a quote.

    Search a Part Number  Upload a BOM / RFQ

    © 2026 Win Source Electronics. All rights reserved. This content is protected by copyright and may not be reproduced, distributed, transmitted, cached, or otherwise used without the prior written permission of Win Source Electronics.