MOSFET vs Relay: When Solid-State Beats Mechanical Switching

  • Home
  • SUPPLY CHAIN INSIGHTS
  • MOSFET vs Relay: When Solid-State Beats Mechanical Switching

    Every switching circuit eventually comes down to the same question: do you move electrons through a semiconductor, or do you physically snap two metal contacts together? MOSFETs do the former; electromechanical relays do the latter. Both have been doing their jobs reliably for decades, and both continue to ship in enormous volumes — because neither has made the other obsolete.

    What has changed is the range of applications that now clearly favor one approach over the other. Modern power electronics, motor drives, and battery management systems have tilted the balance toward solid-state switching in ways that weren’t obvious even twenty years ago. At the same time, relays remain the right answer for plenty of real-world scenarios — any time you need hard galvanic isolation, straightforward AC mains control, or the ability to switch high-voltage loads without exotic gate-drive circuitry.

    This article walks through the core technical differences between MOSFETs and relays across the dimensions that actually matter in circuit design: switching speed, power loss, isolation, lifespan, load type, and noise. The goal is a clear reference you can return to when a design decision needs to be grounded in specifics rather than convention.

    Engineering Reference
    MOSFET vs Relay

    When Solid-State Beats Mechanical Switching — A Practical Comparison

    5 Key Takeaways

    ⚡ Speed Gap: 6 Orders of Magnitude

    MOSFETs switch in nanoseconds; relays need 5–15 ms — making PWM only possible with solid-state.

    Always-On Coil Drain

    Relays draw 50–80 mA continuously while held. MOSFETs consume near-zero gate power when fully on.

    ♾️ No Contact Wear

    MOSFETs have no contacts to erode. Relays are rated ~100K electrical operations — less than 1 week at 10×/min.

    Relays Win on Isolation

    Relays provide inherent galvanic isolation. MOSFETs need an optocoupler or isolated driver for mixed-voltage systems.

    AC Switching = Relay Territory

    Standard MOSFETs are DC-only. Relays handle AC naturally — or use a solid-state relay (SSR) for the best of both.

    ⏱ Switching Speed Comparison

    MOSFET
    Nanoseconds (ns)
    Relay
    5–15 ms

    Bar width scaled to illustrate the ~6 orders of magnitude difference in switching speed.

    By The Numbers

    490–980
    Hz
    Default Arduino PWM — already faster than a relay can respond
    20–32
    kHz
    Pro motor drive PWM — silent, above human hearing
    50–80
    mA
    Relay coil current — continuous idle drain on batteries
    100K
    ops
    Typical relay electrical life — MOSFETs have no contact wear
    <7
    days
    100K cycles at 10×/min = relay service life in automation

    Decision Guide

    USE A MOSFET WHEN
    →DC load, PWM or >10 Hz switching required
    →Long cycle life without maintenance
    →Battery-powered — coil quiescent current is a concern
    →Silent operation and compact PCB profile
    →Vibration/shock environment — no moving parts
    USE A RELAY WHEN
    →AC mains load (HVAC, appliances, industrial)
    →Galvanic isolation needed without extra circuitry
    →Load voltage much higher than control voltage
    →Switching <few times per minute (infrequent)
    →Very low on-state voltage drop required
    Consider an SSR (Solid-State Relay): When you need AC switching with solid-state speed and cycle life — or DC isolation without sacrificing MOSFET longevity.

    Typical Applications

    MOSFET

    PWM Motor Drives LED Dimming Switching Regulators
    Battery Management Solenoid Drivers

    Relay

    HVAC Control AC Mains Switching Industrial Contactors
    Automotive High-Side Appliance Control

    Source MOSFETs, Relays & Discrete Semiconductors

    Global independent distributor of electronic components — component supply, shortage sourcing, lifecycle management & alternative solutions

    Submit RFQ / BOM →

    How Each Device Actually Switches

    A MOSFET (Metal Oxide Semiconductor Field Effect Transistor) is a three-terminal semiconductor device — gate, drain, and source. Applying a sufficient voltage to the gate creates a conductive channel inside the silicon die, allowing current to flow between drain and source. Remove the gate voltage and the channel collapses, interrupting current flow. The entire process takes place inside a solid piece of semiconductor material; nothing moves. Gate drive current requirements are extremely low because the gate is capacitive by nature, which is why MOSFETs can be driven directly from microcontroller output pins or CMOS logic in many designs.

    A mechanical relay works by a completely different principle. A low-voltage control current energizes an electromagnetic coil, which pulls a ferromagnetic armature toward it. That armature physically moves a set of metal contacts, either closing a normally-open path or opening a normally-closed one. When the coil is de-energized, a return spring moves the contacts back. The switching action is therefore entirely mechanical — which brings with it all the strengths and limitations of moving metal parts under electrical load.

    Switching Speed: The Gap Is Enormous

    This is where the two technologies diverge most sharply. A typical mechanical relay takes 5 to 15 milliseconds to open or close — the armature has to physically travel, and that takes time regardless of how fast the coil energizes. A MOSFET, by contrast, switches in the nanosecond range. That difference of roughly six orders of magnitude has profound practical consequences.

    The most direct consequence is PWM (Pulse Width Modulation) compatibility. PWM motor control, LED dimming, and switching regulators all depend on rapidly cycling the switch on and off at controlled duty cycles. A common Arduino PWM default runs at 490–980 Hz, meaning each cycle lasts about 1–2 milliseconds — already faster than a relay can mechanically respond. Professional motor drive applications routinely operate at 20–32 kHz, keeping audible switching noise above the threshold of human hearing. A relay cannot follow these frequencies at all, and attempting it would destroy the contacts quickly. MOSFETs handle these frequencies without difficulty, provided the gate drive circuit can charge and discharge the gate capacitance quickly enough — a task often handled by a dedicated gate driver IC at higher switching frequencies.

    For simple on/off control where switching happens only a few times per minute or hour, the relay’s slower response is irrelevant. The speed advantage of a MOSFET only matters when the switching rate itself is part of the control strategy.

    Contact Bounce, Arcing, and EMI

    One underappreciated consequence of mechanical switching is contact bounce. When a relay’s contacts close, the metal surfaces don’t make clean, single contact — they physically bounce 2 to 10 times over a period of 1 to 5 milliseconds before settling into a stable closed state. Each bounce creates a brief arc between the contacts. These arcs erode the contact surface over time, generate electromagnetic interference (EMI), and can cause false triggering in sensitive digital circuits monitoring the switched path.

    Arcing becomes more significant as load current and inductance increase. Under inductive loads, the collapsing magnetic field drives a voltage spike across the opening contacts — precisely the worst conditions for contact longevity. Over thousands of switching cycles, this electrical erosion progressively increases contact resistance and eventually causes the contacts to fail to make reliable connection. The electrical life of power relay contacts under load is often a small fraction of their rated mechanical life for this reason.

    MOSFETs produce none of this. Because switching occurs inside a semiconductor junction with no physical contact movement, there is no bounce, no arcing, and no EMI generated by the switching mechanism itself. (High-frequency MOSFETs do produce switching noise through fast voltage and current transitions, but this is a different and more controllable phenomenon than arc-induced EMI.)

    Power Consumption and Thermal Behavior

    Relays consume power continuously in the coil to maintain contact position. A small 5V relay coil typically draws 50–80 mA while energized, regardless of what the load is doing. In battery-powered or energy-sensitive applications, this idle coil current is a persistent drain. Latching relays exist that require only a pulse to change state and consume no power in either stable position, but they add complexity and cost.

    MOSFET power consumption is more nuanced. The gate itself is capacitive and draws negligible steady-state current — a fully-on MOSFET consumes no gate power. The real losses come from two sources. First, conduction loss: when the MOSFET is conducting, current flows through the drain-to-source on-resistance (RDS(on)), and the resulting I²R dissipation generates heat. Modern power MOSFETs have pushed RDS(on) values into the single-digit milliohm range for low-voltage devices, but at high currents even a few milliohms becomes significant. Second, switching loss: during each transition between on and off states, there is a brief period when both voltage and current exist across the device simultaneously. At high switching frequencies, these transition losses accumulate and can exceed conduction losses in some designs.

    Thermal management is a genuine engineering consideration for high-current MOSFET designs. Heat sinks, PCB copper pours, and in forced-air systems, direct airflow across the device are all common measures. Relays, by comparison, dissipate most heat in the coil, which is generally cooler and less thermally stressed than a MOSFET junction at high current.

    Electrical Isolation and Safety

    A relay provides galvanic isolation by default. The control circuit (coil) and the load circuit (contacts) are physically separated by the relay housing. There is no semiconductor path connecting the two sides — the only coupling is magnetic, via the field produced by the coil. This makes relays inherently appropriate for applications where a low-voltage microcontroller needs to switch 230V AC mains without any risk of the mains voltage appearing on the logic side.

    MOSFETs do not provide this separation. The gate, drain, and source are all part of the same semiconductor structure. In mixed-voltage systems, isolating the microcontroller from the power stage requires additional components: typically an optocoupler between the control signal and the gate driver, or an isolated gate driver IC. This adds cost and board space, but it also gives the designer explicit control over the isolation barrier characteristics — something that matters in safety-critical designs where the isolation voltage and leakage current need to be specified and verified.

    For purely DC circuits where the control voltage and load voltage are from the same supply rail and ground reference, isolation is often not a concern, and the MOSFET’s direct connection is an advantage rather than a problem.

    Lifespan and Reliability

    Relay datasheets specify two different life ratings: mechanical life (switching with no load, dominated by spring fatigue) and electrical life (switching under rated load, dominated by arc erosion). The electrical life is invariably shorter — often dramatically so. A relay rated for 10 million mechanical cycles may be specified for only 100,000 electrical operations at full load. In an automated system switching 10 times per minute, 100,000 cycles represents less than one week of continuous operation.

    MOSFETs don’t wear out through switching. There is no physical mechanism analogous to contact erosion. A MOSFET that is properly protected against overvoltage (with a clamp or flyback diode for inductive loads) and operated within its current and thermal ratings with sensible margin does not accumulate wear from the act of switching. Its long-term limit is thermal cycling of the package — bond wires and die attach fatigue as the junction heats and cools — which is why high-cycle designs keep temperature swings small. Failure modes for MOSFETs are different in character — they fail from exceeding VDS(max), from thermal runaway when dissipation exceeds cooling capacity, or from gate oxide damage — but these are design-margin problems, not inherent wear mechanisms.

    In environments with significant mechanical shock or vibration — automotive, industrial machinery, aerospace — mechanical relay contacts are vulnerable in additional ways. The armature can vibrate open under high-g loads, and contact surfaces exposed to humidity or contamination can corrode. Semiconductor devices have no such mechanical fragility.

    Handling Inductive Loads

    Both device types face challenges with inductive loads — motors, solenoids, transformers, and relay coils themselves all store energy in their magnetic fields and release it as a voltage spike when current is interrupted. The voltage spike can be many times higher than the supply voltage and can easily destroy an unprotected MOSFET.

    For MOSFET circuits, the standard protection is a flyback diode (also called a freewheeling or snubber diode) placed across the inductive load in the reverse-biased direction. When the MOSFET turns off and the inductive spike appears, the diode clamps the voltage and provides a path for the stored energy to dissipate safely. For more demanding designs, a Zener or TVS clamp lets the load current decay faster — useful where a solenoid must release quickly — at the cost of a higher clamp voltage that the MOSFET must be rated to withstand. With proper protection, MOSFETs handle inductive loads reliably and are the standard choice in PWM motor drives and solenoid drivers.

    Relay contacts, when switching inductive loads, experience arcing at the moment of contact opening. Suppression networks (RC snubbers across the contacts, or diodes for DC inductive loads) can reduce arcing, but they add components and require careful selection. Even with suppression, relay contact life under inductive loads is shorter than under resistive loads of equal current.

    AC vs DC Switching

    Standard power MOSFETs are fundamentally DC switching devices. Their internal body diode conducts in one direction only, which means a single MOSFET cannot block AC in both half-cycles. Switching AC with MOSFETs requires a back-to-back configuration (two MOSFETs with sources tied together, or with their body diodes opposing), adding circuit complexity. For most AC mains applications, the relay remains the simpler and more conventional choice.

    Relays switch AC naturally — the physical contacts simply open or close the circuit regardless of current direction or polarity. This is one area where the electromechanical approach has a genuine structural advantage. AC-powered HVAC equipment, compressors, industrial contactors, and household appliance control circuits almost universally use mechanical relays or contactors for exactly this reason.

    Solid-state relays (SSRs) bridge this gap by packaging a MOSFET or TRIAC output stage with an optocoupled input, giving the user an isolation interface that looks like a relay but switches electronically. SSRs are the preferred solid-state solution for AC load switching when the speed and cycle-life advantages of semiconductor switching matter more than the extremely low on-resistance of a mechanical contact.

    Decision Guide: Which One Do You Need?

    There is no universal answer — the right choice depends on the specific electrical requirements of the circuit. The following considerations cover the most common decision factors:

    • Use a MOSFET when: the load is DC; switching frequency is above ~10 Hz or PWM control is required; the design demands compact size and low profile; long cycle life without maintenance is important; silent operation matters; or the application is battery-powered and coil quiescent current is a concern.
    • Use a relay when: the load is AC mains; galvanic isolation is needed without additional isolation circuitry; the load voltage is significantly higher than the control voltage; switching happens infrequently (a few operations per minute or less); or very low on-state voltage drop across the switch matters (relay contacts have milliohm-range resistance).
    • Consider a solid-state relay (SSR) when: you need AC switching with solid-state speed and longevity, or when you need isolation for a DC load but want the cycle-life and noise advantages of MOSFET switching.
    • Consider combining both: some designs use a MOSFET for fast local switching and a relay for the high-voltage isolation stage. The MOSFET handles PWM or soft-start logic; the relay handles the final mains-connected load. This approach captures the benefits of each technology at the appropriate point in the circuit.

    The cost balance also shifts with volume and application. Relays are generally less expensive at the component level for simple on/off switching applications, and they require no gate-drive design effort. MOSFETs become clearly cost-effective once their circuit-level advantages — smaller PCB area, elimination of flyback protection for the coil, longer service life in high-cycle applications — are factored into the system cost.

    Quick Reference Comparison

    Parameter MOSFET Mechanical Relay
    Switching mechanism Semiconductor (voltage-controlled channel) Electromagnetic coil + mechanical contacts
    Switching speed Nanoseconds 5–15 milliseconds
    PWM compatibility Yes (kHz to MHz range) No (contacts weld or jam)
    Galvanic isolation No (requires optocoupler or isolated driver) Yes (inherent)
    AC switching Requires back-to-back topology Natural — polarity independent
    Steady-state power draw Near zero (gate is capacitive) Continuous coil current (50–80 mA typical)
    On-state resistance RDS(on) — milliohms to tens of milliohms Very low (typically milliohm-range contacts)
    Cycle lifespan No contact wear; limited by thermal cycling and overstress ~100,000 at rated load (electrical life)
    Contact bounce / arcing None Present at every switching event
    Vibration / shock resistance High (no moving parts) Moderate (armature can vibrate open)
    Typical applications Motor drives, PWM regulators, LED dimming, battery management HVAC, AC mains control, industrial contactors, automotive high-side switching

    Conclusion

    MOSFETs and relays have been coexisting in electronics for decades, and that isn’t changing. They solve different problems with different engineering tradeoffs, and the decision between them is almost always clear once you know the operating frequency, the load type, the isolation requirements, and the cycle-life expectations of the application.

    The solid-state advantage is most decisive when switching speed and longevity matter: PWM motor drives, switching regulators, high-cycle automation, and battery management systems are all scenarios where the MOSFET’s nanosecond response and freedom from contact wear are decisive. Relays hold their ground wherever galvanic isolation, AC mains control, or extremely low on-state voltage drop are the primary requirements — and for low-frequency switching of large resistive or AC loads, their simplicity and cost remain competitive. Understanding both technologies thoroughly — rather than defaulting to one by habit — is what leads to better circuits.

    Frequently Asked Questions

    Can a MOSFET replace a relay?

    For DC loads, often yes: a MOSFET switches faster, has no contact wear, runs silently and draws almost no control power. It does not provide galvanic isolation on its own and cannot block AC as a single device, so AC mains switching or isolation needs a relay, a solid-state relay, or an isolated gate driver.

    Why can’t a relay be used for PWM?

    A mechanical relay takes several milliseconds to open or close, while even a basic PWM signal cycles every millisecond or two and motor-drive PWM runs at tens of kHz. The contacts cannot follow, and repeated switching under load would erode them rapidly. PWM needs a semiconductor switch such as a MOSFET.

    Does a MOSFET need a flyback diode?

    When it switches an inductive load such as a motor, solenoid or relay coil, yes. Interrupting the current produces a voltage spike that can exceed the MOSFET’s drain-source rating. A diode across the load, or a Zener or TVS clamp where faster current decay is needed, gives the stored energy a safe path.

    What is the difference between a relay and a solid-state relay?

    A mechanical relay moves physical contacts with an electromagnet. A solid-state relay uses a semiconductor output stage — a MOSFET for DC, typically a TRIAC or SCR pair for AC — driven through an optocoupled input, giving isolation with no moving parts, no bounce and much longer switching life, at the cost of higher on-state voltage drop and heat.

    How long does a relay last compared with a MOSFET?

    Relay datasheets give a mechanical life and a much shorter electrical life at rated load, often on the order of 100,000 operations. A MOSFET has no contacts to wear; within its ratings its long-term limit is thermal cycling of the package rather than the number of switching operations.

    Part discontinued, obsolete or hard to find?

    WIN SOURCE is a global independent distributor of electronic components, supporting component supply, shortage sourcing, lifecycle management and alternative solutions. Visual inspection, non-destructive testing and electrical testing are applied according to material risk, customer requirements and the applicable quality process, and orders are covered by the published return policy and a 3-year warranty on eligible components.

    Stock and pricing are updated daily — search a part number or contact us for current availability, lead time and a quote.

    Search a Part Number  Upload a BOM / RFQ

    © 2026 Win Source Electronics. All rights reserved. This content is protected by copyright and may not be reproduced, distributed, transmitted, cached, or otherwise used without the prior written permission of Win Source Electronics.