* Question
What are the characteristics of dual in-line Integrated Circuits(ICs)s? |
* Answer
DIP has the following characteristics.
(1) It is suitable for perforation welding on printed circuit board (PCB), which is easy to operate. (2) The ratio between the chip area and the package area is large, so the volume is also large. (3) There are no special requirements other than the size and number of pins. |
COMMENTS