* Question
| How to apply SJAl000? |
* Answer
| The register and pin configuration of SJAl000 allows it to use a wide variety of integrated or discrete CAN transceivers.Since there are different microcontrollers connected to 1:3, different microcontrollers can be used in the application.Figure 10.6 shows a typical SJAl000 application that includes an 80C51 microcontroller and a PCA82C251 transceiver.It can also be controlled by an address decoder, such as when the address/data bus is used for other peripheral devices. |