• Home
  • QUESTIONS & ANSWERS
  • Integrated Circuits (ICs)
  • What is the structure of the hot wire air flow sensor?

    * Question

    What is the structure of the hot wire air flow sensor?


    *
    Answer

    The hot wire air flow sensor can be divided into two types according to the installation position of the measuring component: the first one is a hot wire air flow sensor called a mainstream measuring method in which the hot wire is installed in the main intake port.The second is to install the hot wire in the bypass airway, called the hot-wire air flow sensor in the bypass measurement mode.


    COMMENTS

    WORDPRESS: 0
    DISQUS: 0