• Home
  • QUESTIONS & ANSWERS
  • RF/IF and RFID
  • What parameters are affected by the identification range?

    * Question

    What parameters are affected by the identification range?


    *
    Answer

    The identification range is one of the most important parameters of the RFID tag. It is mainly affected by two parameters, that is, the tag can just get the maximum distance Rtag (tag activation distance) from the reader to open enough power and the reader can detect the tag.The maximum distance of the backscattered signal, Rreader,