* Question
| If the ADC and DAC are enabled and powered up before the sample rate is changed, the sample rate value change will be valid, so how is the sample rate set? |
* Answer
| The sampling rate setting steps are as follows:
(1) Enable and power up the ADC and DAC through registers 26h and 3Ch; (2) Enable register 2Ah bit [0]VRA; (3) Change the sample rate value in the respective registers. |