• Home
  • Q&A
  • Programmer, development system
  • What are the main technical features of the TPS7510x?

    * Question

    What are the main technical features of the TPS7510x?


    *
    Answer

    1 Eliminates the influence of electromagnetic interference (EMI) because it does not need internal switching signal;

    2 output current matching accuracy is: 2%;

    3 common cathode structure, driving up to 4 LEDs with each 25mA power; 4 in lithiumIn ion battery applications,The default LED current saves external components;

    7 with the innovative factory EEPROM programming technology, the default value can be set in the range of 3 ~ 10mA (step increment is lmA); 8 with over current and overheat protection.