* Question
What are the development trends of RFID electronic tags? |
* Answer
(1) The cost is lower.From the development of electronic tags, electronic tags will gradually mature in the next few years, especially in high-frequency and long-distance electronic tags, and have a broader prospect.The cost reduction will further promote the application of RFID technology.
(2) The volume is smaller.With the development of low-power IC design technology, the operating voltage of the electronic tag will be further reduced, and the required power consumption is reduced to less than 5 μW or even lower.The tag requires less energy, which further increases the range of the tag. (4) Suitable for the recognition of high-speed moving objects.The tag data should be strictly encrypted, and the communication process should be encrypted. This requires an electronic tag with stronger intelligence and better encryption characteristics, so that the tag can better hide its information and prevent unauthorized information.Was obtained. |
COMMENTS