• Home
  • QUESTIONS & ANSWERS
  • Programmer, development system
  • What are the layers of OLEDoS?

    * Question

    What are the layers of OLEDoS?

    The structure of the OLEDoS: First, a high work function metal is deposited on the monocrystalline silicon Integrated Circuits(ICs) chip as the anode of the OLED.In addition to the original anode metal layer, all other layers are thermally evaporated and compatible with conventional OLED device processes.A complete wafer can be used in a variety of processes, including the packaging process.Finally, the silicon wafers are separated into individual microdisplays.

    * Answer


    COMMENTS

    WORDPRESS: 0
    DISQUS: 1