* Question
How to connect without using dual network card? |
* Answer
Connect the ADSL Modem to the hub (providing a network card, which occupies one more hub port), and each host is connected to the hub.Each host can establish a broadband connection. Of course, only one host can establish a broadband connection at the same time, so that other hosts can share it.(1) Establish a broadband connection on a host and dial up to connect to the Internet.Such as 192.168.X.1 (X is not 0) and serves as the gateway address of other hosts.If you do not use the dual NIC mode, 192.168.0.1 is used as the gateway address of other hosts. |
COMMENTS