* Question
| Precautions when using transistors |
* Answer
| If a piece of soldering piece is attached to the bolt, the circuit lead is soldered to the soldering piece in advance, and the transistor pin is sandwiched between the two nuts on the bolt to reduce the risk of damage.Finally, the solder tabs are marked with the appropriate letters on the bakelite strip, and the color points are applied to the collector, and the leads of the circuit are also colored as shown (or a colored sleeve is placed).Special emphasis must be placed on the fact that the electrode connection will cause the transistor to burn out during use. |