* Question
What are the circuit characteristics and circuit analysis methods? |
* Answer
(1) The negative full-wave rectification circuit is the same as the positive full-wave rectification circuit. Two rectifier diodes are used to form a set of rectifier circuits. The AC voltage input circuit is the same. The difference is that the two rectifier diodes and the power transformer are twice.The ends of the winding are connected instead of the positive pole. |
COMMENTS