• Home
  • Q&A
  • Integrated Circuits (ICs)
  • What Are the Structural Types of LED Digital Tubes?

    * Question

    What Are the Structural Types of LED Digital Tubes?

    * Answer

    LED digital tubes, also known as seven-segment LED displays, are electronic display devices used to show numbers and limited characters.
    Their structures are defined by electrical connection method, physical packaging, and display configuration, each affecting driving方式、应用场景和系统设计。

    Below are the main structural types of LED digital tubes.

    1. Common-Cathode Structure

    Structure Description

    • All LED cathodes are connected together internally
    • Individual segments are controlled by applying a HIGH levelto the anodes

    Electrical Characteristics

    • Requires the driver to source current
    • Common in TTL/CMOS logic-driven designs

    Typical Applications

    • Microcontroller-based systems
    • Educational and industrial display modules

    2. Common-Anode Structure

    Structure Description

    • All LED anodes are internally connected
    • Segments light up when a LOW levelis applied to the cathodes

    Electrical Characteristics

    • Requires the driver to sink current
    • Widely used with transistor arrays and driver ICs

    Typical Applications

    • High-current display driving
    • Systems using ICs like ULN2803or LED driver chips

    3. Single-Digit vs. Multi-Digit Structures

    Single-Digit LED Digital Tubes

    • Contain one complete seven-segment display
    • Simple wiring and control

    Multi-Digit LED Digital Tubes

    • Combine multiple digits in one package
    • Often use multiplexed scanningto reduce pin count

    Common formats include:

    • 2-digit
    • 4-digit
    • 6-digit displays

    4. Integrated Decimal Point (DP) Structure

    Most LED digital tubes include a decimal point LED, which:

    • Is electrically independent
    • Requires separate control
    • Expands numeric display capability

    This is especially important for measurements such as voltage, current, or frequency.

    5. Package and Assembly Structures

    Through-Hole (DIP) Packages

    • Traditional pin-through-hole design
    • Strong mechanical stability

    Surface-Mount (SMD) Packages

    • Compact size
    • Suitable for automated assembly

    Light-Emitting Orientation

    • Front-emitting (standard)
    • Side-emitting (used in slim enclosures)

    Engineering Insight

    Selecting the correct LED digital tube structure directly impacts:

    • Driver circuit complexity
    • Power consumption
    • MCU I/O resource usage
    • Brightness uniformity

    For example, common-anode displays are often preferred in high-current, multi-digit scanning applications, while common-cathode displays simplify logic-level interfacing.

    Conclusion

    LED digital tubes can be structurally classified by:

    • Electrical connection type: common-cathode and common-anode
    • Display configuration: single-digit and multi-digit
    • Functional integration: with or without decimal point
    • Physical packaging: DIP or SMD

    Understanding these structures helps engineers select suitable display modules and design reliable driver circuits for embedded and industrial applications.