• Home
  • Q&A
  • Integrated Circuits (ICs)
  • What Kind of Device Is the SJA1000?

    * Question

    What Kind of Device Is the SJA1000?

    * Answer

    The SJA1000 is a standalone CAN (Controller Area Network) controller, originally developed by Philips Semiconductors and later maintained by NXP Semiconductors.

    It is designed specifically to handle CAN communication, and it works together with other components in a CAN system rather than operating independently.

    1. How the SJA1000 Is Classified

    From a functional point of view, the SJA1000 can be classified as:

    ✅ CAN bus controller

    ❌ Not a microcontroller (MCU)

    ❌ Not a CAN transceiver

    What this means in practical terms:

    • The SJA1000 does not run application programs
    • It cannot control the system by itself
    • It does not connect directly to the physical CAN bus

    Instead, it focuses only on managing CAN communication, while other devices handle processing and signal transmission.

    2. What the SJA1000 Actually Does

    The SJA1000 implements the core functions of the CAN 2.0A and CAN 2.0B protocols, including:

    • CAN message transmission and reception
    • Bus arbitration and synchronization
    • Error detection and fault handling
    • Message filtering
    • Interrupt signaling to the host controller

    In simple terms, the SJA1000 acts as the “CAN communication manager” inside a system.

    3. How the SJA1000 Is Used in a Typical CAN System

    In a standard CAN node, the SJA1000 is usually used together with:

    • A Microcontroller (MCU)

    Runs the application software

    Decides what data to send or receive

    • The SJA1000 CAN Controller

    Handles all CAN protocol-related tasks

    • A CAN Transceiver

    Converts logic-level signals into CAN bus differential signals

    Each component has a clear role, and the SJA1000 sits between the microcontroller and the CAN bus interface, ensuring reliable CAN communication.

    4. Why the SJA1000 Is Not a Microcontroller

    Although the SJA1000 is sometimes mistaken for an MCU, it differs in key ways:

    • It has no CPU for running user code
    • It has no program memory
    • It cannot operate without an external controller

    This separation helps system designers keep communication handling and application logic clearly divided, which was especially important in early and long-life industrial CAN systems.

    5. Typical Application Scenarios

    The SJA1000 is commonly found in:

    • Industrial control equipment
    • Automotive and transportation systems
    • Legacy CAN-based devices
    • Maintenance and upgrade projects requiring CAN compatibility

    Although many modern microcontrollers now integrate CAN controllers internally, the SJA1000 is still relevant for existing designs, repairs, and replacement needs.

    Conclusion

    The SJA1000 is a standalone CAN bus controller, not a microcontroller.
    Its main role is to manage CAN communication, while an external microcontroller handles application logic and a transceiver handles physical bus signaling.

    Understanding this distinction helps customers and engineers select the correct CAN-related components and avoid system design confusion.