* Question
What Is the Definition of Network Capacity?
* Answer
Mutual inductance refers to the phenomenon in which a changing current in one coil induces a voltage in another nearby coil due to the shared magnetic field between them.
This interaction occurs because the magnetic flux generated by one coil links with the turns of the second coil, creating an induced electromotive force (EMF).
Mutual inductance is a fundamental principle in transformers, inductive sensors, wireless charging systems, and EMI/EMC behavior in circuit design.
1. How Mutual Inductance Works
When electric current flows through Coil A, it generates a magnetic field. If Coil B is placed within this field:
- Any changein Coil A’s current causes the magnetic flux to vary.
- The varying flux induces a voltage in Coil B based on Faraday’s Law.
Mathematically:
VB=M*dIA/dt
Where:
- VB= induced voltage in Coil B
- M = mutual inductance between the two coils
- dIA/dt= rate of change of current in Coil A
2. Factors That Determine Mutual Inductance
Several physical and geometric parameters influence the magnitude of mutual inductance:
2.1 Distance Between Coils
Closer coils result in greater magnetic coupling.
2.2 Orientation
Coils aligned coaxially (same axis) achieve higher mutual inductance.
2.3 Core Material
A magnetic core such as ferrite or laminated steel increases flux linkage.
2.4 Number of Turns
More coil turns → more flux linkage → higher mutual inductance.
3. Real-World Applications of Mutual Inductance
Mutual inductance is essential to the operation of several critical components:
Transformers
Transformers rely entirely on mutual inductance to step voltage up or down. A device such as the Coilcraft SER1360 series inductor demonstrates how magnetic coupling efficiency influences performance.
Wireless Power Transfer
Systems like Qi wireless chargers use closely coupled coils to transfer energy through magnetic fields.
Signal Isolation
Digital isolators and isolation transformers use mutual inductance to safely transfer signals across high-voltage domains.
Inductive Sensing
Position and current sensors exploit magnetic coupling to detect movement or current flow.
4. Engineering Insight
Mutual inductance is both beneficial and challenging:
- It enables intentional energy transfer (e.g., transformers).
- It also causes unwanted coupling, leading to electromagnetic interference (EMI).
PCB designers often consider mutual inductance when spacing inductors or routing high-frequency traces near power coils.
Components such as Murata DLW series common-mode chokes are used specifically to manage and control magnetic coupling effects in signal lines.
Conclusion
Mutual inductance describes the coupling of magnetic fields between two coils, where a changing current in one coil induces a voltage in the other. It is a foundational concept in power conversion, communication systems, isolation design, and electromagnetic compatibility engineering.
A solid understanding of mutual inductance helps engineers design efficient circuits, optimize magnetic components, and minimize unwanted interference.