* Question
What are the commonly used types of absolute pressure sensors?
* Answer
Absolute pressure sensors are devices that measure pressure relative to a perfect vacuum (0 Pa or 0 bar), rather than relative to atmospheric pressure or another reference point.
They are essential in applications such as altitude measurement, vacuum systems, aerospace, weather instruments, and industrial process control, where accurate and stable readings are required regardless of environmental changes.
Commonly used absolute pressure sensors can be categorized based on their sensing principles and structural design.
1. Piezoresistive Absolute Pressure Sensors
These are the most widely used type.
They employ a silicon diaphragm with integrated piezoresistive elements (strain gauges). When pressure is applied, the diaphragm deflects, changing the resistance of the gauges.
This change is converted into an electrical signal proportional to the applied pressure.
Key features:
- High sensitivity and linearity
- Compact and cost-effective
- Suitable for automotive manifold pressure (MAP) and barometric applications
2. Capacitive Absolute Pressure Sensors
These sensors use a capacitor formed by a flexible diaphragm and a fixed electrode. When pressure changes, the diaphragm deflects, altering the capacitance.
The capacitance variation is measured to determine absolute pressure.
Key features:
- Excellent long-term stability
- Low temperature drift
- Ideal for low-pressure and barometric measurements (e.g., weather stations, altimeters)
3. Resonant (Quartz or Silicon) Absolute Pressure Sensors
Resonant sensors rely on the frequency shift of a vibrating element—typically a quartz or silicon resonator—caused by pressure-induced stress.
Because frequency signals are less susceptible to noise and temperature variations, these sensors provide high precision and long-term stability.
Key features:
- Very high accuracy
- Excellent repeatability and stability
- Common in aerospace, calibration, and scientific instrumentation
4. Optical (Fiber-Optic) Absolute Pressure Sensors
Optical pressure sensors measure diaphragm deflection using fiber-optic interferometry or intensity modulation.
They are immune to electromagnetic interference (EMI) and suitable for harsh or high-voltage environments.
Key features:
- EMI immunity
- Suitable for high-temperature or corrosive conditions
- Used in oil exploration, aerospace, and medical devices
5. Microelectromechanical System (MEMS) Absolute Pressure Sensors
MEMS-based sensors integrate the sensing diaphragm and signal conditioning circuitry on a single silicon chip.
They combine miniaturization, low power consumption, and mass-production capability, making them widely used in consumer electronics and IoT devices.
Key features:
- Compact, low-cost, and scalable
- Integrated temperature compensation
- Found in smartphones, drones, and wearable devices
Summary Insight
In summary, absolute pressure sensors can be classified into piezoresistive, capacitive, resonant, optical, and MEMS-based types, each offering a unique balance of accuracy, stability, and environmental compatibility.
Their selection depends on the measurement range, required precision, operating environment, and integration needs.
In modern designs, MEMS piezoresistive and capacitive sensors dominate due to their high performance-to-cost ratio, while resonant and optical types remain preferred for precision industrial and aerospace applications.