• Home
  • Q&A
  • Cable Assemblies
  • What are the operating modes of the PeliCAN controller?

    * Question

    What are the operating modes of the PeliCAN controller?

    * Answer

    The PeliCAN controller — a widely used implementation of the CAN (Controller Area Network) protocol — provides several operating modes that allow flexible control, testing, and fault management within CAN-based communication systems. These modes determine how the controller transmits, receives, and processes data frames on the CAN bus, ensuring both functional performance and diagnostic capability.

    1. Normal Mode

    This is the standard operating mode for regular CAN communication.
    In Normal Mode, the controller can both transmit and receive CAN messages according to the protocol rules.

    • All error detection, acknowledgment, and retransmission mechanisms are active.
    • Nodes participate fully in bus arbitration and data exchange.
      This mode is used during normal system operation in vehicles, industrial controllers, and embedded networks.

    2. Sleep Mode

    The Sleep Mode is designed to minimize power consumption when no bus activity is detected.

    • The CAN controller stops internal activities and waits for a wake-up signal(from the CAN bus or host processor).
    • Upon wake-up, it transitions back to Normal Modefor communication.
      This mode is essential in automotive applications where ECUs must conserve battery power during idle conditions.

    3. Initialization Mode

    Initialization Mode is used for controller configuration before active communication begins.

    • In this state, software can set up bit timing, acceptance filters, interrupt configurations, and other control parameters.
    • Message transmission and reception are disabled to prevent bus interference during setup.
      Once configuration is complete, the controller switches to Normal Mode.

    4. Listen-Only Mode

    This mode allows the controller to monitor all CAN bus traffic without participating in communication.

    • It does not send acknowledgments (ACKs) or error frames.
    • Useful for bus analysis, network diagnostics, or passive monitoring
      Listen-Only Mode ensures non-intrusive observation of the network, ideal for debugging or validation.

    5. Self-Test Mode (Loopback Mode)

    In Self-Test Mode, also known as Loopback Mode, the controller internally routes transmitted messages back to its receive buffer without sending them onto the bus.

    • Enables verification of CAN functionality without physical bus connections.
    • Useful for firmware testing, software validation, and controller diagnostics.
      This isolated environment ensures system reliability before deployment.

    6. Bus-Off Mode

    When the controller experiences persistent transmission errors, it automatically enters Bus-Off Mode to prevent network disruption.

    • The node stops transmitting and disconnects from the bus.
    • Recovery requires software intervention or automatic reinitialization after a predefined idle period.
      This protective mechanism maintains overall network stability and data integrity.

    Summary

    Mode

    Purpose

    Key Features

    Normal Mode

    Regular CAN communication

    Full transmit/receive with error handling

    Sleep Mode

    Power saving

    Waits for wake-up signal

    Initialization Mode

    Configuration setup

    No active communication

    Listen-Only Mode

    Passive monitoring

    Non-intrusive observation

    Self-Test (Loopback)

    Functional testing

    Internal message routing

    Bus-Off Mode

    Fault protection

    Disconnects after severe errors

    In summary, the PeliCAN controller supports multiple operating modes that balance performance, safety, and flexibility. From low-power standby to diagnostic and test configurations, these modes enable engineers to manage CAN communication effectively across diverse automotive and industrial environments.