• Home
  • Q&A
  • Integrated Circuits (ICs)
  • What kinds of finite state machines are classified according to their structure?

    * Question

    What kinds of finite state machines are classified according to their structure?

    * Answer

    Finite State Machines (FSMs) — also called finite automata — can be classified in several ways, but when the classification is based on their structure, they are mainly divided into two fundamental types:

    Moore Machine

    Mealy Machine

    These two types differ in how the outputs are generated relative to the states and inputs.

    1. Moore Machine

    Definition:

    A Moore machine is a finite state machine in which the output depends only on the current state, not directly on the input.

    Output=f(State)

    Characteristics:

    Each state has a fixed output value associated with it.

    Outputs change only when the machine changes states (i.e., synchronized with state transitions).

    Typically simpler to design and easier to debug.

    Advantages:

    More stable output (does not fluctuate with input changes).

    Suitable for synchronous systems.

    Disadvantages:

    May require more states than an equivalent Mealy machine to describe the same behavior.

    Example:

    If a Moore FSM is in state S1, it always produces the same output (e.g., 1), regardless of the input.

    2. Mealy Machine

    Definition:

    A Mealy machine is a finite state machine in which the output depends on both the current state and the current input.

    Output=f(State,Input)

    Characteristics:

    Outputs are associated with transitions between states, not the states themselves.

    Outputs can change immediately when inputs change, even without a state change.

    Advantages:

    Requires fewer states to implement the same logic as a Moore machine.

    More responsive, as output can react instantly to input variations.

    Disadvantages:

    Output can be less stable since it depends directly on inputs.

    More complex timing and design considerations.

    Example:

    If a Mealy FSM is in state S1 and receives input A, it may produce output 1; but with input B (same state), it may produce output 0.

    3. Comparison Summary

    Feature

    Moore Machine

    Mealy Machine

    Output depends on

    Current state only

    Current state and input

    Output changes

    On state change

    On input or state change

    Output stability

    More stable

    Less stable (input-sensitive)

    Number of states

    More

    Fewer

    Response speed

    Slower

    Faster

    Implementation

    Output logic tied to state register

    Output logic tied to transition logic

    4. Summary

    When classified according to structure, finite state machines are divided into:

    Moore Machine – output depends only on the state.

    Mealy Machine – output depends on both the state and the input.

    Both are widely used in digital logic design, embedded systems, and control circuits.
    The choice between them depends on design priorities — simplicity and stability (Moore) or compactness and responsiveness (Mealy).