• Home
  • Q&A
  • Programmer, development system
  • What is OLEDoS?

    * Question

    What is OLEDoS?

    * Answer

    OLEDoS stands for OLED on Silicon, a display technology that integrates an organic light-emitting diode (OLED) display layer directly onto a silicon-based backplane rather than a traditional glass substrate.

    This approach enables ultra-high-resolution, compact, and high-brightness displays, making OLEDoS a key component in microdisplay applications such as augmented reality (AR), virtual reality (VR), and wearable optics.

    1. Basic Principle

    An OLEDoS display operates on the same fundamental principle as a conventional OLED:

    Each pixel contains organic materials that emit light when an electric current passes through.

    Because OLEDs are self-emissive, no backlight is required — resulting in excellent contrast, deep blacks, and high efficiency.

    The difference lies in the substrate:

    Conventional OLED → fabricated on glass or plastic for large panels (like TVs or smartphones).

    OLEDoS → fabricated on a silicon wafer, allowing integration of driving circuits directly beneath the pixels.

    2. Structure of OLEDoS

    An OLEDoS device consists of three major layers:

    Silicon Backplane

    Contains CMOS circuits that control each individual pixel (current drivers, switches, etc.).

    Provides precise electrical control for high refresh rates and pixel uniformity.

    OLED Emissive Layer

    Thin organic layers that generate red, green, and blue light through electroluminescence.

    Encapsulation and Optics

    A protective layer seals the organic material.

    Additional optics (lenses, prisms) are added for magnification or projection in AR/VR systems.

    3. Key Features

    Feature

    Description

    High Resolution

    Can achieve >4000 PPI (pixels per inch), far higher than smartphone OLEDs.

    Compact Size

    Silicon backplane allows microdisplay sizes of less than 1 inch diagonal.

    Fast Response

    OLED’s inherent microsecond response time supports smooth AR/VR motion.

    High Contrast Ratio

    True blacks since pixels emit light individually.

    Low Power Consumption

    No backlight needed; efficient for portable applications.

    4. Main Applications

    OLEDoS is mainly used in microdisplays where small size and high pixel density are essential:

    AR and VR headsets (Apple Vision Pro, Sony, Meta Quest prototypes)

    Head-Up Displays (HUDs) in vehicles or avionics

    Electronic viewfinders in cameras

    Wearable displays and smart glasses

    5. Comparison: OLEDoS vs. MicroLED on Silicon (LEDoS)

    Feature

    OLEDoS (OLED on Silicon)

    LEDoS (MicroLED on Silicon)

    Light Source

    Organic materials

    Inorganic LEDs

    Brightness

    Moderate (≤5,000 nits typical)

    Very high (>10,000 nits possible)

    Efficiency

    Good

    Excellent

    Lifetime

    Shorter (organic aging)

    Longer

    Maturity

    Commercially available

    Emerging technology

    Cost

    Lower

    Higher (currently)

    6. Industry Landscape

    Leading companies developing or producing OLEDoS technology include:

    Sony – pioneer in micro OLED panels for EVFs and AR/VR.

    eMagin (acquired by Samsung Display) – AR/VR microdisplay innovator.

    BOE, SeeYA, Olightek, and Kopin – active in China’s microdisplay sector.

    Apple – reportedly uses Sony’s OLEDoS panels in the Vision Pro headset.

    7. Summary

    OLEDoS (OLED on Silicon) is a microdisplay technology that combines the visual quality of OLED with the precision control of a silicon backplane.
    It offers ultra-high resolution, fast response, and compact form factor, making it ideal for AR/VR and wearable applications.
    While MicroLED-on-silicon (LEDoS) may eventually surpass it in brightness and longevity, OLEDoS remains the most mature and commercially viable microdisplay solution today.