• Home
  • QUESTIONS & ANSWERS
  • Others
  • What conditions do TL loops need to meet?

    * Question

    What conditions do TL loops need to meet?


    *
    Answer

    (1) The T1 loop is a closed loop in which birds have an even number (at least two) of positively polarized junctions (not shown in the figure).

    (2) In the TL loop, the number of forward-biased emitters arranged in the clockwise direction (CW) must be equal to the number of positive-polarized emitters arranged in the counterclockwise direction (CCW).


    COMMENTS

    WORDPRESS: 0
    DISQUS: 0