• Home
  • Q&A
  • Power Supplies - Board Mount
  • What three conditions does the UCC28610 need to start the next cycle modulator?

    * Question

    What three conditions does the UCC28610 need to start the next cycle modulator?

    * Answer

    The UCC28610 from Texas Instruments is a quasi-resonant flyback controller designed for high-efficiency, low-standby AC/DC power supplies.
    Its control logic uses a cycle-by-cycle modulation scheme, and before it can initiate the next switching cycle, three critical conditions must be satisfied.
    These conditions ensure that energy transfer, timing, and control remain stable throughout the converter’s operation.

    1. Transformer Demagnetization Must Be Complete

    Before the next MOSFET turn-on event, the transformer core must be fully demagnetized — meaning the secondary current has decayed to zero.

    The controller monitors the demagnetization signal via the auxiliary winding.

    When the auxiliary winding voltage rises above the demagnetization threshold (VDEMAG), it confirms the core has reset.

    Purpose:
    Ensures all stored magnetic energy from the previous cycle has been delivered to the load, preventing core saturation and enabling valley switching for higher efficiency and lower EMI noise.

    2. The Control Voltage (VCOMP) Must Exceed the Minimum Threshold

    The COMP pin provides the internal control voltage output from the error amplifier, which represents the system’s power demand.

    The UCC28610 compares VCOMP to an internal minimum threshold (VCS_MIN).

    If VCOMP is above this level, it indicates that output regulation requires a new energy pulse.

    If it is below, the controller holds off switching — entering skip-cycle mode at light load to save power.

     Purpose:
    Prevents unnecessary switching during low-load or standby conditions, improving efficiency and reducing standby power consumption.

    3. The Maximum Off-Time (TOFF(MAX)) Must Expire

    The controller imposes a maximum off-time limit to control the lowest switching frequency.
    Even if the first two conditions are met, the UCC28610 waits until the internal frequency clamp timer expires before allowing the next turn-on.

    Purpose:
    Maintains frequency stability across wide load and input ranges and prevents the switching frequency from dropping too low under heavy load or high-line operation.

    Summary Table

    Condition

    Signal/Parameter

    Purpose

    1. Transformer demagnetized

    Auxiliary voltage above VDEMAG

    Ensures full energy transfer and valley switching

    2. Control voltage above minimum

    VCOMP > VCS_MIN

    Indicates load demand and avoids idle switching

    3. Maximum off-time expired

    TOFF(MAX) timer complete

    Keeps switching frequency within safe range

    Conclusion

    In summary, the UCC28610 initiates the next modulation cycle only when:

    The transformer is fully demagnetized,

    The control voltage exceeds the minimum threshold, and

    The maximum off-time period has elapsed.

    This coordinated control ensures high efficiency, low EMI, and stable quasi-resonant operation, making the UCC28610 ideal for flyback power supplies in industrial, communication, and consumer applications.