* Question
What are the main parameters of the humidity sensitive Resistors?
* Answer
Table of Contents
Toggle1) Nominal resistance R0R_0
Definition: Resistance under specified conditions (typically 25 °C, 60 %RH, defined test voltage/frequency).
Typical range: 10 kΩ to 1 MΩ.
Measurement note: Prefer AC excitation (e.g., 0.1–1 Vrms, 1–10 kHz) to avoid DC polarization and self-heating.
2) Humidity operating range & resolution
Range: Commonly 20–95 %RH (or wider).
Resolution: Set by your readout/ADC and curve slope; the sensor has no fixed “step size.”
Tip: Emphasize effective resolution under real conditions (temperature, airflow), not the theoretical ADC bits.
3) Sensitivity / humidity coefficient
Definition: Relative resistance change per %RH, e.g.
S=ΔR/R0/ΔRH or d(logR)/dRH
Behavior: Generally monotonic, often log/exponential; use a calibrated transfer curve (linear/quadratic/log fits).
4) Linearity / nonlinearity
Definition: Max deviation from best-fit curve, usually as % of full scale.
Typical: ±1–±3 %FS. Lower nonlinearity simplifies calibration.
5) Accuracy & repeatability
Accuracy: Error vs. reference at specified points (e.g., 25 °C, several RH points).
Repeatability: Short-term standard deviation over repeats.
Typical: Accuracy ±2–±5 %RH; repeatability better than ±1 %RH.
6) Hysteresis (adsorption/desorption)
Definition: Difference between up-sweep and down-sweep at the same RH.
Typical: 1–3 %RH. Polymer elements often show more hysteresis than some ceramic/glassy types.
Tip: For applications with oscillating RH, prioritize low hysteresis.
7) Response / recovery time
Definition: t90 to reach 90 % of a step change (humidifying / dehumidifying).
Typical: Seconds to tens of seconds; protective membranes slow it down.
Specify test conditions: 25 °C, airflow (e.g., 1 m/s).
8) Temperature effect (TCR at constant RH) & temperature range
TCR: Drift at fixed RH vs. temperature, in %/°C or ppm/°C.
Operating range: e.g., −20 to +60 °C; exceeding it can age the sensing film.
Compensation: Use a co-located temperature sensor and 2-D compensation (RH & T).
9) Long-term stability / drift
Definition: Change in zero/slope over time (e.g., 1000 h, 1 year).
Typical: ≤ ±1–±2 %RH/year in benign environments.
Practice: Plan periodic calibration for critical uses.
10) Excitation & maximum measuring power
Prefer AC drive; DC can cause electrolysis/ion migration → drift & hysteresis.
Limit current/voltage (e.g., ≤ 10–50 µA) to avoid self-heating.
11) Cross-sensitivity & environmental robustness
Cross-sensitivities: Organic solvents, acidic/alkaline gases, silicones, dust.
Condensation: Causes temporary errors; use hydrophobic, breathable membranes and anti-fog/anti-condensation strategies.
12) Package / protection
Forms: SMD, probe, vented packages with membranes.
Trade-off: Better protection → slower response.
Selection & application notes
Target band: If the application lives in 30–80 %RH, optimize accuracy and hysteresis in that band.
Temperature compensation: Pair with a temperature sensor; build a 2-D calibration table.
Readout circuits:
AC drive + bridge / transimpedance / divider → ADC, keeping sensor power tiny.
Or current source + sense resistor, again minimizing dissipation.
Calibration: Use saturated salt solutions at 25 °C to generate reference RH points (typical values):
LiCl ≈ 11 %, MgCl₂ ≈ 33 %, Mg(NO₃)₂ ≈ 54 %, NaCl ≈ 75 %, KCl ≈ 85 %, K₂SO₄ ≈ 97 %. Record temperature.
Maintenance: Define reconditioning/drying steps and re-calibration intervals (e.g., every 6–12 months).
Quick reference table (example values)
Parameter | Typical value | Notes |
Nominal R0R_0 | 100 kΩ @ 25 °C, 60 %RH | AC 1 kHz, 0.5 Vrms |
Operating range | 20–95 %RH; −20 to +60 °C | Avoid condensation |
Accuracy | ±3 %RH (25 °C) | Often better in mid-range |
Linearity | ±2 %FS | Vs. best-fit curve |
Hysteresis | 1–3 %RH | Up vs. down sweep |
Response/ recovery | 10–30 s / 20–60 s | t90; membrane dependent |
Temp coefficient | 0.05–0.2 %RH/°C | Needs compensation |
Drift | ≤ ±1 %RH/year | Typical environment |
Excitation | AC 0.1–1 Vrms, 1–10 kHz | Low power, low self-heat |
One-line takeaway: Specify and validate sensitivity curve, hysteresis, temperature effects, long-term drift, and safe excitation limits—with clear test/calibration conditions—and you’ll have a sensor that’s both accurate and durable in the field.

COMMENTS