• Home
  • Q&A
  • Others
  • Why is the current digital oscilloscope level not enough to completely replace the analog oscilloscope?

    * Question

    Why is the current digital oscilloscope level not enough to completely replace the analog oscilloscope?

    * Answer

    Even though digital storage oscilloscopes (DSOs) dominate today’s labs, analog oscilloscopes are not fully obsolete. Here’s why the current digital technology still doesn’t completely replace analog scopes:

    1. Real-Time Display vs. Processed Display

    Analog oscilloscopes display the signal directly as it is, in real time, because the input drives the CRT (cathode ray tube) without intermediate processing.

    Digital oscilloscopes first digitize the signal (ADC), store it in memory, then reconstruct it on the screen.

    Result: For very fast or unpredictable transients, analog scopes can still feel more “live” and natural, whereas digital scopes may show aliasing, missed spikes, or interpolated waveforms.

    2. Response to Transients

    Analog scopes instantly show fast glitches or brief anomalies if they occur, because the beam responds continuously.

    Digital scopes rely on sampling rate and memory depth. If a glitch happens between samples, it can be missed unless advanced triggering or very high sample rates are used.

    3. Signal Integrity & Display Smoothness

    Analog scopes inherently show a continuous, smooth waveform, with natural intensity grading (bright where the beam lingers, dim where it’s rare).

    Digital scopes display discrete data points, often connected by interpolation. This can introduce artifacts, making subtle waveform details less obvious.

    4. Latency and “Feel”

    On an analog scope, what you see is truly instantaneous, directly tied to the probe input.

    On digital scopes, there is always some processing delay, even if very small, which can affect real-time intuition when tuning analog circuits.

    5. Cost and Simplicity in Certain Use Cases

    Analog scopes are simpler, cheaper (second-hand), and don’t require menus, storage depth, or firmware.

    For quick classroom demonstrations or basic troubleshooting, some engineers still find them more intuitive.

    Summary Table

    Aspect

    Analog Oscilloscope

    Digital Oscilloscope

    Real-time display

    Continuous, instantaneous

    Sampled, reconstructed

    Transient/glitch capture

    Naturally visible (if within bandwidth)

    Requires high sample rate/trigger sophistication

    Waveform “look”

    Smooth, intensity-graded

    Discrete, may show artifacts/interpolation

    Latency

    Zero (direct electron beam)

    Some processing delay

    User experience

    Intuitive, direct

    More features but more complex menus

    Insight

    Modern DSOs are far more powerful overall (deep memory, advanced math, FFTs, storage, multi-channel), but analog scopes still offer unmatched immediacy and fidelity for real-time, fast-changing signals. That’s why in precision analog debugging or transient visualization, some engineers still keep an analog scope on the bench.