• Home
  • QUESTIONS & ANSWERS
  • Programmer, development system
  • What are the steps in the inkjet process for inkjet printers using piezoelectric technology?

    * Question

    What are the steps in the inkjet process for inkjet printers using piezoelectric technology?

    * Answer

    Inkjet printers that use piezoelectric technology follow a precise and controlled process to deposit ink droplets onto a substrate (such as paper or flexible electronics). Here’s a detailed breakdown of the steps involved in the piezoelectric inkjet printing process:

    1. Ink Supply and Preparation

    Ink is stored in a reservoir and delivered to the piezoelectric printhead.

    The ink must meet specific criteria:

    Viscosity and surface tension suitable for droplet formation.

    Nozzle-compatible (non-clogging, chemically stable).

    Filtered to remove particles that could block the nozzles.

    2. Electrical Pulse to Piezoelectric Actuator

    A voltage pulse is applied to a piezoelectric crystal or element located behind the ink chamber in each nozzle.

    This causes the piezoelectric material to deform (bend or flex) rapidly, which either:

    Compresses the ink chamber (push mode), or

    Expands the chamber (pull mode), depending on the printhead design.

    3. Ink Droplet Ejection

    The mechanical deformation from the piezo element creates pressure, forcing a tiny ink droplet out through the nozzle.

    The volume and velocity of the droplet are precisely controlled by:

    Voltage amplitude

    Pulse duration

    Frequency of pulses

    4. Droplet Flight

    The ejected ink droplet travels through the air toward the substrate.

    During flight:

    Some systems use charge control or aerospace correction to improve accuracy.

    Trajectory is maintained by carefully controlled jetting angle and environmental conditions.

    5. Droplet Deposition

    The droplet lands on the designated location on the substrate (paper, plastic film, PCB, etc.).

    The position is governed by:

    Printhead movement (usually via a carriage or a moving substrate platform).

    Software-controlled rasterization and printing instructions.

    6. Ink Drying or Curing

    Once the droplet is deposited, the ink undergoes:

    Evaporation (for water-based inks),

    UV curing (for UV-curable inks), or

    Thermal baking (in printed electronics).

    This step ensures adhesion, durability, and color stability.

    Summary: Steps in Piezoelectric Inkjet Printing

    Step

    Description

    1. Ink Supply

    Ink is filtered and fed to the nozzle chamber

    2. Electrical Activation

    Voltage pulse deforms piezoelectric actuator

    3. Droplet Ejection

    Actuation forces ink droplet out of the nozzle

    4. Droplet Flight

    Droplet travels toward substrate with controlled trajectory

    5. Deposition

    Ink lands precisely at target point on the substrate

    6. Drying/Curing

    Ink is solidified or fixed to ensure performance and stability

    Additional Notes:

    Piezoelectric inkjet printing is non-thermal, unlike thermal bubble inkjet systems.

    It allows the use of a wider range of inks, including solvent-based, pigment-based, and functional inks (e.g., conductive, biological).

    It’s widely used in industrial printing, printed electronics, bio-printing, and graphic arts.

    COMMENTS

    WORDPRESS: 0
    DISQUS: 0