• Home
  • QUESTIONS & ANSWERS
  • Others
  • What is included in the CPU Interrupt Enable Register?

    * Question

    What is included in the CPU Interrupt Enable Register?

    * Answer

    The CPU Interrupt Enable Register (often abbreviated as IE or INT_EN) is a special control register within a CPU or microcontroller that determines which interrupts are allowed to trigger the processor’s interrupt handling mechanism. Here’s a detailed breakdown of what it typically includes:

    Overview: What Is the CPU Interrupt Enable Register?

    The Interrupt Enable Register is used to mask (disable) or unmask (enable) specific interrupt sources. By setting or clearing bits in this register, software can control which peripheral or system events are allowed to interrupt the CPU.

    It plays a central role in interrupt-driven systems, where events like timer overflows, external signals, or UART data reception need to be handled immediately by interrupt service routines (ISRs).

    Typical Contents of an Interrupt Enable Register

    The exact layout depends on the CPU architecture (e.g., ARM Cortex-M, x86, AVR, MIPS, RISC-V), but generally includes bit fields for each interrupt source:

    Bit Position

    Name

    Description

    Bit 0

    INT0_EN or TIMER0_IE

    Enables interrupt from external pin 0 or Timer 0 overflow

    Bit 1

    INT1_EN or TIMER1_IE

    Enables interrupt from external pin 1 or Timer 1

    Bit 2

    UART_RX_IE

    Enables UART receive interrupt

    Bit 3

    UART_TX_IE

    Enables UART transmit complete interrupt

    Bit 4

    ADC_IE

    Enables ADC (Analog-to-Digital Converter) conversion complete interrupt

    Bit 5

    GPIO_IE

    Enables GPIO port change or pin interrupt

    Bit 6

    I2C_IE

    Enables I2C-related interrupts (e.g., bus activity or data received)

    Bit 7

    SPI_IE

    Enables SPI transmission/reception complete interrupt

    These bits are writeable, and:

    Setting a bit to 1 enables that interrupt source.

    Setting a bit to 0 disables it.

    Global Interrupt Enable

    Some CPUs (especially microcontrollers) include a global interrupt enable bit, often outside this register:

    In AVR: Bit I in the SREG (Status Register)

    In ARM Cortex-M: PRIMASK register controls global interrupt masking

    In x86: IF (Interrupt Flag) in the EFLAGS register

    This global bit must also be set to allow any interrupt to be acknowledged by the CPU.

    Example: 8051 Interrupt Enable Register (IE)

    For the Intel 8051 microcontroller family, the IE register layout is as follows:

    | EA | — | ET2 | ES | ET1 | EX1 | ET0 | EX0 |

    EA: Global enable/disable for all interrupts

    ET0, ET1, ET2: Timer 0, 1, 2 interrupt enables

    EX0, EX1: External interrupts 0 and 1

    ES: Serial port interrupt enable

    Usage in Code

    In embedded C:

    IE |= 0x01;  // Enable external interrupt 0

    IE &= ~0x08; // Disable serial port interrupt

    In ARM CMSIS:

    NVIC_EnableIRQ(UART0_IRQn);   // Enable UART0 interrupt

    NVIC_DisableIRQ(TIMER1_IRQn); // Disable Timer1 interrupt

    Summary

    The CPU Interrupt Enable Register includes:

    Individual bits for enabling/disabling specific interrupt sources

    Often tied to peripherals like timers, UART, ADC, GPIO, etc.

    Works alongside a global interrupt enable flag

    Allows fine-grained control over what events are allowed to interrupt the CPU

    It is a critical component in designing responsive embedded systems and is typically configured during system initialization or as part of dynamic interrupt control.