• Home
  • QUESTIONS & ANSWERS
  • Others
  • How to set the DC Master communication area?

    * Question

    How to set the DC Master communication area?

    * Answer

    To set the DC Master communication area, you need to define and configure the memory regions used for exchanging data between the master and its connected slaves. This communication area is crucial for real-time, deterministic control in distributed systems, such as motion controllers using EtherCAT or similar fieldbuses.

    1. Understanding the DC Master Communication Area

    The DC Master communication area typically consists of:

    Send Area (Output): Master writes data to this area; slaves read from it.

    Receive Area (Input): Slaves write data here; master reads it.

    These areas are mapped in the master’s memory and used for cyclic process data exchange. Each area must be:

    Predefined in size

    Correctly aligned in memory

    Consistently structured to match slave devices’ data expectations

    2. Configuration Steps (Generic Process)

    Step 1: Define Buffer Sizes

    Determine the number of bytes needed for input and output data.

    c

    #define SEND_AREA_SIZE   128   // e.g., 128 bytes for outputs#define RECV_AREA_SIZE   128   // e.g., 128 bytes for inputs

    Step 2: Allocate Memory

    Allocate buffers for the send and receive areas.

    c

    uint8_t sendArea[SEND_AREA_SIZE];uint8_t recvArea[RECV_AREA_SIZE];

    Step 3: Set Communication Area in Master Configuration

    If you’re using a DC Master API (e.g., via C/C++), use functions provided by the SDK:

    c

    DCMaster_SetSendArea(sendArea, SEND_AREA_SIZE);

    DCMaster_SetReceiveArea(recvArea, RECV_AREA_SIZE);

    For platforms like EtherCAT:

    Use the configuration tool (e.g., TwinCAT, SOEM, Codesys) to map PDOs (Process Data Objects) into the communication memory.

    Step 4: Map Slaves’ Process Data

    Assign each slave’s input/output to specific offsets within the send/receive areas.

    c

    // Example: Set 16 bytes to Slave 1 output starting at offset 0

    DCMaster_MapOutput(slaveID = 1, offset = 0, size = 16);

    Step 5: Activate Cyclic Communication

    Start the DC Master’s real-time loop:

    c

    DCMaster_Start();

    3. Example in EtherCAT Context

    If you are using EtherCAT with DC synchronization:

    The communication area is configured by:

    Mapping RxPDOs (outputs) and TxPDOs (inputs)

    Setting memory offsets and data size

    In TwinCAT:

    Open I/O configuration

    Select slave device → Map PDO entries → Assign to variables

    Link to memory (e.g., Global Variable List)

    4. Best Practices

    Practice

    Reason

    Ensure proper memory alignment

    Required for some DMA-capable masters

    Match slave data layout

    Prevents misinterpretation of control/status bytes

    Use fixed offsets

    Simplifies debugging and slave data access

    Use watchdogs/timeouts

    Increases system safety if communication fails

    Summary

    To set the DC Master communication area, you must:

    Define input/output buffer sizes

    Allocate and assign memory

    Map each slave’s data to a specific location

    Use master SDK or configuration tools to initialize and start communication

    This setup ensures fast, synchronized exchange of control and feedback data in real-time applications such as robotics, CNC, or industrial automation.

    COMMENTS

    WORDPRESS: 0
    DISQUS: 0