• Home
  • QUESTIONS & ANSWERS
  • Integrated Circuits (ICs)
  • What are the important registers of the MSCAN module?

    * Question

    What are the important registers of the MSCAN module?

    * Answer

    The MSCAN (Multifunctional Serial Communication Controller) module is commonly used in microcontrollers for CAN (Controller Area Network) communication. It includes various registers that control and configure the operation of the CAN bus. Below are the important registers associated with the MSCAN module:

    1. MSCAN Control Register (MCR)

    Purpose: Configures the overall behavior of the MSCAN module.

    Key Bits:

    MCR[LOM]: Listen-Only Mode

    MCR[STM]: Self-Test Mode

    MCR[FRZ]: Freeze Mode

    MCR[TX]: Transmit Enable

    MCR[RX]: Receive Enable

    2. MSCAN Status Register (MSR)

    Purpose: Provides information about the current status of the MSCAN module.

    Key Bits:

    MSR[IDLE]: CAN Bus Idle Flag

    MSR[BUSY]: CAN Bus Busy Flag

    MSR[ERROR]: Error Flag

    MSR[RX]: Receive Flag

    MSR[TX]: Transmit Flag

    MSR[OVR]: Overrun Flag

    3. MSCAN Transmit Buffer Register (MTB)

    Purpose: Holds the data to be transmitted via the CAN bus.

    Key Bits:

    Data bytes that will be transmitted on the CAN bus.

    This register is typically written to in order to queue a message for transmission.

    4. MSCAN Receive Buffer Register (MRB)

    Purpose: Holds the data received from the CAN bus.

    Key Bits:

    Data bytes that have been received on the CAN bus are stored here.

    Typically read to retrieve incoming CAN messages.

    5. MSCAN Error Counter Register (ECR)

    Purpose: Keeps track of the number of transmission errors.

    Key Bits:

    ECR[TEC]: Transmit Error Counter

    ECR[REC]: Receive Error Counter

    The error counters help in determining if the module is in an error state and assist in error management and diagnostics.

    6. MSCAN Bit Timing Register (BTR)

    Purpose: Configures the timing parameters for the CAN communication.

    Key Bits:

    BTR[BRP]: Baud Rate Prescaler

    BTR[TSEG1]: Time Segment 1

    BTR[TSEG2]: Time Segment 2

    BTR[SJW]: Synchronization Jump Width

    These bits configure the baud rate and timing for CAN communication, allowing for proper synchronization between CAN nodes.

    7. MSCAN Interrupt Enable Register (IE)

    Purpose: Enables or disables interrupt sources for the MSCAN module.

    Key Bits:

    IE[RXF]: Receive FIFO Interrupt Enable

    IE[TXF]: Transmit FIFO Interrupt Enable

    IE[ERR]: Error Interrupt Enable

    IE[IDLE]: Idle Interrupt Enable

    These bits allow the user to enable or disable interrupts for various events (e.g., receive buffer full, transmit buffer empty, etc.).

    8. MSCAN Acceptance Mask Register (AMR)

    Purpose: Configures the message acceptance filter to define which messages are allowed based on their identifier.

    Key Bits:

    AMR[AM]: Acceptance Mask for filtering identifiers.

    The AMR allows for filtering CAN messages, making it possible to only receive specific messages (those with matching identifiers).

    9. MSCAN Identifier Registers (ID)

    Purpose: Stores the CAN message identifiers (both standard and extended) used for filtering and transmitting.

    Key Bits:

    ID[SID]: Standard Identifier (11 bits for standard CAN frames)

    ID[XID]: Extended Identifier (29 bits for extended CAN frames)

    10. MSCAN Control/Status Register (CSR)

    Purpose: This register provides control over certain features of the MSCAN module, such as enabling/disabling specific transceiver features and status flags.

    Key Bits:

    CSR[TX]: Transmit Command

    CSR[RX]: Receive Command

    CSR[FP]: Freeze Mode

    CSR[DP]: Data Phase

    11. MSCAN Timer Register (TMR)

    Purpose: Allows the configuration of timers used by the MSCAN module for various timing-related tasks.

    Key Bits:

    TMR[TM]: Timer Mode (configures timer settings)

    TMR[TO]: Timeout Value (sets a timeout for CAN operations)

    12. MSCAN Global Control Register (GCR)

    Purpose: Configures global settings for the CAN controller, including the operation mode (e.g., normal, silent, loopback).

    Key Bits:

    GCR[SYN]: Synchronization Bit (synchronizes the MSCAN with the external CAN bus)

    GCR[LOOP]: Loopback Mode Enable

    GCR[SIL]: Silent Mode Enable

    Summary of Key Registers:

    MCR (Control)

    MSR (Status)

    MTB (Transmit Buffer)

    MRB (Receive Buffer)

    ECR (Error Counters)

    BTR (Bit Timing)

    IE (Interrupt Enable)

    AMR (Acceptance Mask)

    ID (Identifier)

    CSR (Control/Status)

    TMR (Timer)

    GCR (Global Control)

    Each register is used to configure different parts of the MSCAN controller to ensure proper operation of the CAN communication, including message filtering, error handling, interrupt management, and timing control.