* Question
What is the detection method of the electromagnetic pulse type crank position sensor?
* Answer
Table of Contents
ToggleDetection Method of Electromagnetic Pulse Type Crank Position Sensor
An electromagnetic pulse type crank position sensor (also called a variable reluctance sensor (VRS) or magnetic pickup sensor) detects the rotational position and speed of a crankshaft using electromagnetic induction. This type of sensor is commonly used in internal combustion engines for ignition timing and fuel injection control.
Detection Principle
Magnetic Field Generation
- The sensor consists of a permanent magnet, a coil winding, and a soft iron core.
- The permanent magnetproduces a magnetic field around the coil.
Reluctance Variation & Induced Voltage
- A toothed reluctor wheel (trigger wheel)is attached to the crankshaft and rotates past the sensor.
- As each tooth approaches and passes the sensor, it changes the magnetic fluxthrough the coil.
- This change in magnetic flux induces a voltage pulsein the coil based on Faraday’s Law of Electromagnetic Induction.
Generating a Sinusoidal Signal
- When a toothapproaches the sensor, the magnetic field strengthens, causing a positive voltage spike.
- When the tooth alignswith the sensor, the voltage momentarily stabilizes.
- As the tooth moves away, the magnetic field weakens, producing a negative voltage spike.
- This results in an AC sine wave signalwhose frequency corresponds to the crankshaft’s rotational speed.
Signal Processing & Use
- The Engine Control Unit (ECU)processes the AC signal to determine:
- Crankshaft Position– By identifying specific reference points (e.g., missing teeth).
- Engine Speed (RPM)– The frequency of the AC signal correlates with rotational speed.
- Ignition & Fuel Timing– The ECU synchronizes ignition and fuel injection with crankshaft rotation.
Advantages of Electromagnetic Pulse Type Sensors
✔ No External Power Required – Self-generating AC signal.
✔ High Durability – Works well in harsh environments (dust, oil, heat).
✔ Reliable at High Speeds – Effective in high-RPM applications.
Limitations
❌ Signal Weak at Low Speeds – Induced voltage is low when the crankshaft turns slowly.
❌ Susceptible to Interference – External magnetic fields or nearby electrical noise can affect accuracy.
❌ Requires Precise Alignment – Improper gap between the sensor and reluctor wheel can lead to weak signals or misfires.
Comparison with Hall Effect Crank Sensors
Feature | Electromagnetic Pulse Sensor | Hall Effect Sensor |
Signal Type | AC Sine Wave | Digital (Square Wave) |
Low-Speed Detection | Weak | Strong |
Power Requirement | No External Power | Requires Power Supply |
Noise Immunity | Lower (susceptible to EMI) | Higher (less affected by EMI) |
Durability | High | High |
Applications
- Found in older and modern internal combustion engines(used for ignition and fuel injection).
- Common in automotive, motorcycles, aircraft engines, and industrial machinery.
This type of crank position sensor remains popular due to its simplicity, durability, and effectiveness in high-speed applications.

COMMENTS