* Question
What conditions must the device meet in order to comply with the PMBus specification?
* Answer
The PMBus (Power Management Bus) specification defines a communication protocol and standards for power management devices. To comply with the PMBus specification, a device must meet the following conditions:
1. Compatibility with SMBus
– PMBus is built on the System Management Bus (SMBus) protocol, which itself is based on I²C. The device must:
– Use I²C-compatible hardware for communication.
– Support SMBus timing and electrical specifications, such as clock speed (typically up to 400 kHz).
– Support SMBus-specific features like bus arbitration and clock stretching.
2. Support for PMBus Commands
– The device must implement PMBus-defined commands and adhere to their functional descriptions. These include:
– Standard Commands: Such as `READ_VOLTAGE`, `READ_CURRENT`, `WRITE_PROTECTION`.
– Manufacturer-Specific Commands: Optional commands that extend the functionality while following PMBus rules.
– It must respond correctly to mandatory commands defined in the PMBus specification.
3. Addressing
– Must support 7-bit addressing as specified in SMBus/I²C standards.
– The device must have a unique address and potentially allow dynamic address assignment if required.
4. Data Formats
– Support the specific data encoding formats defined by PMBus, including:
– Linear Data Format: A two-byte representation for parameters like voltage and current.
– Direct Data Format: Values directly related to physical quantities.
– VID Data Format: Voltage Identification encoding for processors.
5. Timing Requirements
– Must adhere to SMBus timing specifications for:
– Clock stretching.
– Data hold and setup times.
– Start and stop conditions.
6. Error Handling
– Must implement error detection and handling mechanisms, including:
– PEC (Packet Error Checking): Optional but recommended for ensuring data integrity.
– Timeout for bus communication as specified in SMBus standards.
7. Device Capabilities and Identification
– The device must support commands to query its capabilities, such as:
– Supported features and command sets.
– Manufacturer identification via `MFR_ID` and `MFR_MODEL`.
8. Alert and Fault Handling
– The device should support PMBus-defined fault handling and reporting mechanisms, such as:
– Generating alerts for overvoltage, overcurrent, or temperature events.
– Using the `ALERT` pin for fault reporting, following SMBus alert standards.
9. Optional Features
– While not mandatory, the device may support advanced PMBus features, such as:
– Group command protocols for simultaneous updates.
– Dynamic bus frequency adjustment.
– Synchronization with multiple PMBus devices.
10. Interoperability
– The device must work seamlessly with other PMBus-compliant devices on the same bus.
– Ensure backward compatibility with SMBus/I²C to avoid conflicts in mixed environments.
Summary
To comply with the PMBus specification, a device must support its communication protocol, timing requirements, data formats, standard commands, and fault/error handling mechanisms. Additionally, it should maintain compatibility with SMBus/I²C and ensure robust and interoperable operation in multi-device environments.

COMMENTS