• Home
  • QUESTIONS & ANSWERS
  • Integrated Circuits (ICs)
  • Which four different information frames does CAN define?

    * Question

    Which four different information frames does CAN define?

    * Answer

    The CAN (Controller Area Network) protocol defines four types of frames to facilitate communication between nodes. Each frame serves a specific purpose in the CAN network. Here are the four different information frames defined by CAN:

    1. Data Frame
    – Purpose: To transmit data from one node to another in the network.
    – Details:
    – Contains actual data payload (up to 8 bytes in Classical CAN or up to 64 bytes in CAN FD).
    – Includes fields such as the identifier, control bits, data length, and a CRC for error detection.

    2. Remote Frame
    – Purpose: To request data from another node without transmitting data itself.
    – Details:
    – Similar to the Data Frame but with no data field (data length is specified as 0).
    – Contains the identifier of the requested data frame.
    – Typically used in applications where one node queries another for specific information.

    3. Error Frame
    – Purpose: To signal errors detected on the network by any node.
    – Details:
    – Triggered when a node detects a communication error (e.g., CRC mismatch or bit stuffing error).
    – Contains error flags and other error-specific information.
    – Helps maintain network integrity by notifying all nodes of an issue.

    4. Overload Frame
    – Purpose: To provide additional time for a node to process data or handle internal conditions.
    – Details:
    – Generated when a node is overwhelmed and cannot process the next frame immediately.
    – Contains overload flags and is sent during inter-frame spaces.
    – Rarely used in modern systems as most controllers handle data efficiently.

    These frame types ensure that the CAN protocol supports robust communication, including data transfer, error handling, and network synchronization.