* Question
What are the requirements for 0LED for conductive glass? |
* Answer
The flatness of IT0 is first required to ensure complete contact between the IT0 electrode and the organic layer.In addition, the resistivity should be small, and the sheet resistance is preferably less than 10 彤, so as to ensure that the power consumed on the ITO electrode is not too large in a high-resolution device. |
COMMENTS