• Home
  • QUESTIONS & ANSWERS
  • Sensors, Transducers
  • What is self-exciting field?

    * Question

    What is self-exciting field?

    * Answer

    A self-exciting field is a concept commonly associated with electrical generators, particularly in the context of alternators. This term refers to the method by which a generator can generate its own field excitation without requiring an external power source. Here’s how it generally works:

    1. Initial Magnetism: Small amounts of residual magnetism in the generator’s iron core provide an initial magnetic field. Even when the generator is off, these remnants can be enough to start the process.

    2. Voltage Generation: As the generator starts, the rotor (which may still have this residual magnetism) begins to spin, cutting through magnetic lines of force and inducing an initial voltage in the armature.

    3. Excitation Buildup: This small voltage is fed back to the field windings of the generator, strengthening the magnetic field. This increased field results in a higher induced voltage, which in turn further strengthens the magnetic field. This feedback loop continues until the generator reaches its full operating capacity.

    4. Stabilization: Once the generator reaches a sufficient level of excitation, additional controls and regulators (like automatic voltage regulators) maintain the field strength to ensure stable operation of the generator.

    Self-exciting generators are particularly valued for their independence from external power sources, making them suitable for remote or backup power applications where reliability and self-sufficiency are critical.

    COMMENTS

    WORDPRESS: 0
    DISQUS: 0