• Home
  • Q&A
  • Sensors, Transducers
  • What is the Hall effect?

    * Question

    What is the Hall effect?

    * Answer

    The Hall effect is a physical phenomenon discovered by Edwin Hall in 1879. It occurs when a magnetic field is applied perpendicular to the flow of electric current in a conductor or semiconductor. This causes a Lorentz force to act on the charge carriers (such as electrons or holes), which deflects them to one side of the conductor. As a result, a voltage, known as the Hall voltage, is developed across the conductor, perpendicular to both the direction of the magnetic field and the current.

    Key Points About the Hall Effect:

    1. Voltage Creation: The Hall voltage is created due to the separation of charge carriers, which generates an electric field opposing their movement. The magnitude of the Hall voltage is proportional to the strength of the magnetic field and the current, and inversely proportional to the charge carrier density of the material.

    2. Sensor Applications: The Hall effect is widely used in Hall effect sensors, which are used to measure magnetic field strength, fluid flow, and even in position sensing applications (such as in automotive ignition systems and industrial equipment).

    3. Material Characterization: It can also help in determining the type of charge carriers (positive or negative) in a material and their density, which is crucial for semiconductor research and development.

    4. Quantum Hall Effect: At very low temperatures and under strong magnetic fields, the Hall effect can manifest in a quantum mechanical version, where the Hall resistance quantizes into discrete steps. This Quantum Hall Effect has significant implications in the fundamental theories of condensed matter physics.

    The Hall effect has led to a variety of practical applications, including magnetic field measurement and speed detection, as well as providing insights into electronic properties of materials, contributing significantly to advancements in technology and theoretical physics.