• Home
  • Q&A
  • Inductors, Coils, Chokes
  • What is the ripple current?

    * Question

    What is the ripple current?

    * Answer

    The ripple current refers to the alternating current (AC) component superimposed on the direct current (DC) level in electronic circuits, typically seen in the output of power supplies including switch-mode power supplies and regulators. This phenomenon occurs due to incomplete suppression of the alternating waveform within power supplies.

    Key aspects of ripple current include:

    1. Source: It mainly arises from the charging and discharging of the capacitor in the power supply’s filtering stage. During the charging phase, the capacitor absorbs energy, and during the discharge phase, it releases energy, leading to fluctuations in current.

    2. Impact: Ripple current can affect the performance of electronic circuits by inducing noise and interference. High levels of ripple can lead to increased heat in components like capacitors and may reduce their lifespan and reliability.

    3. Measurement and Reduction: It is measured as a peak-to-peak value and is typically expressed in milliamps (mA). Using higher quality, higher capacity capacitors or adding additional filtering stages can effectively reduce ripple current.

    The control and minimization of ripple current are crucial in applications where precision and stability are important, such as in audio equipment, sensitive measurement devices, and communication systems.