![](https://blog.win-source.net/wp-content/uploads/2020/05/73.png)
* Question
What is the reason for the wireless system to adopt the PWM scheme?
* Answer
The adoption of Pulse Width Modulation (PWM) in wireless systems is primarily due to its efficiency in controlling power and its effectiveness in signal processing. Here are some of the key reasons why PWM is used in wireless systems:
1. Power Control: PWM is an excellent method for controlling the power output in transmitters. By adjusting the duty cycle of the PWM signal, the power of the output signal can be effectively controlled. This is particularly useful in power-sensitive applications where managing battery life is crucial.
2. Efficient Use of Energy: PWM allows for the efficient use of energy, as it can minimize power loss in electronic control devices. It achieves this by switching the power at a very high frequency, which can be more efficient than other linear power control methods that may result in higher power dissipation.
3. Signal Modulation: In wireless communications, PWM can be used for modulating the signal that is being transmitted. PWM modulation involves varying the width of the pulses in direct proportion to the amplitude of the analog signal data, thereby encoding the information within the width of the pulses.
4. Reduced Interference and Noise: PWM signals, due to their digital nature, are less susceptible to noise and interference compared to analog signals. This makes PWM a favorable choice in environments where interference and signal degradation are concerns.
5. Simplicity and Cost-Effectiveness: PWM circuits are relatively simple to design and implement, leading to cost-effective solutions in many applications. The technology does not require complex DACs (Digital-to-Analog Converters) for generating analog output if the pulse frequency is sufficiently high, simplifying the system design and reducing costs.
6. Speed Control in Wireless Networks: In applications like wireless networked systems controlling motors (for example, in drones or robotic systems), PWM is used to control the speed of motors efficiently and precisely by adjusting the voltage applied to the motor through the duty cycle of the PWM signal.
7. Compatibility with Digital Systems: Since PWM signals are inherently digital (with only high and low states), they integrate well with other digital components and systems in modern wireless technology, facilitating easier system integration and data processing.
Overall, the use of PWM in wireless systems offers a balance of efficiency, control, simplicity, and compatibility, making it a widely adopted scheme in various wireless communication and control applications.
COMMENTS