The Armstrong Hand Tools 64-352 is a precision-engineered dial-type torque wrench for accuracy and reliability in torque applications. Specifically, this torque wrench features a 3/8″ drive and a torque range from 0 to 250-inch pounds, offering versatility for various mechanical tasks that demand precise torque settings.
Here are the key aspects and features of the Armstrong Hand Tools 64-352:
Precision and Versatility: This torque wrench provides a wide torque range, allowing users to adjust and apply torque settings from 0 to 250-inch pounds with exceptional accuracy. The 3/8″ drive makes it compatible with a range of sockets and fasteners, adding versatility to its applications.
Dial-Type Design: Its dial-type design enables easy reading and adjustment of torque settings, enhancing user convenience during operation. The audible click mechanism signals when the preset torque value is reached, ensuring precise torque application.
Durability and Construction: The Armstrong Hand Tools 64-352 is crafted from sturdy steel and built to withstand demanding industrial or mechanical environments. Its robust construction ensures longevity and reliable performance even under heavy-duty usage.
Accuracy and Calibration: The torque wrench maintains an accuracy of approximately +/- 4% in either direction, providing consistent and reliable torque application. While it may not have a calibration certificate, its micrometer-type mechanism allows precise torque adjustments.
Application: This torque wrench is commonly used in mechanical workshops, automotive repairs, machinery maintenance, and assembly lines. It is suitable for tasks that require accurate and controlled torque application to fasteners, ensuring proper tension without overtightening.
The tool might be known by different names globally, such as Armstrong Industrial Hand Tools or simply Armstrong, depending on the region or distributor.
What is Bessey CLSX?
The Bessey CLSX-SET is a classiX sliding arm bar clamp designed and manufactured by Bessey Tools North America. These clamps are known for their sliding arm mechanism and forged steel handles, which offer robustness and versatility in various clamping applications.
Here are the key aspects and features of the Bessey CLSX-SET:
Sliding Arm Mechanism: The “classiX” series by Bessey typically incorporates a sliding arm design, allowing for easy adjustment of the clamping capacity. This feature enables users to swiftly slide the arm to the desired position, accommodating different workpiece sizes.
Forged Steel Handle: These clamps have handles made from forged steel. Forged steel is known for its strength and durability, ensuring the handles are robust enough to withstand considerable clamping forces without compromising performance.
Clamping Functionality: These bar clamps’ primary function is to securely hold workpieces in place during various woodworking, metalworking, or general assembly tasks. They’re instrumental in applications where a robust and reliable grip is needed.
Applications
Bar clamps like the Bessey CLSX-SET are commonly used in woodworking shops, metalworking facilities, carpentry, and other trades where firmly and precisely securing workpieces is crucial. They’re versatile tools suitable for both professional and DIY applications.
Depending on the region or distributor, Bessey Tools North America might be known globally by different names or aliases.
What is Dewalt DCK278C2?
The Dewalt DCK278C2 is a comprehensive cordless tool kit featuring a drill/driver and an impact driver, both powered by the 20V MAX ATOMIC brushless motor technology.
It offers evaluation kits and reference designs related to the Dewalt DCK278C2, possibly providing additional resources for potential buyers.
Tool Kit Details:
- The Dewalt DCK278C2 comprises a cordless drill/driver, a cordless impact driver, two 20V MAX Lithium-Ion batteries, a charger, and a carrying bag.
- The cordless impact driver delivers 1700 in./lbs. It is of torque and is equipped with 3 LED lights for illumination in dark workspaces.
- The cordless drill/driver delivers 340 unit watts out (UWO) of power and features an LED footlight for visibility in low-light conditions.
Tool details about Fluke 325
- The Fluke325 True RMS Clamp Meter can measure up to 400A and 600V AC/DC, making it suitable for various electrical measurements.
- It measures capacitance, temperature, and frequency in addition to AC/DC and voltage.
- Some distributors highlight features such as backlit LCD, jaw capacity, and various functions like resistance, continuity, etc.
Makita large rising base miter saw stand
The Makita Large Rising Base Miter Saw Stand is an accessory designed to support and enhance the functionality of miter saws in professional settings. Here’s a breakdown of its features and purpose:
Versatility and Durability: The stand offers a versatile and durable platform for various professional trades, accommodating the needs of different job sites and applications.
Adjustable Height Configurations: It provides five height configurations, allowing users to adjust the stand according to their preferred working height or material requirements.
Material Support Extensions: The stand includes extensions extending up to 9 ft, providing ample support for long crown molding or other lengthy materials used in woodworking or construction projects.
It is specifically designed to complement and work seamlessly with Makita miter saws (sold separately), ensuring compatibility across a broad range of Makita saw models.
The stand can handle various cutting applications, such as crown molding, baseboard, case, and base, and long wood materials, making it a versatile companion for professionals in woodworking and construction.
The Makita Large Rising Base Miter Saw Stand is a robust, adaptable, and portable platform that supports the precision and efficiency of Makita miter saws across a spectrum of job site requirements and cutting tasks.
Are you looking for affordable and unique electronic components? WIN SOURCE is a reliable destination for diverse, high-quality electronic components. Their inventory boasts a wide selection of components from reputable manufacturers, ensuring quality and variety for various electronic needs. Whether you’re seeking semiconductors, connectors, capacitors, or other essential electronic parts, WIN SOURCE offers a comprehensive catalog that adheres to industry standards.
© 2024 Win Source Electronics. All rights reserved. This content is protected by copyright and may not be reproduced, distributed, transmitted, cached or otherwise used, except with the prior written permission of Win Source Electronics.

COMMENTS