We cannot deny the role of portable electronic devices in our daily lives. Devices like smartphones and advanced wristwatches require a reliable power source to ensure uninterrupted connectivity and productivity throughout our routines.
This blog delves into the world of the CR2430 battery – a lithium-based coin cell that offers numerous advantages, different types, and certain limitations. You can find a range of reliable CR2430 batteries at WIN SOURCE.
Table of Contents
ToggleUnderstanding the CR2430 Battery
Notably, due to their model, the CR2430 battery model delivers higher power output than other zinc-based batteries. Their function marks its excellence due to its ideal size in various devices, including cameras, calculators, and other portable electronic gadgets requiring this battery size. With an extended expiration date, customers can conveniently manage a continuous supply of CR2430 batteries for up to a decade.
Their chemistry influences the performance of batteries. The widely used CR2430 coin cells are crafted from stainless steel coated with nickel. Manganese dioxide forms the cathode, and the electrolyte comprises dissolved manganese salt in an organic solvent. Lastly, the anode cap is fashioned from lithium. It’s crucial to differentiate between primary lithium cells, which lack recharging ability, and secondary lithium-ion batteries, which can be recharged.
Benefits of Lithium Composition
Lithium’s high reactivity facilitates the movement of electrical current within batteries. Additionally, compared to metals like lead, its lightweight nature enhances energy transfer efficiency, making it indispensable for small devices like keyless entry remotes. Lithium is a fundamental component found in most button or coin cells available in the market. Manganese dioxide, another essential element, contributes to the battery’s functionality and durability.
The CR2430 Lithium Coin Battery: Specifications
The CR2430 Lithium Coin Battery has the dimensions of 24.5 millimeters in diameter and 3 millimeters in height. This battery boasts a substantial 300mAh capacity for enduring performance. Its low 200µA discharge rate suits energy-efficient applications, while bulk packaging ensures convenient handling and storage. Proper termination requires a holder. Its compact dimensions, with a 0.96″ diameter and 0.12″ height, make it ideal for fitting into smaller devices.
Advantages of the CR2430 Battery
The CR2430 battery offers a host of benefits that make it a popular choice for various portable devices:
Compact Size: The CR2430 battery’s compact size enables it to fit seamlessly into even the smallest devices, allowing manufacturers to design sleek and lightweight gadgets without compromising performance.
Full Range Power: The tiny CR2430 battery has a high energy density, allowing devices to run for long periods without recharging. The battery is ideal for active people who need a longer-lasting battery.
Durability: The CR2430 is composed of high-quality components to withstand daily use. This guarantees the battery will have a long lifespan and be dependable in various situations.
Wide Application Range: From medical devices to fitness trackers, the CR2430 battery finds its place in diverse applications, showcasing its versatility and adaptability.
Easy Replacement: As the adoption of CR2430 batteries increases, finding replacements becomes more convenient, with electronic stores and online retailers stocking these batteries for hassle-free procurement.
Types of CR2430 Batteries
One type of CR2430 battery can be recharged, whereas another cannot.
One-time-use CR2430 batteries are cheap and easy to find. These batteries were built for specialized applications and operate best in electronics that don’t need power source replacements. Proper disposal is essential since these batteries cannot be reused and may harm the environment.
The rechargeable CR2430 battery doesn’t need replacing. This is greener. Though initially more expensive, their decreased battery replacement frequency makes them a better bargain. Reducing single-use battery use helps the environment.
Understanding Limitations
While the CR2430 battery provides numerous advantages, it’s essential to acknowledge its limitations:
Limited Capacity: Due to its compact size, the CR2430 battery has a relatively limited capacity compared to larger batteries. This limitation makes it suitable for smaller devices but unsuitable for gadgets with high energy demands over extended periods.
Slow Charging (for Rechargeable Batteries): Rechargeable CR2430 batteries may charge slower than disposable alternatives. This aspect can be inconvenient when waiting for devices to charge.
Self-Discharge: Like all batteries, CR2430 batteries experience self-discharge over time, even when not used. This phenomenon may result in a loss of charge when using devices infrequently.
Variants of CR2430 available at WIN SOURCE
1. CR2430: Empowering with Consistency
Introducing Murata Electronics North America’s CR2430 – a compact non-rechargeable lithium coin battery packed with benefits. Its 24.5mm diameter powers wearables like fitness trackers, ensuring seamless connectivity. This 3V silent powerhouse plays a pivotal role in maintaining functionality for portable electronics. The 580333-CR2430, part of the CR2430 series, boasts 300mAh capacity, 200µA discharge rate, and 3V output. Designed by Murata Electronics, it’s a reliable choice for diverse applications, fitting snugly into compact devices.
2. CR2430VP: Trust in Performance
Discover the dependable CR2430VP lithium coin battery by Energizer Battery Company, a trusty power source with a 3V output and 24.5mm diameter. From remote controls to healthcare devices, it fuels seamless operation for calculators, remotes, and medical tools. With a capacity of 290mAh and medium popularity, it ensures your devices’ vitality. Remember, it requires a holder for termination, and you can find it through us with ample supply.
Summing Up
The CR2430 battery unlocks a world of marvels and advantages. Its unassuming appearance belies the remarkable benefits it brings to your devices. It’s the driving force behind your tech essentials, ensuring they function flawlessly and stay powered up when you need them the most.
In essence, the CR2430 battery is a testament to the fact that great things come in small packages. We’re committed to delivering these essential components that enhance your daily experiences. So, the next time you interact with your favorite device, remember that the true magic lies within – the CR2430 battery, your gateway to a world of benefits, available at WIN SOURCE.

COMMENTS